Filtration

How to Solve Baghouse Airflow Restriction in Foundry Applications

How to Solve Baghouse Airflow Restriction in Foundry Applications | Case Study-Foundry_Parker Industrial Gas Filtration and Generation DivisionEfficient operation of baghouses is an expected and necessary element of foundry productivity. These manufacturing facilities and systems assure clean and safe work environments, allowing people and equipment to operate without interruption. When the media, often filter bags, employed in the baghouses plugs with collected solid matter, immediate maintenance is an absolute priority. The proper function of baghouse filtration is integral to efficient foundry operations.

This was the case at a large foundry located in the United States where restricted air flow to mold cooling and sand handling equipment had reached a critical point.

 

How to Solve Baghouse Airflow Restriction in Foundry Applications | Case Study-Download-Case-Study-Parker Industrial Gas Filtration and Generation DivisionFor more information on this application and to learn how BHA® PulsePleat® filters can help you reduce costs and improve baghouse performance, download the full case study.

 

 

 

The problem

The foundry employed a 450-bag Carborundum pulse-jet baghouse. The system had been designed with an air-to-cloth ratio of 9.3:1, aggressive by any standards. The processing at the foundry exposed the filter media to very fine particulate. Specifically, the particulate came from the sand handling system. This particulate, along with high moisture and hydrocarbon carryover from the mold cooling line, formed a substantial and difficult dustcake on the filter media in the baghouse. After only six months of service, blinded filter bags caused differential pressure to exceed 8” w.c., greatly reducing airflow venting of the applications. As a result, time-consuming and costly filter bag and cage change outs were required.


The solution

The foundry determined that they needed the help of experts in the area of filtration, specifically with baghouse efficiency and performance. They turned to Parker Hannifin, a leader in the design and manufacture of filtration systems.  Parker recommended replacing filter bags and cages with BHA® PulsePleat® Filter Elements — a versatile and cost-effective solution. They designed the system in order to increase the total filtration area of the dust collector by over 220%. This was done with no physical modification of the dust collector.

How to Solve Baghouse Airflow Restriction in Foundry Applications | Case Study-Download-BHA PulsePleat Filters-Parker Industrial Gas Filtration and Generation DivisionBenefits of BHA® PulsePleat® filters elements

  • Spunbound polyester media provides superior filtration efficiency.
  • Promote better airflow for increased throughput.
  • Pleated design increases filtration surface area up to 4X.
  • Molded bottom helps resist abrasive wear.
  • Reduce air-to-cloth ratios.
  • Reduce operating differential pressure.
  • Reduce compressed air consumption.
  • Eliminate the need for cages.
  • Easy installation and removal.
  • Installation typically requires no modification to existing equipment.

 


Results

How to Solve Baghouse Airflow Restriction in Foundry Applications | Case Study-Download-Results-Parker Industrial Gas Filtration and Generation Division

 

Performance

The new system, featuring an increased filter surface area of the pleated elements, helped lower average differential pressure to 3.5” w.c. — a greater than 40% reduction from the peak of 8” w.c.  

Fan amps went up by 157%, increasing air volume through the dust collection system and providing the ventilation needed by the process applications for optimum performance.  

Installation and maintenance

The one-piece bottom-load design of BHA® PulsePleat® filters elements reduced filter installation time by 70%.
The increased filter surface area contributed to a dramatic reduction of unplanned maintenance time and expense.


Conclusion

By installing BHA PulsePleat filter elements, the foundry returned to efficient production and avoided the high costs of unplanned maintenance and baghouse redesign or replacement.

To learn more about BHA PulsePleat filter elements, watch this video:


How to Solve Baghouse Airflow Restriction in Foundry Applications | Case Study-Download-Case-Study-Parker Industrial Gas Filtration and Generation DivisionFor more information on this application and to learn how BHA® PulsePleat® filters can help you reduce costs and improve baghouse performance, download the full case study.
 

Article contributed by the Industrial Air Filtration Team.
 

Related content

Foundry Eliminates Shutdowns and Extends Baghouse Filter Life

Filter Upgrade Improves Bin Vent Dust Collector Performance

BHA® Pleated Filter Elements Improve Dust Collection for the Foundry Industry

Filter Upgrade Improves Baghouse Performance in Industrial Manufacturing

Choosing the Best Dust Collector for Air Quality Control in Manufacturing

 

Have a question about Parker products or services? We can help: Contact Us!

Comments for How to Solve Baghouse Airflow Restriction in Foundry Applications


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha