Electromechanical

How Using Electric Linear Actuators Can Save You Money

Save Money with Electric linear motor actuators Parker ETT SeriesIt’s well documented that creating compressed air for use by pneumatic cylinders is not a particularly cost-effective process, largely as a result of generator and system inefficiencies. With accounts departments leaning hard on engineers to deliver lower operating costs, increasing numbers are turning to the latest electric actuator solutions.

 

Why so?

Well, the design features of electric linear actuators mean they are able to deliver enhanced performance levels while also achieving lower total energy consumption. In fact, based on trials, savings of €3,200 can be anticipated for a typical single-actuator application over a two-year period.

 

Two steps become one

In pneumatic systems, two steps are necessary to produce compressed air: electricity first produces air, before air pressure is converted into linear movement using a pneumatic cylinder. Similarly, two stages are required in a traditional electric solution, namely converting motor rotation to the movement of the electric actuator.

Electric linear motor actuators Parker ETT Series Machine Design

However, this double step can be reduced, with subsequent energy savings, by using a linear motor rod-style actuator solution such as a Parker ETT series unit, which is able to directly generate linear motion through the principle of electromagnetism.

Another favorable attribute of an electric linear motor actuator compared versus a pneumatic actuator solution is the precise positioning achievable along its entire stroke. On-board feedback via an integrated analogue linear position sensor allows positioning precision to within 0.05mm.

 

Advantages of electric actuators: significant savings potential

The technical advantages of the latest electric linear motor actuators are clear, but what about the cost comparison we hear you ask?

Well, consider electric actuators applications and performance. A typical application involving the transfer of a 15kg load at 30 cycles per minute, for example. Here, a pneumatic cylinder solution would work with a pressure of approximately 2 bar, while the Parker ETT linear motor actuator solution consumes just 30W of electricity every cycle. Sure, the initial start-up cost for the electric actuator solution is higher than its pneumatic counterpart, but the cumulative energy cost savings mean your initial investment would be recouped well within one year.

Savings Chart from Electric Linear Motor Actuators Parker ETT Series

Moreover, just 24 months after start-up, savings will have increased to around €3,200. This savings is for just one actuator—if you multiply the number of actuators found on a typical production line it's easy to see the vast savings possible.

 

Learn more

Download our electric tubular motor catalog to learn more about how your plant can save money on its factory automation.

 

How Using Electric Linear Actuators Can Save You Money-Alessandro Porro-Electromechanical Division Europe-Parker Hannifin CorporationArticle contributed by Alessandro Porro, product manager, Motors, Electromechanical Division Europe, Parker Hannifin Corporation.

 

 

 

 

Related content

Tube Bending OEMs Embracing All-Electric Automation

What’s Trending in Industrial Automation?

Choose the Right Screw Drive Train With Actuator Performance Calculator

Have a question about Parker products or services? We can help: Contact Us!

Comments for How Using Electric Linear Actuators Can Save You Money


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha