Sealing Shielding

How to Enhance Performance and Safety of Static Radial Seals

Seal HSO-ring/back-up ring combinations have thus far been considered the industry standard for static applications at high pressures. In field use, however, they may show weaknesses with respect to their installation and operation in the application. Standard O-rings, for instance, are often prone to twisting while back-up rings are not installed in the proper position or damaged during installation. Furthermore, this sealing combination may exhibit deficits when exposed to pulsating pressures and dirt.

Parker has developed the HS seal profile as a viable alternative to to conventionally used O-ring/back-up ring combinations for static sealing applications at high pressures. The robust symmetrical seal geometry and use of particularly extrusion-resistant Parker polyurethane compounds not only simplifies installation but also enhances the sealing effect in pulsating pressure conditions. As a result, service life is significantly extended.
 

Advantages for the user

The HS seal, compared to the conventional O-ring/back-up ring combinations, offers the following advantages:

  • Easy installation
  • No twisting
  • High extrusion resistance of the polyurethane materials
  • Extrusion resistance many times higher than that of conventional O-rings
  • Longer service life
  • Suitable for standard O-ring grooves with back-up rings
     

Finite elements analysis illustrates reliable operation at high pressures

Finite Elements Analysis of Profile HS

The figures show the results of finite elements calculations on the HS profile in two operating conditions, i.e. when installed at room temperature, in pressure-less conditions (Fig. 1), and after pressure loading of 600 bar plus heating to 60 °C (Fig. 2), each time with a reduced extrusion gap. The colour scale shows the stress levels in the seal in radial direction whereas the length of the vertical lines in the contact area between the seal and the groove represents the level of the surface pressure or sealing pressure that acts there.

The compression areas of the sealing edge pairs of the HS profile can be clearly detected in both figures. This compression leads to a distribution of the sealing pressure with two peaks where the pressure amounts to around 20 MPa. In Fig. 2, it is overlapped by the hydrostatic pressure of 600 bar, with the curve essentially remaining unchanged.

The advantages of the HS seal result from the serial configuration of the two sealing areas, which doubles the protection against leakage compared to a single seal. In addition, with two sealing areas or sealing edge pairs backing up the seal, exceptional protection against twisting of the seal is achieved, both during installation and in operation at pulsating pressures, for instance in combination with breathing components and coaxiality defects of the groove. 

The use of particularly extrusion-resistant materials, especially the P6000 polyurethane compound with 94 Shore A hardness, eliminates the need for back-up rings. This is illustrated in Fig. 2 as here, in the area of the sealing gap on the non-pressurised side, only minor extrusion can be expected even at a pressure of 600 bar and increased temperature. Furthermore, the elimination of back-up rings provides advantages due to simplified installation. 
 

Range of application

The Ultrathan® seal HS is suitable for radial, static applications at high pressures such as:

  • Hydraulic valves
  • Hydraulic cylinders
  • Machine tools
  • Injection-moulding machines
  • Any static sealing point requiring radial sealing

For more information about the HS static radial seal, download the brochure or contact the experts at Parker-Prädifa.

 

Article contributed by Dr. Peter Kreißl,
Market Unit Manager Hydraulics, 

Engineered Materials Group,
Packing Division Europa

 

 

 

Related content:

Tandem sealing system enhances performance of mini excavator actuators 

 

Categories
Recent Posts by Author

How to Solve Large-Size Sealing Challenges at Temperatures up to 800 °C

When classic sealing materials – for instance in temperature ranges above 300°C and below -50°C – reach their limits alternative materials are required such as metal with appropriate coating/plating....

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for How to Enhance Performance and Safety of Static Radial Seals


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha