Climate Control

HVACR Tech Tip: Using Bi-Directional Solenoid Valves for Heat Pumps

HVACR Tech Tip: Using Bi-Directional Solenoid Valves for Heat Pumps - Solenoid valve with built in check valve CE6Hp Series - Parker SporlanA solenoid valve with a built-in check valve is designed to replace a liquid line solenoid valve in parallel with a check valve for reverse flow. This valve may be applied in the liquid line of a supermarket case for positive shutoff during pump down control, while allowing full flow in the reverse direction during reverse gas defrost. It may also be used in the liquid line of a heat pump to prevent migration of refrigerant to the outdoor unit during the heating mode, while allowing full flow in the reverse direction during the cooling mode.

CAUTION: This valve will not close in the reverse flow/cooling mode.

CE6-HP SERIES SOLENOID VALVES

  • For Refrigerants 22, 134a, 404A, 407C, 407F, 410A, 507
  • Bi-Directional Solenoid Valve
  • Supermarket Pumpdown Control
  • Prevents Heat Pump Refrigerant Migration
  • Extended Solder Type Connections
  • MKC-1 Coil, Class F


See Figure 1. The check ball is small and inserted into the pilot port of the disc. When the valve is energized for operation in the refrigeration flow direction, the pressure on top of the disc is bled off through the pilot port and the disc raises. When the evaporator goes into defrost or the heat pump switches to the cooling mode, the solenoid valve must be energized. The reverse flow causes the check ball to close the pilot port from the bottom, pushing the disc up, fully opening the valve. 

 

HVACR Tech Tip: Using Bi-Directional Solenoid Valves for Heat Pumps - figure 1 cutaway of solenoid valve with built in check valve - Parker Sporlan

 

 

 

 

 

 

 

 

 

Figure 1

CE6S1-HP* BI-DIRECTIONAL SOLENOID VALVE* 

The “C” is used in this nomenclature to represent the check valve feature and the“-HP” designates high pressure.
The check valve disc also requires a modification in the stem and plunger assembly. Therefore, the disc and stem and plunger assembly must be changed to convert a standard solenoid valve to one with a built-in check valve. Internal parts kits are available for solenoid valves with the built-in check valve.

 

Name:  Screen Shot 2016-06-28 at 1.38.57 PM.png
Views: 85
Size:  97.4 KB

CE6S1-HP BI-DIRECTIONAL SOLENOID

HEATING MODE (shown above)
Typically, the valve is installed with normal flow to the outdoor coil. When de-energized, this prevents migration of refrigerant to the outdoor coil during heating mode.

COOLING MODE
Typically the valve is installed with normal flow to the outdoor coil. When in cooling mode, the valve is in reverse flow.

For Supermarkets
See Figure 3 below. For reverse gas defrost, a liquid line solenoid valve can be installed with a check valve in parallel, to allow reverse flow to the liquid header. This adds the expense of labor and materials. Or, a Sporlan liquid line solenoid valve with the built-in check valve feature can be installed, saving time and money. 

 

Name:  Screen Shot 2016-06-28 at 1.30.52 PM.jpgViews: 83Size:  83.6 KB

 

Six Reasons Why CDS Conversion Reduces Cost - Dustin Searcy, Product Manager Electric ValvesArticle contributed by Dustin Searcy, Product Manager, Electric and Solenoid Valves, Sporlan Division, Parker Hannifin 

 

 

 

 

 

 

Additional HVACR Tech Tips can be found here:

HVACR Tech Tip: Troubleshooting Solenoid Valves in Refrigeration Applications

HVACR Tech Tip: Guide to Servicing Blended Refrigerants

HVACR Tech Tip: Can You Have Subcooled Refrigerant in the Receiver?

Six Reasons Why CDS Conversion Reduces Costs

Clean-up Procedure for Refrigeration and Air Conditioning Systems

Compressor Overheating Is the Number-One Refrigeration Problem

HVACR Tech Tip: Where Should the TEV External Equalizer Be Installed?

 

Have a question about Parker products or services? We can help: Contact Us!

Comments for HVACR Tech Tip: Using Bi-Directional Solenoid Valves for Heat Pumps


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha