Superheat is the temperature of refrigerant gas above its saturated vapor (dewpoint) temperature. Superheat as it relates to thermostatic expansion valves, can be broken down into three Superheat categories:
Static Superheat – The amount of superheat necessary to overcome the superheat spring force biased in a closed position. Any additional superheat (force) would open the valve.
Opening Superheat – The amount of superheat necessary to open the valve to its rated capacity.
Operating Superheat – The superheat at which the valve operates at normal running conditions or normal capacity. The operating superheat is the sum of the static and opening superheat. The figure below illustrates the three superheat categories. The reserve capacity, as shown in the graph, is important since it provides the ability to compensate for occasional substantial increases in evaporator load, intermittent flash gas, reduction in high side pressure due to low ambient conditions, shortage of refrigerant, etc.
For more information, download TEV &AEV Theory and Application - Catalog E-1a.
Determine the suction pressure at the evaporator outlet with gauge. On close coupled installations, suction pressure may be read at the compressor suction connection.
Use the Pressure-Temperature Chart to determine the saturation temperature at observed suction pressure. For example, with an R-22 system: 54.9 psig = 30°F.
Measure the temperature of the suction gas at the expansion valve’s remote bulb location. For example 40°F.
Subtract the saturation temperature of 30°F (step 2) from the suction gas temperature of 40°F (step 3). The difference 10°F, is the superheat of the suction gas.
Parker “sets” the thermostatic expansion valve superheat at the static condition described above. Turning the adjusting screw clockwise will increase the static superheat. Conversely, turning the adjusting screw counterclockwise will decrease the superheat. Parker valves can also be adjusted at the operating point, indicated above. When a system is operating, any adjustments made will change the operating superheat. The static superheat range of adjustment is 3°F to 18°F. One full turn clockwise will typically increase superheat 2°F to 4°F. Note: Refer to the valve’s installation bulletin for specific directions on superheat adjustment.
For more information, download TEV &AEV Theory and Application - Catalog E-1a.
For more details on Thermostatic Expansion Valves - Theory of Operation, Application, and Selection - Bulletin 10-9.
Article contributed by Glen Steinkoenig, product manager, Thermostatic Expansion Valves, Sporlan Division of Parker Hannifin.
Related, helpful climate control content for you:
HVACR Tech Tip: 12 Solutions for Fixing Common TEV Problems
HVACR Tech Tip: Understanding and Preventing Superheat Hunting in TEVs
HVACR Tech Tip: Principles of Thermostatic Expansion Valves
HVACR Tech Tip: Where Should the TEV External Equalizer Be Installed?
Have a question about Parker products or services? We can help: Contact Us!
Comments for HVACR Tech Tip: Everything You Want to Know About Superheat
Please note that, in an effort to combat spam, comments with hyperlinks will not be published.