Climate Control

HVACR Tech Tip: Understanding Torque Specifications and Applying Torque

Parker Sporlan Defrost Differential Pressure Regulating Valves for Supermarket Systems OLDR-21Working in the HVAC and Refrigeration industry there are many times when you are going to have applied torque when working on a particular job. In this blog, we help you understand the basics of torque and a method of applying torque. A bolt that has been over tightened can be just as disastrous as one that hasn't been tightened enough. A bolt that has been tightened beyond recommended torque specs can easily break in service.

 

Torque Specifications

Torque is measured as a unit of force acting on a rotating lever of some set length. North American made hex head cap screws have radial lines on their heads that indicate their tensile strength. When replacing a fastener, use a quality at least equal to or greater than the original fastener used on the machine. The more marks on the head, the higher the quality. Thus, bolts of the same diameter vary in strength and require a correspondingly different tightening torque or preload. Remembering that torque is the turning effort or force applied to the fastener to preload it, or place it in tension, and is normally expressed in inch-pounds (in.lb) or foot-pounds (ft.lb). A one pound weight or force applied to a lever arm one foot long exerts one foot-pound or twelve inch-pounds of torque. Note: Where possible always use OEM torque values which may differ from the table below.

 

SAE Bolt head markings

SAE Bolt Head Markings

 

 

 

 

 

 

 

Maximum torque table

All torque values are expressed in ft.lb.

Maximum Torque Table

 

Method of applying torque

Always run fasteners up snug (do not over tighten) with a regular wrench and then observe the following four steps unless OEM instructions are available.

  1. Run each fastener in the proper sequence up to 1/3 of their recommended torque setting.

  2. Repeat the process running up to 2/3 of the required torque setting.

  3. Repeat the process again, running every fastener up to full torque.

  4. Repeat step #3 to be positive you have not missed a fastener.

For various HVAC and Refrigeration product information visit www.Parker.com/Sporlan
 

 

Use of Suction line filter driers for clean-up after burnout of HVAC systems - Glen Steinkoenig Product Manager Contamination Control Products, Parker Hannifin Sporlan Division Article contributed by Glen Steinkoenig, product manager, Contaminant Controls, Sporlan Division of Parker Hannifin.

 

 

 

 

Related, helpful climate control content for you:

HVACR Tech Tip: What You Need to Know About Flooded Head Pressure Control

Six Reasons Why CDS Conversion Reduces Costs

HVACR Tech Tip: 12 Solutions for Fixing Common TEV Problems

Have a question about Parker products or services? We can help: Contact Us!

Comments for HVACR Tech Tip: Understanding Torque Specifications and Applying Torque


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha