Climate Control

HVACR Tech Tip: Where Should the TEV External Equalizer Be Installed?

HVACR Tech Tip: Where should the TEV External Equalizer be Installed - Sporlan Thermostatic Expansion Valve Group image - Parker Hannifin Sporlan DivisionIn air conditioning and refrigeration applications, the ability of the thermostatic expansion valve (TEV) to match refrigerant flow to the rate at which refrigerant can be vaporized in the evaporator makes the it the ideal expansion device for most HVACR applications. The TEV controls the flow of liquid refrigerant entering the direct expansion (DX) evaporator by maintaining a constant superheat of the refrigerant vapor at the outlet of the evaporator.

Superheat is the difference between the refrigerant vapor temperature and its saturation temperature. To measure the superheat the TEV controls, the difference between the actual temperature at the sensing bulb and the saturation temperature corresponding to the suction pressure at the sensing bulb location is determined. By controlling superheat, the TEV keeps nearly the entire evaporator surface active while not permitting liquid refrigerant to return to the compressor.

Where do you install?

The purpose of the external equalizer is to sense the pressure in the suction line at the bulb location and transmit it to the TEV diaphragm. This usually means installing the external equalizer immediately downstream from the bulb. This ensures the correct pressure is signaled to the TEV.

In some situations this “ideal” location may not be possible. In these cases, an alternate location, such as at B or C (see diagram), could be used. However, the pressure at these locations must be nearly identical to the pressure in the line where the bulb is located.
 

HVACR Tech Ti: Where should the TEV External Equalizer Be Installed?
 

In other words, locations B and C are acceptable as long as these pressures are essentially the same as A when the system is operating at full load. In the past there has been concern about installing the external equalizer “up-stream” from the bulb. This was due to the possibility of refrigerant leaking past the TEV push rods, passing through the equalizer line and into the suction line, thus falsely influencing the TEV bulb temperature.

Today, with Sporlan’s TEV design, this possibility is virtually eliminated.

 

HVACR Tech Tip: Where should the TEV External Equalizer be Installed? - Jason Forshee product mgr Thermostatic Expansion valves - Sporlan Division, Parker Hannifin

HVACR Tech Tip Article contributed by Jason Forshee, Product Manager,  Sporlan Division of Parker Hannifin

 

 

 

 

Additional resources:

Six Reasons Why CDS Conversion Reduces Costs

Compressor Overheating Is the Number-One Refrigeration Problem

Head Pressure Control for Supermarkets

Using P-T Analysis as a Service Tool for Refrigeration Systems

Clean-up Procedure for Refrigeration and Air Conditioning Systems

How to Use the Smart Service Tool Kit for HVACR Diagnosis

Climate Control Technologies and Key Markets

Categories
Recent Posts by Author

How to Drive Business With HVACR Trends - Infographic

What’s changing in HVAC? It might be simpler to ask what isn’t changing. According to Steve Yurek, the president and CEO of the Air-Conditioning, Heating, and Refrigeration Institute (AHRI),...

HVACR Tech Tip: How to Correctly Size Solenoid Valves

To obtain reliable performance with solenoid valves on refrigeration or air conditioning systems, it demands careful consideration of application requirements during the selection process. Parker...

HVACR Tech Tip: Protect Your System During Maintenance With These Steps

Simple maintenance steps for system reliability There are simple steps that an HVACR technician can take during their routine spring and fall inspections or at any time when onsite to...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for HVACR Tech Tip: Where Should the TEV External Equalizer Be Installed?

David
Thanks this is great information.

Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha