Hydraulics

Hydraulic Cylinders Enable Artistic Architecture at University | Case Study

Hydraulic Cylinders Enable Artistic Architecture at University | Case Study | IST building at Florida Polytechnic University | Hydraulic Cylinder DivisionA massive engineering and design collaboration have brought the vision of world-renowned Spanish architect Santiago Calatrava Valls to life in Lakeland, Florida. The new Innovation, Science and Technology (IST) Building at Florida Polytechnic University will serve as the central building for the campus of Florida’s newest state institution, dedicated to a curriculum of science, technology, engineering, and math. It houses classrooms, auditoriums, administrative offices, common areas and a number of cutting-edge laboratories; including a Supercomputer and Student Data Center, a Visualization and Technology Collaboration Lab, and a Rapid Application Development Makerspace Lab with 3D printing capabilities. The $60 million, two-story building also includes a system of 94 louvered arms that raise and lower to track the sun above a glass roof.

Each louver is manipulated by a Parker Series 2HB Mill-Type hydraulic cylinder. The custom application required five different sized cylinders, with larger cylinders for the longer louvers at the center of the roof and smaller cylinders for the shorter louvers at the ends.

“We are pleased to have supported this highly customized cylinder application with full integration capabilities and precise engineering,”
Tad Brown, cylinder application engineer, Parker Hannifin Cylinder Division

 

Specifying assembly to design

Hydraulic Cylinders Enable Artistic Architecture at University | Case Study | non-tie-rod hydraulic cylinders | Parker Cylinder DivisionSpecified by Parker distributor Atlantic Hydraulic Systems, based in Shirley, N.Y., each cylinder was assembled with integrated cartridge valves on a manifold, which was bolted to the cap and plumbed to the head end of the cylinder. Further, a spherical rod eye was installed at the rod end, and the entire cylinder was painted to match the remainder of the structure. This full integration, along with special pressure decay testing, was all accomplished within Parker’s Cylinder Division in Goodland, Indiana.

Hydraulic Cylinders enable Artistic Architecture at University | Parker 2HD hydraulic cylinder in louver application | Parker Cylinder DivisionThe cylinders act independently from one another and can manipulate the louvers to provide shade and artistic motion. The louvers were designed to eventually accommodate a system of photovoltaic tape to generate power for the campus. Each louver arm is engineered with the capability of a maximum upright position of 65 degrees above the horizontal plane and a maximum lowered position of 48 degrees below the horizontal plane. Traveling the full 113-degree distance takes about 10 minutes.

Construction of the 162,000 square foot IST building took 28 months and was completed by Skanska USA. Headquartered in New York, Skanska USA is one of the largest construction and development companies in the country with expertise in construction, civil infrastructure, public-private partnerships and commercial development initiatives in select U.S. markets. Florida Polytechnic welcomed students for the inaugural day of classes on August 25, 2014. The University offers six undergraduate degree programs with 19 unique areas of concentration and two masters degree programs in the College of Engineering and the College of Innovation and Technology.


Proven design built to industry standards

The 2HB cylinder design in long-stroke industrial applications is an engineering breakthrough that is expected to extend service life, reduce downtime, increase throughput and ultimately increase the profitability of industries requiring stroke lengths over five feet. For OEMs incorporating cylinders into heavy-duty industrial equipment and machines or into apparatus where design aesthetics are important, the 2HB Series of non-tie-rod cylinders offer several differentiating benefits for competitive advantage.

Hydraulic Cylinders Enable Artistic Architecture at University | Case Study | Long-Stroke Industrial Cylinder Performance white paper cover | Cylinder DivsionLearn more about the benefits of non-tie-rod hydraulic cylinders and how they can improve performance in your heavy-duty, long-stroke industrial applications - download our Long-Stroke Industrial Cylinder Performance white paper. 

 

For more information on the award-winning IST building and the new Florida Polytechnic University, visit their website.

 

 

Article contributed by Hydraulic Team, Parker Cylinder Division.

 

 

 

 

 

Related, helpful content for you:

OEM Design Engineer's Guide to Specifying Hydraulic Cylinders

Essential Factors for Selecting Hydraulic Cylinders for Tough Operating Environments in Aluminium Processing

Smart Cylinders Reduce Operational Costs

Challenged with Long-Stroke Hydraulic Cylinder Performance? Read This

Smart Hydraulic Cylinder Optimizes Hydroelectric Dam Gate Control

How to Install Pneumatic Cylinders to Maximise Life and Performance

Have a question about Parker products or services? We can help: Contact Us!

Comments for Hydraulic Cylinders Enable Artistic Architecture at University | Case Study


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha