Food Beverage Filtration

Identifying the Cause of a Beer Quality Issue | Case Study

Identifying the Cause of a Beer Quality Issue_Beer and Hops_Parker Bioscience Filtration

As the brewing industry is becoming more competitive, breweries of all sizes realize the importance of producing a higher quality product while keeping an eye on the bottom line at the same time. When production issues arise that jeopardize production efficiency and final product quality, immediate corrective action is critical. 

When a small brewery, which was using sterile filtration to protect beer quality and flavour, discovered that its final product was not up to standard, they called Parker Bioscience Filtration's technical support group (TSG). The TSG team works with partners in the brewing industry to solve complex challenges involving beer quality and production efficiency.

The brewery had identified that after a beer had been passed through a filtration system following a clean-in-place (CIP) cycle, the product had little or no head. Clearly, this was of significant concern.

 

How did Parker support the brewery?

Parker Bioscience Filtration’s TSG team observed that the brewery was using a caustic detergent containing de-foaming surfactants for CIP of its three-stage filtration system at 60°C. This solution breaks down organic matter, including fats and is therefore commonly used in brewing applications. The antifoaming surfactant components help to control any soaps and surface-active derivatives which may form, especially in processes which feature high mechanical action – such as a CIP process.

The Parker team analysed both the used filters (Parker PEPLYN NG prefilters and BEVPOR BR membrane filters) and a sample of the caustic detergent solution used in the CIP process.

It was found that while the de-foaming surfactant within the solution was soluble at an ambient temperature, it became colloidal at elevated temperatures. This was apparently due to a significantly higher turbidity measurement at 60°C compared to 45°C. After filtration of the solution through a 10µm and 1µm PEPLYN system, turbidity measurements showed a significant decrease.

 

Identifying the root cause

Testing showed that the colloidal de-foaming surfactant within the caustic detergent solution had been trapped and retained by the PEPLYN filters. When the beer was then passed through the filters, the residual de-foaming surfactant present on the filters removed the head from the beer.

 

The solution

TSG supported the brewery on-site while a new CIP regime was successfully trialed and implemented. This CIP regime did not cause residual de-foaming surfactant to be present on the filters, ensuring that the beer product retained its head after filtration.

Visit our website for more information about brewing industry products and solutions.

Amy Miller_technical support scientist_Parker Bioscience Filtration

Katy Angus_research scientist_Parker Bioscience Filtration

This post was contributed by Amy Miller, technical support scientist and Katy Angus, research scientist, Parker Bioscience Filtration, United Kingdom

Parker Bioscience Filtration offers filtration solutions to protect the quality and taste of beverage products. By working with our application experts, manufacturers can develop a tailored solution to ensure their beverage is free from contamination, full of flavour and visibly clear. 

 

Related content

The Benefits of Changing Your Microbial Stabilisation Process to Sterile Filtration

Improving the Shelf-Life of Your Beer with Sterile Filtration

The Sterile Filtration of Beer - Keeping up with Consumer Trends

Sterile Filtration of Beer - Saving Water, Saving Energy

Microbial Control - What’s Spoiling My Beer?

How to Protect Beer Quality at the Lowest Cost

Sterile Filtration of Beer - The Impact on Quantity and Quality

Categories
Recent Posts by Author

Supporting Bottling Operations in the Wine Industry

Parker's Technical Support Group works hand in hand with customers to help them overcome operational challenges and optimize their filtration systems. We build close relationships with...

Putting Filter Blockages Under the Microscope

Filter blockages in a beer production process can cause serious problems for breweries which can include increased expenditure on replacement filter cartridges and a significant amount of downtime in...

Reduce Microbial Hazards in Dairy Manufacturing with Pharmaceutical Best Practices

When it comes to the use of sterile gas for product contact purposes – such as aseptic packaging or product purge applications – no clear guidelines have been adopted by the dairy industry regarding...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Identifying the Cause of a Beer Quality Issue | Case Study


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha