Compressed Air Gas Treatment

Important Reasons to Filter Culinary Steam

Filter Culinary Steam to Protect Food Quality and Reduce CostsCulinary steam is frequently used in food-processing operations.  It is directly injected into the food product stream to control temperature and consistency of the food product. Jets of culinary steam can also be used to open the packaging and sterilize food-contact surfaces. Because it is in direct contact with food products and surfaces, culinary steam must be free of contamination and meet all applicable FDA and USDA food-processing standards.

Delivery methods for culinary steam include heat exchangers and direct injection. Heat exchangers are expensive to purchase, operate, and maintain. As a result, more food processing companies are turning toward direct steam injection systems. These systems cost less than heat exchangers and are smaller, incorporate less stainless steel, and are easier to operate. They also use less energy and steam, which further reduces operating costs. Direct steam injection increases the speed of production and processing because the food product reaches the desired temperature faster compared to heat exchangers.

Improved food safety, lower cost

There are two big advantages to using direct steam injection:

  1. By being able to purify steam to such exact standards, direct steam injection systems protect the integrity of the food product, resulting in increased consumer satisfaction and demand.
  2. Direct steam injection systems reduce overall operating costs compared to heat exchangers. Because the steam is constantly mixed in the process stream, 100 percent of the heat is transferred (with heat exchangers, condensate must be collected). Direct steam injection systems also consume about one-third less energy than heat exchangers, which improves efficiency and reduces operating costs.

Importance of filtration

Although steam is sterile and free of microorganisms, it can carry contaminants such as rust, pipe scale, and other particulate matter. It also contains con­densed water and chemicals from boiler feed water additives. These contaminants must be removed from the steam to protect the food’s natural taste, texture, color, and appearance. Typically, single stage filtration is recommended as close as possible to the point of use.

Parker Balston steam filters, for example, are in full compli­ance with the U.S. Food, Drug and Cosmetic Act and 3A Accepted Practices (609-04) for producing culinary quality steam. They also meet the regu­lations for indirect food additives used as “basic components for repeated use food contact surfaces” as specified in 21 CFR Part 177 and Current Good Manufacturing Practices 21 CFR Part 110. The filters are also accepted by the USDA for use in federally inspected meat and poultry plants.

Other advantages of Parker Balston steam filtration systems include:

  • 98+ percent capture rating at .10 micron of solids, excess condensate, and boiler feed water additives
  • Six-week filter element life
  • Allows for direct injection cook­ing, making the process more efficient and ensuring more even distribution of heat
  • Safe for contacting food

Direct steam injection is a fast, cost-effective method for heating a food product stream, and when properly filtered, it allows food processors to increase production at lower cost, yet still maintain the food product’s natural color, texture, and desired taste on a consistent basis, from batch to batch.

Filter Culinary Steam to Protect Food Quality and Reduce Costs - Parker HannifinRead this marketing application for more information on steam filtration

 

 

 

 

This post was contributed by the Compressed Air & Gas Treatment Blog Team, Parker Hannifin

 

 

 

Related posts:
Is the Compressed Air in Your Food Plant Safe?

Are You Ready for an Audit? Is Your Plant Compressed Air in Compliance with GFSI, SQF, and BRC Codes? Part 1 of 6

How to Manage the Risks of Food Product Contamination from Compressed Air. Part 3 of 6

What’s the Best Line of Defense against Microbial Contamination of Food? Part 6 of 6

 

 
 
Categories
Recent Posts by Author

How Oil Vapour in Ambient Air Affects Compressed Air Quality

Many companies, including those in the food and beverage, pharmaceutical, cosmetics, manufacturing and electronics industries, recognize the negative effects on quality created by oil contact with...

How to Distinguish a Process Water Cooler from a Chiller

There are numerous manufacturers in the water cooler market. Water coolers are also called chillers but it is important to draw a clear distinction between process water coolers and chillers...

Why Are Coalescing Filters Installed in Pairs?

In an industrial manufacturing plant, coalescing filters are probably the most important piece of purification equipment found in a compressed air system. They treat six of the ten main contaminants...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Important Reasons to Filter Culinary Steam


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha