The trucking industry is experiencing tremendous growth. According to the U.S. Bureau of Labor Statistics, the demand for diesel service technicians and mechanics is projected to grow by 12 percent from 2014 to 2024, faster than the average for all occupations. The demand has accelerated based on a variety of conditions, including a growing economy and increased vehicle complexity.
The future of trucking is here
Trucks are quickly transforming into rolling data centers that track everything from emissions to blind zone obstacles, to tire inflation and more. As a direct result, the skill requirements of technicians and mechanics are changing.
Efficient use of your skilled service team is key. One way to increase productivity and make the best use of your service team’s skills is to simplify the processes that are time consuming and routine, such as fleet vehicle oil changes.
Never change oil the same again
Parker’s QuickFit™ Oil Change System provides a path forward for better standardization of oil changes with a more efficient, cleaner and safer process. Whether a veteran mechanic or first-day-on-the-job technician, there’s only minimum training needed to perform an oil change using the QuickFit System. Only three easy steps will complete the process to purge, evacuate and refill oil. This is achieved through a single connection point that allows used oil to drain directly to the waste containment, and then apply a vacuum to extract the used oil from the filter. Finally, the same connection point is used to refill the system with new oil.
Step 1 – Purge Filter
Employs compressed air to purge the oil by pushing it through the filter into the engine sump.
Step 2 – Evac Oil
Oil is drained directly to waste containment, allowing for clean removal of the filter.
Step 3 – Refill Oil
New oil is pumped into the engine using the same connection point.
“Reducing the number of steps in the process eliminates any risk of safety hazards or spills, which creates less consumable waste and is more environmentally friendly. The QuickFit System three-step process helps to lower operating costs, increase profitability and reduce oil change times by about 50%.”
Mario Calvo, division marketing manager, Parker Quick Coupling Division
QuickFit features an ergonomic design that allows for easier access to even the most cramped and isolated engine compartments. This greatly reduces exposure to fluids and lowers the possibility of slips, falls and burns. Plus, oil changes can be completed from start to finish in less than 30 minutes.
The QuickFit system provides a solution that is incredibly easy to use. Maintenance becomes simple, productivity goes up, the risk of spills and contamination is virtually eliminated and it works for engines and machinery across multiple applications.
The future is bright for the trucking industry
The future is bright for the trucking industry, as the demand for experienced technicians and mechanics has never been higher. To properly maintain vehicles, fleet service centers must invest in the latest tooling, equipment and software to keep up with the rapid pace of technology and change. The QuickFit Oil Change System greatly simplifies a crucial aspect of fleet maintenance by allowing technicians and mechanics to change oil in a matter of minutes and focus more time on other key components of equipment maintenance and repair. Simplifying this one process will increase efficiency to allow better use of your highly valued service team.
Ready to get started or have questions? Locate the Parker Distributor near you.
Learn more about Parker's QuickFit™ Oil Change System.
Contributed by Matt Walley, product sales manager, Quick Coupling Division, Parker Hannifin
Related, helpful content for you:
How to Change Your Engine and Machine Oil Faster, Cleaner and Safer
3 Easy Steps to Configure a Wetline Kit for Your Work Truck
Smart Work Truck: The Role of IoT in Building Smarter Work Solutions
Reduce Failure of Hydraulic Systems with Preventive Maintenance
Have a question about Parker products or services? We can help: Contact Us!
Comments for Improve the Efficiency of Your Fleet Service Team
Please note that, in an effort to combat spam, comments with hyperlinks will not be published.