Electromechanical

Improve Your Machine Performance by Controlling Vibration

Improve Your Machine Performance by Controlling Vibration- PSD Servo Drive Range - Parker Electromechanical and Drives Division

Engineers working in industries that use fast-running machinery will almost certainly be familiar with the demands for ever-greater productivity to increase competitiveness and reduce costs. We have seen numerous situations where a thousand cycles per minute appears to be the norm - particularly in packaging applications. Unfortunately, cycle rates such as these cannot be reached using traditional methods.

In many cases, the power of servo motors can reach maximum levels, offering high dynamic speed and power to do the job. Fast cycle times require ultra-fast changes of position set values, which unfortunately may stimulate mechanical resonances in a machine, leading to losses in quality. For this reason, automation experts are looking into more ‘intelligent’ options to give the opportunity to increase speed and save time.

The most common initial reaction is to think about the control loops of existing drives, but without measuring the behaviour of the fluid being transported, it is difficult to implement. Moreover, the cost of the necessary system sensor(s) can be prohibitive.

Improve Your Machine Performance by Controlling Vibration - PSD Vibration Screen Capture - Electromechanical Division Europe-Automation Group-Parker Hannifin Corporation

Therefore, designers may consider generating an optimised profile. The drawback with this approach however, is that you then create a dedicated system. Any change of movement, even slight alterations in speed or position, will require a new profile. In modern production situations, we would expect a method that is flexible and somewhat more adaptable to production changes.

Our PSD series of servo drives offers the potential to provide a solution and has been designed to address some of industry’s most challenging applications.

One that is frequently seen is the need to move open containers filled with liquids as quickly as possible between positions A and B. The PSD series of servo drives can help avoid the stimulation of resonance altogether. In addition, in systems like these, effective vibration suppression can be the key to further process improvements.

If nothing is done, the liquid being moved is likely to spill from its container, especially if cycle rates are increased with the higher speed and the acceleration profile resulting in more turbulence of the liquid.

Effective vibration suppression will help allow increases in acceleration and also remove the frequencies responsible for the turbulence. This results in a motion profile with the same cycle rates as before but with really stable fluid during movement.

Depending on the application, different methods of controlling / suppressing vibration are available, each delivering the same impressive results in terms of stability, high dynamics and productivity.

We have worked successfully with manufacturers in a range of industries to control challenging applications; fluids is just one example. Outcomes have typically delivered faster machine cycle times due to reduced fluid settling time and through this, up to 20% greater productivity.

Learn more

Learn how using the latest drive technologies to suppress vibration can boost your packaging line or production system.

 

Improve Your Machine Performance by Controlling Vibration - Hermann Kamphues - Electromechanical Division Europe-Automation Group-Parker Hannifin Corporation

Article contributed by Hermann Kamphues, product manager drives, Electromechanical & Drives DivisionParker Hannifin Corporation.

 

 

 

 

Related content

What’s Trending in Industrial Automation?

How VFD Technology on Hydraulic Power Units Helps Improve Performance

Is Industry 4.0 Driving the Need for Smarter Motion Control Products?

3 Great Benefits of Using Decentralized Servo Drives

 

Categories
Recent Posts by Author

Practical Applications for Precision Electromechanics in Photonics

In a world of constant technological advances, the photonics industry is seeing rapid growth with no signs of a slow-down. Photonics is the branch of technology concerned with the properties and...

Improve Safety and Air Quality in Europe’s Largest Underground Car Park

The renewal of the entire ventilation system in the underground car park serving the largest European business district, was not limited to the simple replacement of filters and some...

Solutions for Reducing Noise on the Factory Floor

Maintaining a safe and productive work environment should be a top priority in any facility. More and more companies are putting programs in place to improve the working environment and...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Improve Your Machine Performance by Controlling Vibration


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha