Filtration

Improving Power Plant Gas Turbine Performance in Harsh Desert Environments

Improving Power Plant Gas Turbine Performance in Harsh Desert Environments - Desert image with fog and dust - Parker Gas Turbine Filtration DivisionGas turbine performance is affected by the environmental challenges of a specific power plant installation. In a recent project located in the Middle East, a filtration solution to protect the turbine needed to be designed to address each of the conditions faced, including varying amounts of: 

  • Dust
  • Salt
  • Moisture
  • Other contaminants 

The spectrum of potential hazards that could be faced at a turbine installation means one filter cannot meet all needs. Even the different forms of dust or moisture present need to be considered within the design of the filter house.

 

A brutal environment for gas turbines

In the Middle East, a mixture of sandstorms, heat, mist and moisture from random fog events, make for a brutal environment for a gas turbine. It is the combination of the moisture in thick fog combined with high dust concentrations that can be particularly challenging for a gas turbine filter system.

Without the correct design and implementation of a system, the installation is at risk of sudden pressure increases, gas turbine shutdowns, difficult and time-consuming maintenance and greatly shortened filter life. Indeed, as one operator was experiencing, it is not uncommon for pre-filters to require changing every two or three days and final filters to need replacement after just six or seven months, as opposed to a normal life expectancy of over two years. The increased labour and ongoing cost to keep operations running and reduced availability of the gas turbine were having a serious impact on the operation’s bottom line.

The gas turbine installation in question was at a power plant in a coastal, desert location in the Middle East. Seasonal fog events and extremely high levels of dust were causing havoc with the system. After careful review of the installation and specific environmental conditions, however, relatively simple changes led to a dramatic improvement in performance.

 

When to pulse – and when not to

One of the first areas to be considered was the pulse system settings. A pulse system removes dust build-up on the filter and tends to operate in one of two ways. In the first, it can be set to run continuously without regard for the differential pressure.

Alternatively, however, it can be configured to run when the differential pressure across the filter reaches a certain level. Once this level is seen, the pulse system turns on, cleans the filters and then turns off when a low differential pressure setpoint is met.

The site’s pulse system was set to run continuously. The issue this created, however, was that the fine dust in the area was leaving the filters in a dust cloud and simply becoming re-entrained on the filter. The system was changed to operate only when differential pressure reached a pre-set trigger level. The switching levels were established based on testing with the local environmental conditions and found to be optimized with the system turning on at 1.5” wg (water gauge) and off at 1.0” wg. This meant the filters were cleaned before pressure became an issue but not before a dust cake built up on them that enabled gravity to help the dust move down the filter house. Typical set points for pulse cleaning start around 3.0” wg and stop at 2.5 or 2.0” wg.

 

Handling the moisture from the fog

Improving Power Plant Gas Turbine Performance in Harsh Desert Environments - clearcurrent TS1000 filter - Parker Gas Turbine Filtration Division

The next area to be considered were the coalescers, which were experiencing serious issues. Coalescers are used to remove moisture from the air flow prior to it reaching the filter. If there is a lot of moisture in the air flow when it reaches the filtration stages, small moisture droplets combine with the dust and sand to create blockages and sudden increases in differential pressure. The size of these droplets means they can also work their way into the matrix of the filter media and get stuck. Coalescers usually work to prevent this from happening by combining small moisture droplets to form bigger, heavier ones — many of which will then naturally fall out of the airflow.

The site in question had traditional coalescers installed, known as mat coalescers, which employ media similar to that used in dust filtration. The issue with these, however, was that the high volumes of dust were quickly clogging them and, with no path for the inlet air flow, they were being forced out of place. Once the air was able to completely bypass the coalescers, the moist air and dust were continuing to the filter and creating blockages. Placing the coalescing technology with a modern, fully washable, 100% synthetic mesh resolved this issue and, even after 12 months of operation, the coalescers remain firmly in place and doing the task for which they are installed.

Improving Power Plant Gas Turbine Performance in Harsh Desert Environments - close up of filter mesh for clearcurrent media.Unlike the traditional mat equivalents, the new synthetic media coalescers had been specifically designed to allow the sand and dust to pass through. The new units work by using a two-stage coalescence configuration. The first stage is a moisture separator with coalescing efficiency down to 50 microns. The second stage, a clearcurrent TS1000 coalescer, has 99 percent coalescing efficiency for droplets down to 10 microns but which has limited dust removal capability. It is this deliberate limitation of dust removal capability which avoids blockages and significantly reduces the maintenance overheads where high levels of both dust and moisture are present. The dry dust is then easily handled by the filtration system, to prevent it from damaging the turbine.

 

Two simple changes equal huge improvements in performance

Following these two changes on site, pulse system settings and coalescer technology employed, the site has experienced no shutdowns because of problems with the filter system or sudden differential pressure increases. The self-cleaning filter life is exceeding the customer requirement of two years and maintenance intervals have been extended. This has reduced operating costs, limited manual labour interventions required, and increased production availability — significantly improving operating profits.

In regions where extreme conditions as found, such as in the Middle East, operators are advised to:

  • Start the difficult season with new, clean filters.
  • Evaluate all filtration options and new technologies available, as these may offer a major upgrade to existing technology and save a great deal of time and money.
  • Proactively plan outages to be in the best position to survive seasonal, tough environmental conditions.

 

Success is not about paper specifications

Measurement of the success of a filtration solution cannot be measured by specification comparisons or laboratory testing, as these do not portray the real-world conditions of each installation. Instead, success criteria need to be based on critical factors such as the reduction in turbine downtime and outages for filter replacements.

The example given above shows that, with the correct experience and expertise, significant improvements to turbine performance can be gained with even relatively small solutions and adjustments. System design and settings need to be geared towards the real-world environment in which the solution is installed. Working with filtration experts, other turbine operators can benefit from evaluating total solution management of their inlet systems.

 

View the presentation given at Middle East Rotating Machinery Technology and Innovation Conference & Showcase (ROTIC) 2018

 

Attending the 2019 PowerGen International show?

Visit Booth #3119 at POWERGEN International 2019 to see how Parker offers the most comprehensive product and system solutions for today’s power generation environments. Learn more about our filtration products, sealing and shielding, sensors and diagnostics, heated enclosure system, combustion turbine and energy storage solutions.

 

About Parker Gas Turbine Filtration

With more than 50 years of experience delivering innovative solutions for gas turbine inlet filtration and monitoring fleet-wide performance data, our industry and applications experts will select the appropriate filter for your site designed to meet your specific operating goals.

Parker Gas Turbine Filtration supplies a full range of inlet systems and filters engineered to meet your operating goals, including:

  • Higher power output.
  • Lower operating costs.
  • Proven performance utilizing advanced filter technology.
  • Extended gas turbine availability.
  • Maximum protection against corrosion and fouling.
  • Easy maintenance and change out.

Through our Parker brands, altair® and clearcurrent®, we are the choice for advanced filtration for new units and replacement filters. Our inlet system designs include self-cleaning (pulse) and static inlet systems for all gas turbine OEMs. We supply a full range of filter types at all efficiency levels. The predictable and reliable performance of our air filters significantly reduces compressor contamination and the need for unplanned maintenance for gas turbines in power plant applications.

 

Improving Power Plant Gas Turbine Performance in Harsh Desert Environments - David Trisante - Parker Hannifin Gas Turbine DivisionThis article contributed by David Trisante and Dan Burch.

David Trisante is sales director at Parker Hannifin Gas Turbine Filtration division. Trisante earned his engineering degree in the prestigious Universitat Politecnica de Catalunya (Spain) and the Aalborg Univeritet i Esbjerg (Denmark). He holds more than 20 years’ experience in purification and air pollution control markets as well as in a variety of filtration equipment ranging from dust collectors, electrostatic precipitators or gas turbine air intake systems.

 

Improving Power Plant Gas Turbine Performance in Harsh Desert Environments - Dan Burch - Parker Hannifin Gas Turbine Filtration Division

Dan Burch is pricing manager, Gas Turbine Filtration (GTF) Division, Parker Hannifin. He’s covered all aspects of the company’s filtration offerings, with a particular focus on developing marketing and pricing strategies for gas turbine inlet filtration products. He has 15 years of experience in marketing and journalism roles. Dan has a B.A. in journalism from Indiana University and an MBA in marketing from the University of Missouri-Kansas City (UMKC).

 

 

This article originally published in Power Engineering in January 2019

The case study and paper were presented as part of the Middle East Rotary Machinery Technology 2018 conference.

 

Related content

Why Are Coalescing Filters Installed in Pairs?

Condition Monitoring Solutions for Power Generation Plants

What You Need to Know About Coalescing Filtration

Hydraulic Power Units Control All Functions of Hydro-electric Turbine

Categories
Recent Posts by Author

Air Collection System Improves Air Quality at Metal Fabrication Plant

Many metalworking facilities feature large, open workspaces. While ideal for large scale production, this setting presents challenges for air quality and in assuring clean air in the work environment....

Clean Air Makes Boston Hotel a Friendly Neighbor

The Four Seasons Boston Hotel is located in a 13-story structure situated in the heart of historic Boston, Massachusetts. This prestigious hotel group dedicates itself to the highest quality...

SmogHog Eliminates Kitchen Emissions at Sandia Resort and Casino

The Sandia Resort and Casino opened to great anticipation. The Indian gaming operation’s new property in Albuquerque, New Mexico featured multiple dining options, a huge casino and over 200 sleeping...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Improving Power Plant Gas Turbine Performance in Harsh Desert Environments


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha