Hydraulic Filtration

Industrial Machine Vibration Analysis and Condition Monitoring

Industrial Vibration Analysis and Condition Monitoring - industrial pumps and motors Parker Kittiwake A condition monitoring system is concerned with the early detection of failure. Vibration monitoring systems, whether they use traditional techniques based on displacement or acoustic emission sensor techniques, form part of your condition monitoring (CM) tool chest. 

Machinery vibration analysis equipment is part of a machine monitoring system that aims to provide months of warning of developing issues before they become bigger problems. This can save your company from serious disruption by avoiding unnecessary downtime and delays. There is also the potential for both on and offline implementation of these systems, subject to capability and level of available technology for the techniques, which makes them perfect for the food and beverage, power generation, marine and offshore industries. 

If you are interested in learning about our vibration analysis or monitoring systems and equipment, please contact us today to speak to one of our engineers.


Vibration monitoring techniques

Vibration monitoring equipment uses techniques based on the use of accelerometers, which are well known in the field of CM, and can be classified into three main categories:

VM Vibration Monitoring (ISO 10816): Perfect for maintenance engineers, vibration monitoring ISO 10816 offers an instinctive understanding that a machine is vibrating unusually from the non-rotating parts. Great for small machines, electric motors and pumps and production motors.

VA Vibration Analysis (ISO 13373): A mainstream CM option and essential addition to any other technique used, vibration analysis offers a more sophisticated improvement in signal to noise ratio for repetitive defect signals. This highlights what is internally causing the vibration.

AE Acoustic Emissions (ISO 22096): This technique looks for high-frequency signals from cracks or impact rather than a repetitive movement from vibration. As a passive technique, acoustic emissions can diagnose incipient machinery prior to undertaking a lengthy diagnosis. Highly effective in detecting the very early onset of machinery fault conditions where needed most.
 

Acoustic emission machinery

There are many approaches which fall under the umbrella term condition monitoring, each with its own features and areas of excellence. These include machinery vibration monitoring and analysis, and also acoustic emission analysis systems. 
 

Industrial Machine Vibration Analysis and Condition Monitoring - Relative Inputs into CM Assessment

Techniques in BLUE = Technologies available from Parker Kittiwake


Parker Kittiwake focuses on techniques such as an acoustic emission system that provides for the greatest protection or longest period of warning for potential damage and eventual failure. While machine vibration monitoring systems can help prevent the worst cases of damage. 

The use of two (or more) appropriate technologies can provide a more complete picture of the likely failure mechanism, thus offering you reduced machinery downtime and more efficient recovery. The table below identifies the variations of expertise that different condition monitoring options cover.
 

Industrial Machine Vibration Analysis - comparison of the main machinery CM techniques - Parker Kittiwake

 

CM machinery techniques that are available from Parker Kittiwake:

Industrial Machine Vibration Analysis - Condition Monitoring machinery techniques - Parker Kittiwake


Industrial Vibration Analysis and Condition Monitoring - Contact Us - Parker Kittiwake If you are interested in any of the above vibration analysis products and services, or you would like to speak to an engineer about which vibration monitoring option would best suit your needs, please contact us today.

 

Article contributed by the Hydraulic Filtration Team, Parker Kittiwake, part of Parker's Hydraulic and Industrial Process Filtration Division.

 

Additional resources

Bunker Quality: Why Changes to ISO 8217 Increase the Need for Condition Monitoring

What You Need to Know About Testing Your Hydraulic System for Particle Contamination

Reduce Failure of Hydraulic Systems with Preventive Maintenance

Reliability Centered Maintenance Reduces Costly Downtime in Oil & Gas Applications

 

Categories
Recent Posts by Author

How to Perform a Cold Corrosion Test for Cylinder Oil

The oil used to lubricate the cylinders of large 2-stroke marine diesel engines has to contend with high temperatures and acidic products formed during the combustion of sulphur-rich bunker...

Industrial Machine Vibration Analysis and Condition Monitoring

A condition monitoring system is concerned with the early detection of failure. Vibration monitoring systems, whether they use traditional techniques based on displacement or acoustic emission sensor...

Fuel Monitoring Matters

Whether you choose distillates, liquefied natural gas (LNG) or scrubbers to meet the new International Maritime Organization (IMO) fuel regulations in 2020, it will be even more critical to regularly...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Industrial Machine Vibration Analysis and Condition Monitoring


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha