Electromechanical

Is Industry 4.0 Driving the Need for Smarter Motion Control Products?

Is Industry 4.0 driving the need for smarter motion control products-Parker automation controller in use-Electromechanical Div EuropeThe collective term Industry 4.0 refers to the fourth industrial revolution, typically described as the computerization of manufacturing—or in other words, the merging of traditional automation with information technology.

One of the underlying concepts is modular cyber-physical systems that can collaborate with the operator and communicate between themselves in real-time to make autonomous decisions, thereby adapting production processes as needed.

When machine builders select their motion control equipment to design the machines of tomorrow, there are several things to consider.

Logic control is not enough anymore

Not so many years ago, machines were controlled by a programmable logic controller (PLC), which processed discrete input and output signals and followed sequential programs. Servo drives would typically be coordinated by a separate motion controller connected to the PLC via fieldbus. Now digital manufacturing requires a machine controller capable of executing much more complex tasks in parallel.

Consequently, that requirement led to the development of programmable automation controllers (PAC). The modern PAC platform is an enabling technology that allows customers to prepare production equipment for Industry 4.0. This single hardware platform incorporates logic and process control, motion control, visualization, high-level programming languages and software development tools that cut across different disciplines to eliminate interface issues and facilitate modular design principles. 

Tip: When you're selecting a next generation control platform, mitigate risk by looking for compliance with industry standards like IEC61131-3 and PLCopen.

Connectivity is key

To meet the need for higher flexibility and to maximise overall equipment effectiveness, production processes need to automatically adjust to changing demand, which requires intelligent devices talking to each other in real-time and a controller platform that acts as a central hub to enable seamless bi-directional communication from the enterprise network down to the individual actuator.

To avoid future bottlenecks, select intelligent field devices that support industrial Ethernet protocols to communicate to the control system. Programmable control systems with integrated web-publishing can help publish data virtually anywhere and facilitate remote maintenance if required.

Is Industry 4.0 driving the need for smarter motion control products-Parker automation controller system integration-Electromechanical Div Europe

Impact on electrical control panel design

The trend towards smaller batch sizes and mass customisation has led to an increased use of servo drives, as self-adjusting manufacturing processes require precise position control. However, increasing the number of servo drives requires electrical control cabinets to become larger, which may compound installation problems.

The solution here is found with servo drive systems, with a central power supply module that helps to reduce the number of external components. Modern multi-axis systems also come with stackable double and triple axis modules that can help to dramatically reduce the size of control panels. Additionally, single cable servo motors can help to cut cabling costs by half, as they integrate position feedback signals into the motor power cable. 

Before developing a next generation machine, discover how the new EtherCAT-based PAC controller and PSD servo drives from Parker can help customers boost machine performance while reducing development time, installation and operating costs.

Find out more about our programmable automation controller and servo drive systems.

See more products from the Parker Electromechanical Division.

 

 

Is Industry 4.0 driving the need for smarter motion control products-Frank Durban-Electromechanical Div Europe

This article contributed by Frank Durban, division marketing manager, Electromechanical & Drives Division Europe, Parker Hannifin Corporation.

 

 

 

Related content:

Electromechanical Technologies and Key Markets 

What’s Trending in Industrial Automation?

Intelligent Pneumatic Solution Improves Automotive EMC Testing | Case Study

Categories
Recent Posts by Author

Electromechanical and Drives Technology - A Look Back on 2019

Thanks to our loyal followers for all of the interest in the topics covered in this blog over the past year. In examining the most-read blog posts over the course of 2019, it becomes obvious that...

Time-Saving Solution for Servo Presses and Joining Applications

In industry, time is money. So, for engineers who are time-pressured, there is a solution for electromechanical press and joining applications. Push-To-Fit is an innovative electromechanical solution...

High-load Rodless Actuators Powering the Factory Automation Revolution

The arguments advocating more automation in our factories and process plants are gaining momentum and translating into a revolution in production environments.  Parker designs automated linear motion...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Is Industry 4.0 Driving the Need for Smarter Motion Control Products?

Sami REKIK
Dear Sir,
I'm a hydraulics and pneumatics trainer from Tunisia, and I would like to have deeper knowledge about your devices dealing with industry 4.0 and why not have a training in this field.

Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha