Gas Generation

Is Noise Pollution in the Laboratory a Health Risk?

Lab Technician Parker Hannifin Noise pollution in the laboratory, as in any workplace, is a serious health concern. That’s according to the US Occupational Health and Safety Administration (OSHA) whose role it is to enforce the Occupational Noise Exposure Standard (29 CFR 1910.5). Among other requirements, the standard calls for employers to implement a hearing conservation program for workers exposed to a time weighted average noise level of 85 decibels (dBA) or above over an eight-hour work period. The peak permissible exposure level is 90 dBA so for example, a worker may only be exposed to a 95 dBA of noise for four hours over a work period. The National Institute for Occupational Safety and Health (NIOSH) recommends an eight-hour weighted average exposure limit of 85 dBA.

Note: dB and dBA are abbreviations that stand for a decibel, the unit of measure for gauging how loud sound is. It is a logarithmic ratio of the observed level compared to a standard. To see how loud some common everyday sounds are as measured in decibels, refer to Table 1.  From looking at these examples it is clear that reaching a non-compliant noise level might happen easily if lab managers are not careful.

Table 1 Typical Noise Levels

Telephone dial tone 80 dB
City traffic (inside car) 85 dB
Train whistle at 500', truck traffic 90 dB
Jackhammer at 50' 95 dB
Subway train at 200' 95 dB
Level at which sustained exposure may result in hearing loss 90-95 dB
Hand drill 98 dB
Power mower at 3' 107 dB
Snowmobile, motorcycle 100 dB
Power saw at 3' 110 dB
Sandblasting, loud rock concert 115 dB

 

The Health Risks

Compliance with regulations, of course, is not the only reason lab managers should be concerned about noise. The main reason is that excessive noise is harmful. As far back as 1978, then U.S. Surgeon General William H. Stewart said that:

“Calling noise a nuisance is like calling smog an inconvenience. Noise must be considered a hazard to the health of people everywhere.”

A number of studies have shown that there are significant health effects from even moderately high noise levels during a single eight-hour shift.  Noise-induced hearing loss is an obvious one but others include increased incidence of coronary artery disease, vasoconstriction or narrowing of the arteries, and a statistical rise in blood pressure of five to 10 points as well as an increase in stress.

One of the problems with controlling noise levels in the laboratory is that there are many diverse sources of noise such as fume hoods, automated analyzers, or tissue homogenizers; and their effects are cumulative. For example, two instruments operating at 52 dB produce a noise level of 58 dB.  Adding a third instrument operating at 58 dB yields a noise level of 62.5 dB. In the workplace a level more than 55 dB(A) is generally considered noise pollution. Also, about 35 to 40 percent of workers in office settings find levels 55-60 dB irritating.

Clearly, noise pollution is an issue lab managers might overlook, given how “easy” it is to let happen. However, they need to manage it if they are to provide a healthy, safe, stress-free and compliant environment. 

Noise Pollution in the Laboratory White Paper ImageRead White Paper for additional information on Noise Pollution in the Laboratory.

 

 

 

 

This is the first of a three part series on Noise Pollution in the Laboratory.

Why You Should Audit Laboratory Noise Sources - Part 2 of 3

A Quieter Approach to Equipment Design - Part 3 of 3

Peter Froehlich, PhD., was contracted by Parker to author the series and white paper. He was assisted by Kim Myers, Product Manager, Parker Hannifin.

Categories
Recent Posts by Author

Nitrogen Generation System Reduces Costs in Additive Manufacturing

Additive manufacturing or 3D printing is a relatively new rapid manufacturing technology that has become mainstream in recent years. It covers a wide variety of processes used to produce a multitude...

Energy-Saving Nitrogen Generator Prevents Gas Supply Disruptions

When it comes to supplying dry, inert nitrogen for manufacturing applications, there’s a lot more to PSA technology (pressure swing adsorption) nitrogen generators than vessels filled with CMS (carbon...

A Safety Plan for Compressed Gases in the Laboratory

Using compressed gases in the laboratory can be a dangerous situation if they are handled improperly. Many gases can be explosive, flammable, corrosive, and toxic. Because the gases are under high...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Is Noise Pollution in the Laboratory a Health Risk?


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha