Gas Generation

Is Your Laboratory Lean?

Is your laboratory Lean - Laboratory Worker - Parker Hannifin Gas Generation Depending on how your laboratory interfaces with the manufacturing world, you may or may not have heard of “lean.” Originating in Japan decades ago, “lean management” is an ongoing, holistic approach to workflow management that eliminates waste and unnecessary steps in the workflow process. The elimination of waste speeds up production, improves quality, reduces mistakes, and lowers overall costs. Lean principles have been used for decades in manufacturing operations around the world, especially the automotive industry. If implemented correctly, lean can become a vital part of the corporate culture and can transform a company’s profitability and productivity.

Although revered in the manufacturing world, lean is less well-known among non-manufacturing industries. Lean can benefit any industry or business. After all, workflow is workflow, whether it is a manufacturing operation, a testing lab, or a headquarters on the thirtieth floor. An example of a non-manufacturing industry that has embraced lean is health care, which has become highly focused on improving quality of care and reducing costs by identifying and eliminating waste.

Value stream mapping

The goal of lean is to remove waste from any work process (and just about every process contains waste).

Value stream mapping is one of the most effective lean tools that can be implemented easily. This is a highly visual, pencil-and-paper exercise that maps out, on a single piece of paper, a "current state map" which consists of every step in a process or operation. This is generally an eye-opening exercise, even for those who are highly experienced in the process being mapped. Once the map (essentially a flow chart) is completed, the “bottlenecks” and non-value-added steps are identified. Participants brainstorm the best ways to eliminate these wasteful steps to better utilize time, talent, and equipment. Sometimes a solution is as simple as re-arranging work stations for better work flow.

For a laboratory, the value stream map will show a stream coming in from the side that consists of the steps that comprise the acquisition of high purity gases such as hydrogen, nitrogen, and zero air which are commonly used for a broad range of instrumental methods including Gas Chromatography (GC) with Flame Ionization Detector (FID), Liquid Chromatography-Mass Spectrometry (LCMS), and Fourier Transform Infrared Spectroscopy (FTIR). The steps involved in the process include placing the order, receiving the order, storing the tanks, and transporting tanks to and from the laboratory as needed.

Factors that affect the gas acquisition process that don’t show up in the value stream map include possible delivery delays, unplanned downtime due to running out of gas, inflexible delivery schedules, accidents with the tanks, and the extra administrative costs of dealing with vendors and contracts. These inconveniences can create extra steps in the value stream process. The bottom line is that more steps result in added complexity and risk, which translates into higher costs.  

Is your laboratory Lean? - Parker domnick hunter Hydrogen Generator - Parker HannifinThe entire gas-delivery arm of the value stream map can be eliminated by installing an in-house gas generator that can be connected directly to the instrument to provide the necessary gas at the pressure and flow required by the application on a continuous basis with minimum user interaction. Parker offers a variety of gas generators including hydrogen generators, nitrogen generators, zero air generators, and FT-IR purge gas generators.

Getting lean

The final step of value stream mapping is implementing the process improvements the team has identified. Even small changes can bring big results that improve efficiency, productivity, and worker satisfaction. It is critical for management to commit the necessary resources to make these changes happen, including capital improvements such as an in-house gas generator. The cost of purchasing and operating a gas generator is attractive when compared to the use of high pressure cylinders. The payback period is usually calculated at less than one year depending on the specific usage and required purity.  Most importantly, the cost to operate and maintain an in-house gas generator is very low, when compared to the cost of ordering, transporting, storing, and handling high pressure gas cylinders. 

Installing an in-house gas generator is one of the best ways to start the lean transformation of an analytical laboratory. It eliminates the extra steps and costs that are associated with gas tanks.

Watch this video to learn more about in-house laboratory gas generators:

Once it becomes part of the company culture, lean never ends; in fact, a process must go through multiple periods of value stream mapping before it is really considered lean. To learn more about lean, visit the Lean Enterprise Institute at http://www.lean.org/

 

Attending Pittcon 2020?

Pittcon LogoVisit Parker at Pittcon March 1 - 5 in Chicago, IL 2020, booth 2311, and see our range of on-site gas generators for Gas Chromatography and Mass Spectrometry instruments. 

 

Related posts:

In-House Gas Generation Is Ideal for LC-MS

Why Nitrogen Is Better than Helium for Gas Chromatography

 

This post was contributed by the Gas Generation Technology Blog Team, Parker Hannifin.

 

Categories
Recent Posts by Author

Is Your Laboratory Lean?

Depending on how your laboratory interfaces with the manufacturing world, you may or may not have heard of “lean.” Originating in Japan decades ago, “lean management” is an ongoing, holistic approach...

Nitro Iced Coffee Uses Self-Contained Nitrogen Generators | Case Study

Battle Grounds Coffee is a small, community-oriented coffee shop in Haverhill, MA. The owners were challenged to find a more efficient and consistent way to deliver Nitro Coffee to their customers.  ...

How to Prevent Contamination & Corrosion in Demineralized Water Storage Tanks

Power generation plants rely heavily on demineralized and deionized water to maintain required levels of water purity during process operations. Managing the water supply is critical under...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Is Your Laboratory Lean?


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha