Pneumatics

Know Your Pneumatics: 3 Ways to Increase Your ROI from Rotary Actuators

Know Your Pneumatics: 3 Ways to Increase Your ROI from Rotary Actuators - Rotary Actuator Stroke Adjustment-Pneumatic Division Europe - Automation Group - Parker Hannifin CorporationDid you know that pneumatic rotary actuators are a durable and simple way to convert compressed air pressure in rotary movement? Capable of operating in hazardous environments and when utilized to their full potential, rotary actuators deliver a high force for their size. Here, we outline three ways to ensure you are magnifying the return on investment from your rotary actuators.

 

1. Let the rotary actuator carry the load.

Many engineers don’t realize that due to their integrated bearings, rotary actuators can adequately support a working load, this means engineers may not need to include additional bearings into their mechanical design. This is especially true of rack and pinion actuators which utilize large bearings.

 

2. Size for stopping the load not starting the load.

A key point to understand is that rotary actuators should typically be sized based on their ability to stop a load rather than their ability to move the load. That’s because the kinetic energy of a rotating mass is exponential as the load moves further away from the rotation point. A component of the equation for mass moment of inertia is k2, meaning that the load gets exponentially worse the farther away it is from the shaft.

Know Your Pneumatics: 3 Ways to Increase Your ROI from Rotary Actuators - Load Stopping Diagram - Pneumatic Division Europe - Automation Group - Parker Hannifin Corporation

For example, let’s say a 2-inch/50mm vane rotary actuator at 100 psi/6 bar has an output rating of 65 lb-in/7.4Nm of torque. In a typical application, this little actuator is easily able to get the load moving over 270° quickly. However, stopping the load via the internal vane against the stator is an instant stop, very much like a hammer to a hard surface. Further, be conscious of over-center loads where gravity can greatly add to the rotational velocity.

Imagine a small child pushing an adult on a playground swing; the child has the ability to start moving an adult in a full swing, but it would take many large adults to stop the swinging person in a short distance. Similarly, once the actuator gets to the end of the stroke, we must consider the kinetic energy absorption ability of the actuator.

In high speed and load applications, the critical specification is not torque output but rather the kinetic energy rating. It is common to learn that the application requires a larger actuator because the larger unit will have more capacity to stop a load. If the designer sizes the actuator based on torque output alone—on starting the load—then external stops will likely be required to stop the load. Basic rule: Consider both the demand torque and the kinetic energy absorption rating.

All manufacturers of rotary actuators provide torque output and kinetic energy absorption ratings. Some units have optional pneumatic cushions and internal hydraulic shock absorbers, which greatly enhance the stopping ability of the actuator.

 

3.  Use the available built-in stroke adjustment.

With many models, options are available to adjust the rotational angle of travel. Most manufacturers provide adjustable stops as an option providing an additional level of control over the application. This feature greatly simplifies set-up time.

For more help in maximizing the ROI on your application, see our range of E-tools including online calculators and online CAD library

 

Know Your Pneumatics: 3 Ways to Increase Your ROI from Rotary Actuators - Kevin Hill-Pneumatic Division Europe - Automation Group - Parker Hannifin CorporationArticle contributed by Kevin Hill, European product manager pneumatic actuators, Pneumatic Division Europe, Parker Hannifin Corporation.

 

 

 

 

Related content

Know Your Pneumatics: Rotary Actuator Basics

Know Your Pneumatics: Which Rotary Actuator should I choose?

Know Your Pneumatics: Selecting a Pneumatic Cylinder | Operating Environments

Know Your Pneumatics: 3 Ways to Adopt Advances in Pneumatic Valve Technology

Know Your Pneumatics: Rodless Linear Actuators with Integrated Valves - 5 Advantages

Know Your Pneumatics: Safety & Understanding Rod Locking Cylinders 

 

Categories
Recent Posts by Author

The Fundamentals of IO-Link

IO-Link is a point-to-point communication technology that can be implemented into most PLC configurations or integrated into most existing industrial Ethernet networks via a device called IO-Link...

Central Tire Inflation System for Off-highway Vehicles

Parker's Central Tire Inflation System (CTIS) offers improved mobility when operating vehicles in severe off-road or soft soil conditions. Ideally suited for the agriculture and military markets, this...

What are the Challenges for Pneumatics in the Food Industry?

Starting from agriculture and food processing arriving at the packaging operation, automation is everywhere in the modern food plants and plays a fundamental role to address the required...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Know Your Pneumatics: 3 Ways to Increase Your ROI from Rotary Actuators


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha