Pneumatics

Know Your Pneumatics: How to Size a Pneumatic Rotary Actuator

Know Your Pneumatics: How to Size a Pneumatic Rotary Actuator-Rotary Actuator-Pneumatic Division Europe-Automation Group-Parker Hannifin CorporationOnce you have selected the type of pneumatic rotary actuator best suited for an application, the next step is to select an appropriate size. Here’s a breakdown of the three main design criteria to consider to help you along with the process:

  1. Torque output
  2. Kinetic energy absorption
  3. Bearing load capacity

Torque output

Check the data sheet or catalogue specifications for the torque output. Select a rotary actuator with enough muscle to move the load from resting to the desired speed. Typical torque units are expressed in pound-inches or Newton-meters.

Remember, there  will always be losses due to friction in the actuator. If theoretical output torques are provided, allow 10–15% for frictional losses for actual output torque. In rack and pinion rotary actuators this friction is caused by separation forces of the rack and pinion gears as well as seal friction. In vane actuators, seal friction exists, as well as a slight bypass leakage over the vane seals.

Many manufacturers do provide this information in their specifications, providing actual output torque values that have subtracted out the inefficiencies. For example, a rack and pinion actuator may be 90% efficient.  If actual output torque values are provided, the designer does not need to do the math… just be aware that the output specification factors in the frictional losses (efficiency).

Kinetic energy absorption

Next, look at the kinetic energy absorption rating. Typically, the designer finds that a larger actuator will be necessary in order to reliably stop the load. If the kinetic energy requirement drives a much larger unit, and it becomes more costly, then the designer may make the decision to specify a small rotary actuator and stop the load externally. It’s more design work, but when very high loads and moments are involved, it will usually be less costly to design external stops than to specify a much larger actuator.

Load handling

Finally, look at load on the output shaft. It will take some math to calculate the load of the application, which is greatly affected by the distance of the load from the shaft. Manufacturers provide tables for the capacity of load handling based on the bearings and gear trains. If there is a load handling requirement, especially a heavy load, size the rotary actuator based on its ability to hold the load. Again, this may require a larger actuator, as the bearing size is based on the size of the gear.

Learn more

For more help with sizing for your application, see our range of E-tools including online calculators and online CAD library.

 

Know Your Pneumatics: How to Size a Pneumatic Rotary Actuator-Kevin Hill-Pneumatic Division Europe-Automation Group-Parker Hannifin CorporationArticle contributed by Kevin Hill, European product manager pneumatic actuators, Pneumatic Division Europe, Parker Hannifin Corporation.

 

 

 

 

Related content

Know Your Pneumatics: Rotary Actuator Basics

Know Your Pneumatics: Which Rotary Actuator Should I Choose?

Know Your Pneumatics: Selecting a Pneumatic Cylinder | Operating Environments

Know Your Pneumatics: 3 Ways to Adopt Advances in Pneumatic Valve Technology

Know Your Pneumatics: Rodless Linear Actuators with Integrated Valves - 5 Advantages

Know Your Pneumatics: Safety & Understanding Rod Locking Cylinders 

 

 

Categories
Recent Posts by Author

Know Your Pneumatics: Basics of Rodless Cylinders

Pneumatics have always played an important role in achieving maximised productivity for manufacturing automation applications and the technology is constantly evolving to solve engineering challenges. ...

Three Things to Consider When Choosing a Smart Sensor

The latest generation of smart sensors for actuators are able to share information with the controller, typically via technologies such as IO-Link. They can also receive commands and...

How to Use Smart Sensors to Aid Predictive Maintenance Strategies

When optimally selected and applied, the latest generation of smart sensors can have a positive impact on predictive maintenance strategies for fluid power applications. Real-time data collection via...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Know Your Pneumatics: How to Size a Pneumatic Rotary Actuator


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha