Pneumatics

Know Your Pneumatics: Safety Exhaust Valves

Know Your Pneumatic: Safety Exhaust Valve_Pneumatic Division EuropeAny engineers who are involved in machine building as part of their core activities will know all about the EU Machinery Directive 2006/42/EC. Most will have stood in front of a newly built machine performing a risk assessment, trying to pick out potential danger points.

Of course, in identifying any safety risks, one must subsequently design them out or guard against them accordingly. Indeed, the Machinery Directive mandates the keeping of a technical file to show what risk avoidance was implemented to create a safer machine.

Although the directive does not mandate the use of safety-rated products, it clearly differentiates standard components used in a safety application from those built and intended as safety-rated products. The latter are classified separately and subjected to more rigorous requirements, testing and performance expectations.

The directive states that common sense strategies be employed on machinery, such as the use of e-stop buttons and the removal of air in pneumatically operated machines to protect from unexpected movement (where safe to do so). 

know your pneumatic: safety exhaust valves_P33T/D_Pneumatic DivisionSome manufacturers specialise in the development of safety-rated components for pneumatic applications. Here at Parker, for example, we have recently developed the P33 safety exhaust valve series, which meets the needs of the Machinery Directive to remove air from machines during either an e-stop or a faulted condition.

When incorporated into an air preparation system, a safety exhaust valve lets you safely and reliably shut-off the pneumatic energy, stopping the flow of compressed air to the machine and allowing downstream pressure to exhaust.

The P33 valve is designed for two-channel control architectures and is externally monitored. Moreover, the valve has a patented fail-safe design that is suitable for use in applications up to Cat 4 PL e. External monitoring gives greater control at the safety device for an application, a feature that also reduces machine complexity with regard to valve start-up or reset functions.

For those seeking further assurances, the P33 ticks all the major criteria associated with specifying a safety exhaust valve, namely: fast exhaust time to faulted condition; fast switching time; utilising series-parallel flow so that both valve elements (redundant design) shift to supply air downstream; high B10 value (life expectancy in switching cycles); and comprehensive monitoring capability to achieve the highest level of diagnostic coverage.

Installing a pneumatic safety exhaust valve, such as the P33, is a simple and cost-effective way to achieve machine safety and comply with the directive. After all, safety allows no room for error. Knowing that products exist which incorporate the needs of the directive and provide an enhanced level of certified safety, brings peace of mind to machinery designers and engineers responsible for enhanced and integrated safety - be safe, not sorry.

If you would like to find out more about Parker’s P33 series of safety exhaust valves and the benefits they can bring to your machine-building projects, please download and read the white paper Selecting & Integrating Pneumatic Safety Exhaust Valves

Learn more

Understanding the Machinery Directive – MSG_Linda Caron – Parker Hannifin Pneumatic Division North AmericaArticle contributed by Linda Caron, global product manager for Factory Automation, Pneumatic Division.

 

 

 

 

Related content

Understanding the Machinery Directive

How to Achieve Safe Motion Control in ATEX Environments

Know Your Pneumatics: Safety & Understanding Rod Locking Cylinders

 

 

 

 

Categories
Recent Posts by Author

Central Tire Inflation System for Off-highway Vehicles

Parker's Central Tire Inflation System (CTIS) offers improved mobility when operating vehicles in severe off-road or soft soil conditions. Ideally suited for the agriculture and military markets, this...

What are the Challenges for Pneumatics in the Food Industry?

Starting from agriculture and food processing arriving to the packaging operation, automation is everywhere in the modern food plants and plays a fundamental role to address the required...

What is End Position Cushioning in Rodless Cylinders and How To Adjust

In the world of industrial automation, pneumatic rodless cylinders can now be found just about anywhere; from food and beverage packaging to pharmaceutical and chemical production lines. They have a...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Know Your Pneumatics: Safety Exhaust Valves


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha