Pneumatics

Know Your Pneumatics: Safety & Understanding Rod Locking Cylinders

Know Your Pneumatics - Understanding Rod Locking Cylinders- P1F-L Rod Locking Pneumatic Cylinder-Pneumatic Division Europe-Parker Hannifin CorporationIn today's modern, fully automated manufacturing applications, assessing the potential risks to personnel is an essential part of overall system design. It’s vital to take appropriate measures in order to reduce the risk of injury to machinery operators or those in the vicinity, and prevent damage to the products being assembled or manufactured. During any kind of stop in operation, the equipment must be rendered safe; this is an installation prerequisite.

One of the most common causes of a stop in a process is an interruption to the power driving the system. Usually in industrial automation systems the method of power is electrical, hydraulic fluid or compressed air.

In pneumatic systems the removal of power is typically associated with a break or significant drop in the pressure of the air supply. Typically this can be caused by either the failure of a compressed air pump or other equipment, or by a major breach or leakage in the supply line.

Where the need for safety is deemed critical and "safe" failure is a necessity, one solution is the utilisation of rod locking cylinders.

How do rod locking cylinders deliver safety?

Rod locking pneumatic cylinders, such as Parker's P1F Series of ISO cylinders, have been designed to hold loads safely in position in a situation where the compressed air supply fails. The rod locking feature is a mechanical function provided by a cartridge through which the piston rod passes and is mounted transversally in the rod lock unit of the cylinder.

When an air failure occurs, causing a loss of signal pressure, the force from a set of internal springs pushes the mechanism to lock the piston using jaw clamps. It is important to note that these can only be used in dry piston rod applications as any grease, lubricants or coolants will reduce the effectiveness of locking. Parker's rod locking cylinders use air / spring activation with the mechanism fully integrated into the cylinder design, saving space and simplifying installation.

Parker supplies two basic variants of rod locking cylinders:

Both are able to hold the piston at any point in its stroke. The locking mechanism disengages when air pressure is re-established so that normal operation can resume.

Dynamic applications

Certain rod locking pneumatic cylinders may be used for dynamic applications where they can, within stated limits, be engaged when the rod is moving, acting as a brake.

Operation is achieved by the axial movement of a piston; with no signal pressure a number of high force springs force the piston to move axially. The movement is applied to the cylinder via the conically shaped inner ring of the piston. This is then converted into radial movement of clamping sleeves using hundreds of high precision steel balls, resulting in the hardened sleeves being pressed onto the piston rod with a high, stable holding force. 

The surface of the clamping sleeves that are applied to the piston rod have a special design with a pattern of grooves that provide maximum grip. This design feature improves the holding capabilities of the cylinder significantly – especially in applications where there is a risk that the piston rod will be exposed to oil, grease, dirt or other liquid and contaminants.

Static applications

Know Your Pneumatics - Understanding Rod Locking Cylinders-P1F-H Rod Locking Pneumatic Cylinder-Pneumatic Division Europe-Parker Hannifin CorporationIn static applications – where piston rod locking only takes place when there is no piston movement of the piston and no pressure signal – the rod lock unit is usually externally flange-mounted on the front end cover of the cylinder body.

The locking force is provided by the cartridge which is mounted transversally in the rod lock unit. The piston rod passes through the cartridge and when there is no signal pressure, the force from the internal springs pushes the over-the-center mechanism to lock the piston with the jaws clamping onto the piston rod and holding the cylinder firmly and safely in position.

In the case of the static rod locking cylinder, designers need to be aware that the sharp edge of the jaws will be damaged if the piston rod is not stationary before the rod lock unit is engaged.

Learn more

It is important to note that rod locking cylinders should not be used as the only safety component in an application; they are designed for emergency use. Other technologies should be used to achieve planned braking or holding.

Download a catalog to learn more about our P1F premier series of pneumatic cylinders, including our rod locking cylinders.

 

Know Your Pneumatics - Understanding Rod Locking Cylinders-Franck Roussillon EMEA Product Manager Automation Actuators-Pneumatic Division Europe-Parker Hannifin CorporationArticle contributed by Franck Roussillon, EMEA product manager -  Automation Actuators, Pneumatic Division Europe, Parker Hannifin Corporation.

 

 

 

 

Related content

Know Your Pneumatics: Selecting a Pneumatic Cylinder | Operating Environments

Know Your Pneumatics: Rodless Linear Actuators with Integrated Valves - 5 Advantages

Best Practices: Tube Line Clamping for Hydraulic, Pneumatic and Lubrication Systems

 

Categories
Recent Posts by Author

Central Tire Inflation System for Off-highway Vehicles

Parker's Central Tire Inflation System (CTIS) offers improved mobility when operating vehicles in severe off-road or soft soil conditions. Ideally suited for the agriculture and military markets, this...

What are the Challenges for Pneumatics in the Food Industry?

Starting from agriculture and food processing arriving to the packaging operation, automation is everywhere in the modern food plants and plays a fundamental role to address the required...

What is End Position Cushioning in Rodless Cylinders and How To Adjust

In the world of industrial automation, pneumatic rodless cylinders can now be found just about anywhere; from food and beverage packaging to pharmaceutical and chemical production lines. They have a...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Know Your Pneumatics: Safety & Understanding Rod Locking Cylinders


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha