Pneumatics

Know Your Pneumatics: Understanding IO-Link

Know Your Pneumatics - Understanding IO-Link-GettyImages171577309 Car Plant-Welding - Pneumatics Division Europe-Automation Group-Parker Hannifin CorporationIO-Link is a point-to-point communication technology that can be implemented into most PLC configurations or integrated into most existing industrial Ethernet and fieldbus networks via a device called an IO-Link master. It is the first standardized IO technology worldwide (IEC 61131-9) for point-to-point communication between sensors, actuators and control devices – comparable to an “industrial USB” and is the perfect local extension of a superior industrial Ethernet or fieldbus network.

There are multiple advantages for engineers when designing an IO-link architecture for their latest equipment. For example: when applying an IO-link connected Moduflex valve island, in addition to simplified and standardized wiring, they can also realize the benefits of remote configuration, monitoring, and increased data availability, leading to enhanced diagnostics. 

Utilizing IO-Link can also be especially beneficial for machine applications where there are frequent changeovers or reconfiguration as this time can be reduced, as can unplanned downtime.

Installing IO-Link

IO-Link doesn’t require any special or complicated wiring, which is a major benefit for adopting it as a communication method. Instead, IO-Link devices can be connected using standard 3-wire cables, the same you would use to connect a standard proximity switch.

Know Your Pneumatics - Understanding IO-Link - IO Link with Moduflex Valve Island - Pneumatics Division Europe-Automation Group-Parker Hannifin Corporation

If previously you were using 25-pin wiring for a pneumatic valve manifold, then an upgrade to IO-Link would offer similar diagnostics and performance as with a fieldbus (e.g. Profinet) but at a significantly lower cost and with a less complex system:

  • Highly cost-effective solution - It replaces an analog I/O and its 4-20mA/0-10V signal with the IO-Link digital information from an analog sensor, or to an analog device such as pressure regulator, saving on inventory costs
  • Enables possibilities for customer to de-centralize devices - On small- to medium-sized machines, many of the available IO-Link masters are IP67 and can be placed on the machine near the I/O points instead of in a centralized cabinet
  • Suitable for SAFE power source - Some IO-Link devices, including Parker’s Moduflex IO Link solution, are even suitable for use with a SAFE power source which is becoming an important requirement on many markets due to new machine directives

Data availability and maintenance

IO-Link offers an increase in availability of data to the PLC, which helps to reduce time and money spent on troubleshooting analysis. There are three data types available:

  • Process data – Cyclic information that is transferred between device and the master automatically on a regular basis, used as I/O for the machine controls
  • Service data – information about the device itself, such as model and serial number, or error messages and maintenance warnings (e.g. device overheating, maximal current is exceeded, coil short circuit)
  • Parameter data – information that can be written in, or read from the device on request such as voltage level or counting cycles to support preventive maintenance needs
Know Your Pneumatics - Understanding IO-Link - IO Link Module - Pneumatics Division Europe-Automation Group-Parker Hannifin Corporation

With IO-Link, you can read and change device parameters through the control system software which enables faster configuration and commissioning, plus changes can be made dynamically from the control system as needed. IO-Link also offers the ability to monitor device outputs, receive real-time status alerts, and adjust settings from virtually anywhere. Users can identify and resolve problems that arise in a timely manner and make decisions based on real-time data from the machine components themselves.

With visibility into errors and health status from each device, users can see not only what the device is doing but also how well it is performing. These extended diagnostics allow users to easily identify when a device is malfunctioning and diagnose the problem without shutting down the line or machine.

The combination of real-time and historical data available via IO-Link helps to ensure smooth operation of system components, simplifies device replacement and enables the operator to optimize machine maintenance schedules – saving cost and reducing the risk of machine downtime.

Learn more

You can find out more about IO-Link in our brochure or use our configurator on Parker.com to discover how you can utilize IO-Link for your application.

Know Your Pneumatics - Understanding IO-Link - P Berdal - Pneumatics Division Europe-Automation Group-Parker Hannifin CorporationArticle contributed by Patrick Berdal, EMEA Product Manager for Control Devices, Pneumatic Division Europe, Parker Hannifin Corporation.

 

 

 

 

Related content

Know Your Pneumatics: 3 Ways to Adopt Advances in Pneumatic Valve Technology

Reducing Compressed Air Consumption in Beverage Manufacturing | Case Study

When is a Standard Pneumatic Valve Not Good Enough?

Categories
Recent Posts by Author

Central Tire Inflation System for Off-highway Vehicles

Parker's Central Tire Inflation System (CTIS) offers improved mobility when operating vehicles in severe off-road or soft soil conditions. Ideally suited for the agriculture and military markets, this...

What are the Challenges for Pneumatics in the Food Industry?

Starting from agriculture and food processing arriving to the packaging operation, automation is everywhere in the modern food plants and plays a fundamental role to address the required...

What is End Position Cushioning in Rodless Cylinders and How To Adjust

In the world of industrial automation, pneumatic rodless cylinders can now be found just about anywhere; from food and beverage packaging to pharmaceutical and chemical production lines. They have a...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Know Your Pneumatics: Understanding IO-Link


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha