Hydraulics

Lightraulics C-Series Actuators: High Pressure Hydraulics for Lightweight Applications

Lightraulics® C-Series Actuators: High Pressure Hydraulics for Lightweight Applications - Composite Technologies Business Unit

During the last decades, the market share of products made of reinforced plastics increased rapidly. The low density, corrosion resistance and high fatigue performance of such materials provide a wide range of benefits for different applications. Parker Hannifin has developed fully composite hydraulic cylinders for 380 bar applications which are up to 60 percent lighter than their standard steel cylinder equivalents. The fully composite cylinders were tested extensively under various mechanical and environmental influences to verify the robustness of the products. The results confirmed that the new composite barrel technology for hydraulic actuators is competitive to standard metal solutions while providing further benefits in terms of weight and corrosion resistance.

 

Industrial demand on products with low density in combination with outstanding mechanical properties requires continuous R&D effort. While for metals the development of new lightweight alloys and their joining technologies is the common approach, developments and production of composite materials moved into the focus as a reasonable alternative. Compared to metal matrix composites, fibre reinforced plastics offer additional weight savings by the low density of the matrix material. 

Figure 1

For high pressure hydraulic cylinders, accumulators and pressure vessels typically high strength steel alloys are chosen. Such materials are not suitable for lightweight applications. Depending on the level of weight efficiency of the original design, utilization of high performance metal alloys, typically based on aluminium or titanium, is the current state-of-the-art lightweight solution. Because an increase in strength typically results in low ductility and, correspondingly, reduced fatigue performance, their benefits for actuators are rather limited. Incorporation of fibre reinforced plastics can overcome the conflict of reduced fatigue at higher strength. Ideally, the load-bearing structure of the products would be made entirely out of composite, thus without a metallic liner, and without a metallic barrel that supports the axial loads applied on the end caps. Parker has developed an ultra-lightweight high pressure fully composite hydraulic cylinder series called Lightraulics®. An example of a Lightraulics® C-Series composite hydraulic actuator is shown in Figure 1.


To learn more about Parker's new technology, register to see the full white paper.

 

 

 

 

 

 

 

 

Article by Dr.-Ing. Olaf Stelling, the Value Stream Manager for the Composites Technologies Europe Business Unit of Parker Hannifin in Stuhr, Germany. He holds a diploma in Production Technologies and a PhD on New Developed Lightweight Aluminum Alloys, both from the University of Bremen in Germany. He began his career with Parker in 2010 but previously held research engineering positions at the Material Testing Institute University of Stuttgart and the Foundation Institute of Materials Technology, Department Lightweight Materials in Bremen.

 

Lightraulics® Composite Tool Cylinders: Making On-site Operations Lighter

Smart Cylinders Reduce Operational Costs

Hydraulic Technologies and Key Markets

 

Categories
Recent Posts by Author

Integrated ISOBUS Functions Help Agriculture Sector Plow Ahead

As the case is across many sectors, electronics systems are the primary drivers of innovation in today‘s agricultural industry. However, those working in this sector may have noticed that any major...

Unique Team Effort Completes Upgrading of Pressure-Relief Valves at Hoover Dam

Hoover Dam -- one of the most impressive engineering feats of the 20th century – generates hydroelectricity for millions of homes and businesses across the Southwest, and it’s a constant challenge...

Hydraulic Cylinders Enable Artistic Architecture at University | Case Study

A massive engineering and design collaboration have brought the vision of world-renowned Spanish architect Santiago Calatrava Valls to life in Lakeland, Florida. The new Innovation, Science...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Lightraulics C-Series Actuators: High Pressure Hydraulics for Lightweight Applications


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha