In point of care testing (POCT) systems, liquids are typically
moved through a self-contained consumable cartridge using air
pressure. These instruments can call for precise response times...
Posted On 04/15/2021
Read More ►
Life Science is a broad and far-reaching industry and includes
numerous segments such as Medical Devices, Pharmaceuticals,
Biotechnology, Clinical Diagnostics, and Analytical Chemistry. Many
of the...
Posted On 04/06/2021
Read More ►
In clinical diagnostics, the fastest-growing segment is
point-of-care testing (POCT). POCT consists of medical
diagnostic testing performed close to the patient, instead of a
traditional centralized...
Posted On 02/10/2021
Read More ►
Aerospace technology has been applied to demanding industrial
applications in order to gain performance improvement, increased
efficiency, and longer life. Parker's technology innovation...
Posted On 12/08/2020
Read More ►
Tractors, combines, wheel loaders, bulldozers, and excavators—you
know, the big stuff— are called upon daily to perform the heavy
lifting on the front lines of the agricultural and...
Posted On 09/08/2020
Read More ►
Point-of-care testing (POCT) is a rapidly expanding segment of
the healthcare industry. This expansion is driven by an
increasingly diverse array of advanced medical diagnostic equipment
that can be...
Posted On 07/22/2020
Read More ►
Since the advent of the semi-automatic water conditioning control
valve followed by the automatic control valve, a common weakness
has been the brine tubing connections between the brine valve and
the...
Posted On 03/05/2020
Read More ►
Compamed is a yearly international trade fair event located in
Dusseldorf, Germany with a focus on delivering world-class high
tech solutions for medical technology. This year the
event occurred on...
Posted On 01/30/2020
Read More ►
Today, gas chromatography (GC), mass spectroscopy (MS) and similar
life science instrumentation are contributing to results in drug
discovery, drug development, forensic labs, and the next...
Posted On 07/31/2019
Read More ►
Ball valves are used in a variety of industries such as
manufacturing, oil, and gas, automotive, marine, agricultural and
heavy truck. Applications may vary but include operations for
processing,...
Posted On 07/23/2019
Read More ►
Liquid valves are a critical component in the next generation of
analytical equipment used for clinical diagnostics, analytical
chemistry, environmental monitoring, agent detection, and other
life...
Posted On 06/27/2019
Read More ►
Check valves are unseen and undervalued. These valves are found in
just about every mobile and industrial hydraulic system on the
planet. Simply put, if there’s a pump, most likely you will find...
Posted On 04/04/2019
Read More ►
Valve technology has come a long way with many available features.
Gas and liquid multimedia valves that are used in chemical analysis
such as Gas Chromatography/Mass Spectrometry (GC-MS) and
Liquid...
Posted On 03/08/2019
Read More ►
Clinical and analytical laboratories are under constant pressure to
increase throughput. Throughput is the amount of material or items
passing through a system. In this case, it’s analyzing a
higher...
Posted On 02/01/2019
Read More ►
Before the advent of thermoplastic fittings, the water conditioning
industry was basically limited to brass, bronze, galvanized and
copper tubing for connecting Point-of-Entry (POE) filters,
softeners...
Posted On 09/05/2017
Read More ►
As we move into the future, the need for transportation is merging
with society’s concerns about pollution, climate change, depletion
of natural resources and the long-term sustainability of our...
Posted On 04/21/2017
Read More ►
Wherever water, chemical mixtures, oil, and gases are transported
through pipes, solenoid valves are instrumental in remotely or
automatically controlling the flow and transfer of fluids. But...
Posted On 10/04/2016
Read More ►
Some of the biggest challenges for designing battery operated,
handheld medical devices are size, weight and battery life. All
three can be significantly improved by using our new miniature
solenoid...
Posted On 03/31/2016
Read More ►
Four years ago, the International Energy Agency (IEA) asked: “Are
we entering the golden age of gas?” Today, the North American shale
gas boom, expansion of LNG trade, and new LNG and natural gas...
Posted On 10/29/2015
Read More ►
Requiring oxygen can be a difficult change in a person’s life.
Patients are being diagnosed with medical conditions like COPD at
younger ages and are not ready to give up an active lifestyle. This
is...
Posted On 10/27/2015
Read More ►