Sealing Shielding

Low Drag Dynamic Sealing for Hydraulic Clutch Applications

Low Drag Dynamic Sealing for Hydraulic Clutch Applications | Automatic Transmission | EMG GroupAs automatic transmissions become more advanced as a system, the components within must evolve as well. Performance drives the design and there are many factors that must mesh together to achieve the overall goal. Parker used its materials science and design expertise to enable an engineering breakthrough—a cost effective alternative to traditional sealing in radial seal applications where low friction is critical.

 

Efficiency drives system improvement

Improved efficiency is the leading factor when it comes to system improvement. The move to eight, nine, and ten-speed automotive transmissions are focused around improving fuel economy. Obviously, with the increased number of gear ratios, the number of clutches and clutch pistons has also increased. A reduction in the amount of energy needed to engage and retract a clutch piston directly reduces the parasitic loss of energy within the entire system. This has resulted in a significant focus on the impact of seal drag within each clutch piston. 

 

D-Rings provide advantages for automotive transmission clutch pistons

For more than a decade, D-Rings have been the preferred sealing technology for automotive transmission clutch pistons as they provide Low Drag Dynamic Sealing for Hydraulic Clutch Applications | D-Ring | EMG Groupseveral advantages to other seal designs including:

  • Bi-directional sealing capability,

  • Symmetrical design simplifies assembly,

  • Lower drag than other radial compression seal designs,

  • Reduced variation in drag response, and

  • Eliminates potential spiral failure existent with O-rings.


In the past, there was always enough fluid pressure to overcome seal drag and activate the clutches. Because these same size pumps must supply so many more clutch circuits in the transmission, this energy supplied is in greater demand. Similarly, heavy springs in the past provided enough return force to ensure immediate disengagement of the clutch. Limited availability of space, as well as lower cost targets, have resulted in smaller, lower force return springs.

 

D-Ring cuts drag forces by 50%

Low Drag Dynamic Sealing for Hydraulic Clutch Applications | Low Drag D-Ring | EMG GroupOur engineers have developed a low drag D-ring which reduces the drag forces in the application by 50%. All other advantages of D-ring seals are maintained including the symmetrical profile which simplifies the assembly process. This improves the first time through capability and reduces warranty costs.

 

Low Drag Dynamic Sealing for Hydraulic Clutch Applications | Formula | EMG GroupBy creating volume space to which the deflected rubber can easily flow to, the reaction forces against the mating surface (normal force) is reduced while still maintaining sufficient sealing forces.

 

In addition, Parker’s unique manufacturing approach provides a significant cost reduction over compression and injection molded designs. The absence of mold parting lines in this new technology also eliminates molded rubber flash on the sealing surface which is inherent with injection or compression molded products.

Low Drag Dynamic Sealing for Hydraulic Clutch Applications | Drag forces reduced chart | EMG GroupLower clutch seal drag provides several advantages including:

  • Smoother shifts,

  • Overall improvement in system efficiency, and

  • Smaller return springs save space, weight, and cost.

 

Low Drag Dynamic Sealing for Hydraulic Clutch Applications | D-Ring vs. Low Drag D-RingThis technology is also available for applications beyond transmission clutches. Any reciprocating piston application can benefit from low drag D-rings. Examples would include active differentials and other torque management applications.

 

Please contact one of Parker’s application engineers to discuss how low drag seals can improve the performance and efficiency of your applications.

Parker's Purpose is all about how we impact the world around us. It's about using our expertise to enable engineering breakthroughs. It's about nurturing customer ideas—from complex challenge to real life application. Finally, it's about creating a better, more efficient, more sustainable tomorrow. And the Low Drag D-Ring checks every box.

 

IFPE 2020

Planning on attending IFPE 2020?

To learn more about Parker's off-road machinery solutions, stop by booth #S80245 at IFPE/CONEXPO-Con/AGG in Las Vegas, March 10-14.

 

 

 

Scott A. Van Luvender, automotive applications engineering managerArticle contributed by Scott A. Van Luvender, automotive applications engineering manager, Engineered Materials Group.






 

Related content for you:

Clutch Sealing for Today's Automatic Transmissions

Custom Seals Provide Trusted Results for Automotive Industry Challenges

A Simple Guide to Radial Seals | Sealing Fundamentals

 

 

Categories
Recent Posts by Author

6 Tips When Selecting an Electrically Conductive Adhesive

There are many ways to improve the electrical continuity of electronic enclosures and the resultant EMC performance using a variety of electrically conductive gaskets and mechanical fasteners.  Such...

Installation of Linear Fluid Power Seals

  So, you’ve unboxed the shiny new Parker seals you ordered – now what?  Installing seals for the first time can be challenging without the right know-how and tools. In this article we’ll discuss best...

Reduce Downtime and Costly Seal Replacements: Seal Failure Diagnosis Part 1

There are many situations where an O-Ring may not last as long as one thinks that it should. When the expectation is realistic and yet the seal fails earlier than expected, the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Low Drag Dynamic Sealing for Hydraulic Clutch Applications


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha