Careful and correct sensor installation is vital if accurate and reliable information is to be measured and communicated from the sensor.
What all engineers want when it comes to sensor installation is a simple, secure and rapid assembly process, without complicated processes such as the need for additional mountings.
The P8S proximity sensor offers universal use, flexible integration and excellent form. Its square design is also suitable for rapid installation in industry-standard T-slots, regardless of cylinder profile or brand. The upshot of this direct, drop-in design – as opposed to ‘turn-in’ or ‘slide-in’ concepts – is a significant reduction in installation time.
Among the innovations with the P8S are retaining ribs on the side of the sensor body that enable simple mounting, including hard-to-reach locations or overhead assemblies. These ribs ensure the sensor conveniently holds its position in the T-slot even before the screw is tightened.
To begin the installation, simply slide the sensor into the T-slot. When in the desired position, a quarter-turn of the eccentric stainless steel screw is all that is required to secure the sensor. To further simplify mounting, the screw head design is such that it accepts either a flat-blade screwdriver or Allen key. The mounting screw even features a knurled head that helps to withstand shock or vibration.
Of course, not all cylinders have T-slots. With P8S sensors this is not a problem as they also mount externally to cylinders. As a result, fitment to round, tie rod and profile cylinders are straightforward.
To make life as simple as possible, every P8S sensor is delivered with a specific adaptor to suit dovetail grooves. Also available are special brackets for round and tie-rod cylinders. The concept is to provide one sensor for all actuator types and brands - not just Parker units.
Cables are be supplied in three or 10 metre lengths (flying lead) or 0.3 metres with an M8 rotating plug, as standard.
Ultimately, automation demands excellent functionality and precision, which in turn requires solid expertise and knowledge at all levels, including best-practice installation.
To discover more about Parker P8S sensors and benefits they can deliver, watch this video:
This article was contributed by Franck Roussilon, product manager, Pneumatic Division Europe, Parker Hannifin Corporation.
Three Things to Consider When Choosing a Smart Sensor
Easy Steps to Installing and Configuring a CPS Sensor
Know Your Pneumatics: Continuous Position Sensing
How to Install Pneumatic Cylinders to Maximise Life and Performance
Know Your Pneumatics: Selecting a Pneumatic Cylinder | Operating Environments
Have a question about Parker products or services? We can help: Contact Us!
Comments for Making Good Sense of Sensor Installation
Please note that, in an effort to combat spam, comments with hyperlinks will not be published.