Sealing Shielding

Medical Polyurethanes for Life Science Applications

Medical Polyurethane Tubing for Life SciencesThe use of polyurethane materials in the construction of medical devices is growing. Characteristics of polyurethane that make it ideal for use in medical devices include:

  • Availability of a wide range of durometers
  • High tensile strength, abrasion resistance and toughness
  • Good biocompatibility
  • Customizable chemistry for different applications
  • Plasticizer-free formulations
  • Resistance to degradation

Slight differences in polyurethane chemistry lead to distinct properties in the final product and  these chemistry variations have led to multiple thermoplastic polyurethane families.  This 8-minute video from Parker’s Engineered Polymer Systems Division helps medical device manufacturers select the optimal polyurethane for their device.

Beginning with the key components in polyurethane synthesis, Parker explains how these polymers are made and how the different chemistries affect their final outcome.  The video steps through the “pre-polymerization method”, explaining how the hard segment, soft segment, and chain extender connect to form polymer chains. The different components contribute to the materials’ high strength properties (the hard segment) and to pliability/flexibility (the soft segment) without the use of plasticizers.

Polyurethanes used in medical devices have evolved over the years, leading to materials better suited for the environments within the human body. Because medical devices are exposed to a variety of chemical attacks, care must be taken when selecting the right material for a device. Typical medical applications include:

  • Vascular access devices
  • Cardiovascular treatment devices
  • Disposable surgical supplies
  • Tracheotomy devices
  • Urological devices
  • Dialysis devices
  • Feeding tubes

This video below explains the different polyurethane families’ strengths and vulnerabilities, including hydrolysis, oxidation, and environmental stress cracking. Click here to download the white paper associated with this video. 

 

Additional articles you may be interested in:

Three Obstacles to Optimal Utility of Patient Care Products

Listening Reveals Opportunity for an Innovative Resealable Septa for Healthcare Applications

Precisely Predicting the Next Big Thing in Medicine 

Categories
Recent Posts by Author

How to Solve Large-Size Sealing Challenges at Temperatures up to 800 °C

When classic sealing materials – for instance in temperature ranges above 300°C and below -50°C – reach their limits alternative materials are required such as metal with appropriate coating/plating....

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Medical Polyurethanes for Life Science Applications


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha