Electromechanical

Meeting Demand for Efficient Automotive Vehicle Testing & Dynamometers

DynamometerThe automotive vehicle industry has experienced introductions of several new technologies and upgrades. One significant example is the rising amount of electrical content per vehicle. Testing for vehicle and engine performance is essential in the wake of additions and conversions from each of the new technologies. 

Concurrently, OEM manufacturers are facing a number of cost pressures that are fueling the dynamometer market, from both regulatory and the consumer base, leading to higher investments in R&D and testing. 

The major drivers for dynamometers use for in-plant automotive facilities are test stands with enhanced accuracy, increasing demand for vehicle quality standards and increasing awareness toward quality in new markets. The challenge faced is how to get the price down on vehicles when all other costs are increasing.
 

Industry trends driving use?

Increasing electric and hybrid vehicle production will require more specialized testing stands:

  • Automotive plants are looking at purchasing new test stands to support the production of electric and hybrid vehicles.

  • Drive/control equipment on existing test stands may go obsolete, so parts and service will be hard to come by.

  • Production costs will rise with energy prices if existing equipment is not replaced with a more energy efficient solution.
     

Test Stand with Parker Drive SystemThe growing need for modernizing dynamometers

Automotive or truck manufacturers or makers of components or sub-systems that go into a new vehicle already have test stands and dynamometer equipment that may be outdated and in need of drive/control retrofit. These customers who already have older test stands suffer from down time, trouble obtaining parts and excessive energy consumption. 

OEMs looking to purchase test stands may want specialized features in the drive/control system and not every supplier can offer that. Or, they may be looking to purchase a new test stand or dynamometer and may want to specify certain equipment in addition. Our engineers will work with the test stand manufacturer on a special design as needed. 

 

The background

A dynamometer is a necessity in automotive vehicle testing equipment used by OEMs, component suppliers and automotive testing service providers for recording several parameters such as force, torque, power and speed of the vehicle.

The use of this testing equipment is essential throughout the production cycle of an automobile, making it a necessary component of all vehicle assembly lines. This testing equipment is also used in vehicle engine manufacturing factories and dynamometer laboratories or the automotive testing service facilities to evaluate vehicle and engine performance.

Test stands and dynamometers cover a wide range of applications, but are most commonly used to test manufactured items for adherence to specification while simulating real-world operating conditions. While “test stand” is a more general term defining a machine that could test nearly any item including pumps, automotive components or electrical components, a “dynamometer” is used to measure torque or power and is more closely associated with motor or motor vehicle testing.

 

Application examples

A drive system is used in these applications to either provide motive force or absorb it, depending upon the type of test stand:

  1. A pump test stand requiring a motor to spin the pump and a drive/control system to regulate the speed and torque delivered to said pump.

  2. A dynamometer used to test an electric motor would require a second motor that would effectively act as a braking device to load the motor under test.The drive and control system would be required to absorb this energy while regulating the speed and torque during the test.

A third example would be a test stand designed to test rechargeable batteries. Here, no motive force is involved, but the test gear would charge and discharge the batteries in a controlled manner, allowing the batteries’ functionality to be evaluated.

 

Save energy!

Many test cell designs are energy wasters. Older technologies like water brakes, fan brakes or eddy current devices, for example, convert kinetic energy from the testing process to heat. Replacing these methods with a regenerative drive system can allow this wasted energy to be recaptured and returned to the power grid. In addition to reducing your carbon footprint, a solid-state drive system will quickly pay for itself in power bill savings. Energy saving features exist even within the drive system, like smart ventilation in the AC890PX series that senses internal temperature and adjusts fan speed to save energy when the unit is lightly loaded, or in cooler ambient temperatures.

 

Parker Dynamometer Drive SystemGreen, clean, controlled power

Parker regenerative drives can harvest energy from the testing process and return it to the power grid, providing a substantial net reduction in a plant’s electric use. Older dynamometers that are widely in use simply burn off the excess power and dissipate it as heat, which is wasteful of resources. In the grand scheme of things, our engineering expertise in special equipment for electric and hybrid vehicle manufacturers contributes to these vehicles being efficiently manufactured and sold, resulting in less polluting gas and diesel-powered vehicles on the road.  
 

Retrofits

Parker can provide a drive/control retrofit that will allow you to keep your existing mechanical equipment and enjoy more efficient operation. And, in many cases, better performance, and have the knowledge that the drive/control system is up to date and serviceable.  

For example, if you have an existing test cell using DC motors as prime movers or absorbers, and do not wish to upgrade to AC technology, the DC590+ digital DC series is a flexible and economical solution for test rigs through 2000 HP. Replace your obsolete SCR units with the latest in digital DC to eliminate costly repairs and downtime, with the added benefit of IoT capabilities.

 

For OEMs of vehicle test stands who are looking to expand into new markets of electric and hybrid vehicle manufacturing, Parker can provide custom or specialized drive and control systems that meet the unique testing needs of these vehicles. For those competing in the more traditional markets, Parker draws from over 30 years of experience in drives and controls to provide systems that are compact, easy to maintain, and energy efficient. 

Have a dynamometer application or just want to learn more? Download our Test Stands and Dynamometers Solutions brochure.

 

Lou Lambruschi, Marketign Services Manager, Parker HannifinArticle provided by Lou Lambruschi, marketing services manager for Parker's Electromechanical and Drives Division.

 

 

 

 

 

 

 

Related, helpful content for you:

Series Hybrid Vehicle Electrical Systems

Series Hybrid Vehicle System Design

5 Reasons to Control your Compressor with a Variable Frequency Drive

Advantageous Series Hybrid Technology Applications

A Simple Guide to Benefits of Electromechanical Technology

Categories
Recent Posts by Author

Electromechanical and Drives Technology - A Look Back on 2019

Thanks to our loyal followers for all of the interest in the topics covered in this blog over the past year. In examining the most-read blog posts over the course of 2019, it becomes obvious that...

Time-Saving Solution for Servo Presses and Joining Applications

In industry, time is money. So, for engineers who are time-pressured, there is a solution for electromechanical press and joining applications. Push-To-Fit is an innovative electromechanical solution...

High-load Rodless Actuators Powering the Factory Automation Revolution

The arguments advocating more automation in our factories and process plants are gaining momentum and translating into a revolution in production environments.  Parker designs automated linear motion...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Meeting Demand for Efficient Automotive Vehicle Testing & Dynamometers


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha