Sealing Shielding

Meeting NASA Low Outgassing Requirements in EMI Shielding Applications

Meeting NASA Low Outgassing Requirements in EMI Shielding Applications - Parker ChomericsDesign factors for satellite, high altitude, and space-based applications vary dramatically from those of land or ship-based programs. These factors include: low payload capacity, low operating temperature, and meeting material limits.

Outgassing standards, established by NASA, set a limit on the release of gasses that can possibly interfere with sensitive technology within vacuum environments such as Low Earth Orbit (LEO). This is especially important for sensitive optical systems or camera lenses where the smallest bit of vapor or gaseous components can dramatically reduce performance. 

Test and metrics

NASA outgassing requirements are often used interchangeably with ASTM E595 which establishes the test method for determining outgassing levels. During the E595 test, small samples of material are kept under vacuum and heated to 125°C for a 24-hour period. While the samples are heated, all gasses are channeled through a single release port where a chromium-plated disk is used to collect the volatile materials.

After the test, there are two key metrics that are collected and used in certifying a material to NASA Outgassing Standards. 

Meeting Low NASA Outgassing Requirementsin EMI Shielding Applications - Total Mass Loss - Parker Chomerics

 

 

 

 

 

 

 

 

 

 

 

 

 

While NASA does keep an extensive database of all materials that they have tested in house, certified labs often run ASTM E595 testing as well. For a complete list of Parker Chomerics products that pass traditional outgassing requirements (and associated NASA Data Reference Numbers), please see: Parker Chomerics NASA Outgassing Information

Outgassing in EMI shielding solutions

The most common materials to release stored vapors and gasses are sealants, adhesives, and less heavily crosslinked elastomers and polymers. Conversely, metals and glasses with few impurities tend to have a very low level of outgassing. 

While often true, many conductive elastomers made of silicone and fluorosilicone can meet these standards due to high quality raw materials and efficient processing. 

General trends for outgassing in EMI Shielding:

Steps can be taken to reduce the amount of vapor or gasses that are released by materials. One such example is known as post-baking, sometimes referred to bake-off or bake-out. This process involves baking materials at elevated temperatures (and sometimes in vacuum environments) after they have been manufactured in order to lower vapor and/or volatile compounds.

It is important to note that some materials that pass NASA outgassing standards are only able to do so after post-baking for some amount of time. It is possible that some NASA post-baking occurred at temperatures above the maximum recommended operating temperature of these materials. This elevated temperature exposure can change the physical, thermal, or electrical properties of tested materials.

Parker Chomerics has a long history of supplying manufacturers with outgassing-compliant solutions to EMI Shielding problems for vacuum and space-based. For a complete list of Parker Chomerics products that pass NASA outgassing requirements (and associated NASA Data Reference Numbers) and more information, please see: Parker Chomerics NASA Outgassing Information.

Meeting Low NASA Outgassing Requirements in EMI Shielding Applications - NASA Outgassing Information - Parker Chomerics

 

 

 

 

 

 

 

 

 

 

 

Meeting Low NASA Outgassing Requirements in EMI Shielding Applications - Ben Nudelman - Parker Chomerics

This blog contributed by Ben Nudelman, market development engineer, Chomerics Division.

 

 

 

 

 

Related content

New Essential Handbook for EMI Shielding Applications

EMI Shielding Gaskets: Spliced Gaskets vs. Molded Gaskets

Can Electrical Resistance Be Used to Predict Shielding Effectiveness?

Have a question about Parker products or services? We can help: Contact Us!

Comments for Meeting NASA Low Outgassing Requirements in EMI Shielding Applications


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha