Filtration

Microfiltration and Venting Solutions for Medical Devices

Microfiltration and Venting Solutions for Medical Devices - Bedside monitor - Parker Performance MaterialsOver the years, medical device manufacturers have improved their products to become highly reliable, compact and non-intrusive. Users benefit from preemptive monitoring of critical measures, proper dosages and the convenience these devices provide. Whether at the bedside or on the body as a wearable, medical devices offer life-protecting and life-improving value to users.

Filtration presents unique challenges to device manufacturers. To ensure reliable, long term operation of equipment, using the best performing, state-of-the-art filtration technologies equalizes pressure and reduces condensation — preventing the ingress of liquids and other contaminants.

Here, we will explore the benefits of microfiltration and venting and highlight product solutions for medical device manufacturers.
 

The importance of microfiltration

Microfiltration and Venting Solutions for Medical Devices - Microfiltration - Parker Performance MaterialsMicrofiltration media, such as aspire® microfiltration membranes, protects equipment from contamination during use. Because of the microporous structure, the protective membrane allows gas to pass through with a low pressure drop while providing a liquid and particulate barrier. Choosing the correct pore size results in bacteria and virus removal from the airstream, and in the case of a suction collection canister, the hydrophobic nature of the filter acts as a safety shut off valve to stop liquids contaminating the vacuum line. 




Typical microfiltration applications include:

  • Vacuum pump filters
  • Sensors
  • Suction collection canister filters
  • Insufflation filters
  • Smoke Filters
  • Medical pumps

 

Venting — for critical protection

Microfiltration and Venting Solutions for Medical Devices - Venting - Parker Performance MaterialsVents, such as aspire® venting membranes, provide critical protection against liquids and particulates while allowing air and gas to pass through the membrane, providing rapid pressure equalization and high airflow. The hydrophobic ePTFE vents can be treated with a proprietary oleophobic coating for added protection against liquids and oils. Vents can be combined with a charcoal adsorbent for use in ostomy and urology bags to permit easy inflation of the device while safely retaining contents and odors.


Typical venting applications include

  • Medical device vents
  • IV administration set vents
  • Spike vents
  • Ostomy bags
  • Urology bags
  • Batteries used in medical products


All of these applications benefit in similar ways by the inclusion of microfiltration and venting membranes in their design.  
 

Application: wearable medical devices

Automated electronic drug administration devices can be worn 24 hours a day. They need to be durable as the patient goes about their normal daily activities, perhaps including things like showering, swimming and jogging. It is imperative that the electronics within the wearable device are protected from the water, soap, dirt and dust that they will be exposed to, and they must vent to assure proper operation. Hence, the venting holes, are covered and sealed with protective aspire® ePTFE membranes. 


Specialized solutions

Parker's aspire® product line includes a full range of microfiltration and venting products in a variety of formats. With decades of engineering and manufacturing experience, Parker's innovative filtration team works closely with customers to solve their most critical challenges. The product portfolio includes a broad range of specialized microfiltration and venting solutions that are available in a variety of formats, including membranes, laminates, and custom die cuts. Consistent airflow, excellent retention and chemical resistant properties are the cornerstone of aspire® products.
 

For more information on aspire® microfiltration and venting membranes, please visit our website.
 

 

Microfiltration and Venting Solutions for Medical Devices - Sarah Propp Parker HannifinArticle contributed by Sarah Propp, engineering manager, Parker Performance Materials.

 

 

 

 

Related content

Supporting Medical Device Manufacturing

Bringing Medical Devices to Market Faster With Early Supplier Involvement

Point-of-Care Testing Requires Microfluidic Precision

Flexible Displacement Sensors Improve Medical Diagnostics

Learn more about Parker's solutions for Healthcare and Life Science Industry

 

Have a question about Parker products or services? We can help: Contact Us!

Comments for Microfiltration and Venting Solutions for Medical Devices


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha