Fluid Gas Handling

Mini Subcomponents for Medical Devices Make a Big Design Difference

Mini Subcomponents for Medical Devices Make a Big Design Difference - micor pumps group image - Precision Fluidics Division of Parker Hannifin Miniaturization is big in all fields these days. This trend is a challenge for machine designers faced with packing the same capabilities into a smaller space. Take the life sciences, for example. Medical device manufacturers continue to offer more portable devices in their portfolios, which forces the design engineer to fit all the performance their customers demand into a package that takes up less work space.

The struggle for size reduction also extends into larger instruments. According to a Parker Hannifin survey of lab equipment manufacturers and users, component miniaturization is key to helping them meet the demand for instruments that consume less laboratory space, fewer reagents and require smaller test samples. What’s more, these factors are critical to reducing the overall cost of ownership of an instrument, these respondents reported.

 

Supplying OEMs with a sizable advantage

This size reduction trend is dependent on getting equipment design correct at the subcomponent level. Doing more with a smaller and more efficient pump is a common strategy that can provide OEMs with a sizable advantage.

Optimized pump design and how the pump is controlled can enable a compact footprint for the pneumatic circuit. This is often done by balancing high and low flow periods of operation to allow for a smaller pump, and by achieving higher efficiencies by running the pump only at the level that matches demand allows for a smaller battery. This requires active control of the pump speed and flow, and is commonly the dividing line between mechanical engineers and electrical engineers. Mechanical engineers responsible for designing the pneumatic elements tend to be challenged in terms of how to electrically control pump flow. However, when these disciplines are combined, often through Applications Engineers, the results can be impressive.

 

Miniature pumps allow flexibility in matching motor and speed control to the design.

For example, an environmental monitoring device often requires a wide dynamic air flow range to sample the environments of workspaces, both small and large. These devices must also be as portable as possible and offer a full day’s battery life. Proper dynamic control of a single pneumatic pump makes this possible, and increased efficiency can reduce battery size

In in vitro diagnostic (IVD) instruments, a vacuum pump is often used in the waste circuit, and the load on this pump depends on the sample throughput rate of the instrument. By actively controlling the pump speed, a single smaller pump can maintain peak flow periods during waste removal and run at a slower more efficient pace to maintain a vacuum reservoir in the system between these cycles.

Most innovative life science and medical device manufacturers are demanding more control over the pump generated gas flow for improved patient therapies and more accurate patient monitoring. This flow rate flexibility is available in most diaphragm pumps; however, utilization requires close attention and collaboration between OEM engineers and pump supplier applications engineers. Once the supplier properly configures the pump and motor, it is then the responsibility of the OEM engineering team to control the pump properly. To integrate and control the pump correctly, the engineer must have a good understanding of motor/pump speed control methods.

Speed control is commonly used for all of the available Parker Precision Fluidics motor types, Iron Core Permanent Magnet Direct Current (PMDC) motor (often called “brush motor,” Coreless DC brush motor, and Brushless Direct Current (BLDC) motors.

 

Mini Subcomponents for Medical Devices Make a Big Design Difference - Example of  Parker Pumps with Flexible Motor OptionsPMDC brush motors offer two methods for changing speed: Pulse Width Modulation (PWM) or direct adjustment of the input voltage to the motor. Due to the cost and complexity of variable power supplies, direct adjustment of the motor voltage is not common; it is more typical for designers to use PWM to change the effective voltage to the motor.

 

 

 

 

Example of  Parker Pumps with Flexible Motor Options

 

A 20% duty cycle PWM signal

Like brush motors, BLDC motors can be controlled with direct input voltage adjustment or PWM of the input voltage, but because BLDC motors use an electronic controller to operate (which is built into some pumps), these motors offer more speed control options. Many BLDC motors can also be controlled independent of the input voltage, using a low current PWM signal or a low current 0–5 Vdc analog speed control. 

 

Mini Subcomponents for Medical Devices Make a Big Design Difference - Example of a 20% Duty Cycle PWM Signal - Precision Fluidics - Parker Hannifin

 

The four most common methods for controlling the motor/pump speed are:           

  1. Input Voltage (brush or BLDC): adjusting the voltage changes the speed of a motor proportionally. For example, the flow rate of a 12 Vdc pump can be reduced by operating the pump slowly at 6 Vdc (depending on the application).

  2. Input Voltage PWM (brush or BLDC): similar to adjusting the voltage, the speed of the motor is reduced with a lower effective voltage. A lower voltage is simulated by turning off the fixed input voltage at a fast rate, often 20 kHz. The ratio of on-time to off-time (duty cycle) defines the effective voltage applied to the motor.

  3. External PWM (BLDC only): the input voltage on the first two wires of the motor is fixed and does not change; the speed is adjusted by applying a PWM signal to a third wire. A low current signal is externally switched to ground at a high frequency (by the system controller). The internal BLDC motor controller responds to this signal to reduce the speed proportionally to the signal duty cycle.

  4. 0–5 Vdc Analog Speed Input (BLDC only): the input voltage on the first two wires of the motor is fixed and does not change; the speed is adjusted using an externally supplied DC voltage applied to the third wire. The internal BLDC motor controller responds to this signal to reduce the speed linearly with the input voltage. For example, 5 Vdc could be at 100% speed, 2.5 Vdc at 50%, and at 0 Vdc the motor would be off.

 

Mini Subcomponents for Medical Devices Make a Big Design Difference - Jamie CampbellArticle contributed by Jamie Campbell, applications engineer – Precision Fluidics Division, Parker Hannifin Co. and was originally published in DesignNews Sept 2015.

 

 

 

 

Other related content:

How to Integrate Motor Speed Control for Pump Motors in Medical Devices

Advanced Liquid Valves Expand Microfluidic Possibilities

Why Servo Motors Top Stepper Motors for Precision Liquid Dispensing

Categories
Recent Posts by Author

How Condition Monitoring Can Transform the Food and Beverage Industry

Our sense of taste is changing. We’re becoming more health conscious of the foods and beverages we consume to living a better life. No more perplexing and hard-to-pronounce food labels....

Frequently Asked Questions About Seal-Lok for CNG Fittings

Seal-Lok for CNG Fittings and Adapters provide reliable natural gas fuel conveyance in CNG applications with an O-ring face seal design that incorporates an elastomeric seal compound made of...

Any pressure. Any project. One solution. Infographic

GlobalCore is the future that OEMs and end users around the world have been asking for: a unified family of robust hydraulic hoses designed to endure the tough conditions where work gets...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Mini Subcomponents for Medical Devices Make a Big Design Difference


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha