Mining
How An Alternative Axial Piston Pump Delivers Design Flexibility and Cost Savings - Infographic
Finding a cost-effective piston pump for a heavy-duty application with a shorter lead time and design flexibility can be very uncommon in the marketplace.  However, Parker's PVplus Axial Piston...
Read More ►
Types and Causes of Corrosion in Off-Road Machinery | Infographic
Corrosion management and prevention is a critical factor in many industrial settings. Left untreated, corrosion can put infrastructure, safety and business performance at risk – with potentially...
Read More ►
Off-Road Machinery- Key Technologies Tackling Challenges With Solutions
Combining innovative thinking with core technological competency can tame the challenges of off-road machinery operating in hazardous mining, agricultural, forestry, material handling, and...
Read More ►
Electric Mining Equipment is Poised to Power the Industry
Traditionally dependent on fossil fuels to run key equipment, mining is known as a carbon-intensive industry. New trends, such as battery-powered underground mining equipment, are promising to disrupt...
Read More ►
Mining Automation Promises Improvements to Safety, Productivity
Difficulty and danger have always been inherent in the mining profession. Miners typically face risks ranging from flying debris to mine collapse, to vehicular incidents. But as mining operations move...
Read More ►
Helical Rotary Actuator on Mining Rock Drilling Machine Helps Reliability
The Tamrock Axera 226 — built in Lyon, France, by Sandvik Mining and Construction — is a rubber-tired, twin-boom rock-drilling machine. Typically used for underground hard-rock mining and tunneling...
Read More ►
New Motor and Generator Solution Supports Cleaner Vehicles of the Future
Electrification remains one of the primary trends in the automotive sector, as vehicle makers push hard to introduce cleaner technologies that result in lower emissions. According to a recent report...
Read More ►
Overcoming Design and Maintenance Issues in Hose Applications | Infographic
Fluids are integral to the functionality of industrial and mobile equipment, and as conduits for these fluids, hose assemblies are critical to system performance. It's well known that formed hose and...
Read More ►
Best Practices for Dust Suppression in Underground Coal Mines
Prevention is better than a cure. In coal mining, these words offer particularly good guidance. Underground mining presents numerous hazards ranging from structural collapses, flooding and...
Read More ►
New Measuring Device Supports Predictive Maintenance in Construction
Predictive maintenance is essential to maintaining the value and the long-term, reliable function of expensive machinery and systems. This can be easier said than done. Systems, equipment,...
Read More ►
Pumps in Hydraulic Systems are Key to Tire Recycling Solution for Mining
Mining trucks encounter heavy, frequent loads throughout their life cycle, and replacing their large tires, which could be in the realm of 13 feet or even larger, can occur as much as 4 to 6 times...
Read More ►
Redefining Working Under Pressure with Screw-to-Connect Couplings
The performance of heavy equipment and machinery is dependent on the reliability of every component. Whether in the factory or out in the field, the failure of a single mechanical element...
Read More ►
5 Reasons to Choose this Axial Piston Pump for your Next Mobile Application - Infographic
The next generation mobile hydraulic pump is designed for mobile and built to perform.   The  P1M Series Mobile Open Circuit Medium Pressure Axial Piston Pump, increases equipment’s performance and...
Read More ►
Dust is More Damaging Than You Think
Equipment in the field, including mining and construction, is subject to any number of conditions, from pouring rain to damaging winds, but dust is one factor that could be more damaging than...
Read More ►
Portable Ash Probe Provides Accuracy in Harsh Mining Environments
The Ash Probe is a portable instrument for measuring the ash content of coal, providing the user with highly accurate readings within seconds. Instantaneous readings can be made of coal quality on...
Read More ►
Screw-to-Connect Couplings Make Hard Work Easier
Hard working excavators, tunnel boring, mining, oil field and forestry equipment use a variety of tool attachments. This allows them to be versatile for a multitude of activities, all necessary to...
Read More ►
Fluid Conveyance and Asset Tracking in Mining
As one of the leading suppliers to the mining market, Parker provides its customers with a broad portfolio of fluid handling technologies capable of increasing the efficiency and productivity of ore...
Read More ►
Using a Mobile Display as a Dynamic Numeric Keypad Input Device
Control of vehicle speed is important to equipment operators. The ability to accurately set the speed of a conveyor or roller in applications such as road paving or striping, crop sprayers and sugar...
Read More ►
Do You Know How Extreme Cold Affects Your Hydraulic Hose Properties?
Extremely cold environments with conditions such as snow, ice, and high wind speeds are a challenge for all rubber hydraulic hoses.  Frequently, hoses must withstand temperature ranges below -57 °C...
Read More ►
Keep Employees Safe with Engineered Breathing Air Systems
In many applications across a multitude of industries like mining, hazmat and pharmaceuticals, employers must supply breathing air systems when necessary to keep employees safe. A variety of hazardous...
Read More ►