Sealing Shielding

Need Better Flow Rate Control? Look to THERM-A-GAP GEL 37

Need Better Flow Rate Control? Look to This Dispensable Thermal Material | GEL 37 Dispensable | Parker ChomericsThe demand for dispensing thermal interface material (TIM) has increased exponentially because dispensables offer engineers flexibility in the designs and patterns that can be applied to electronics packaging.

Single-component, dispensable TIMs such as THERM-A-GAPTM GELs, can cover a variety of gaps and form complex geometries which provide reduced thermal contact resistance, thus reducing the temperature and increasing the efficiency of the application. 
 

Ideal for precise dispensing

In applications that require precise dispensing, like automotive vision and controller modules found on Advanced Driver Assistance Systems (ADAS) systems, high volume dispensing machines can dispense large volume cartridges or pails of TIM on thousands of parts per hour.

  • These dispense machines offer the greatest control and yield

  • As well as the fastest cycle times with generally the lowest material cost per piece

  • The proper equipment choice will be a function of geometry, throughput requirements, material type, and package 

However, issues tend to arise when these large cartridges and pails must be changed out when the material is used up. Today, many customers deploying high volume dispensing on their lines are running into throughput issues due to downtime and re-calibration required to change out an empty cartridge or pail.  
 

Increase output, lower downtime

Need Better Flow Rate Control? Look to This Dispensable Thermal Material | GEL 37 | Parker Chomerics

In some instances, our engineers have seen customer downtime go from minutes to hours or even days when processing and other systems need to be adjusted between changeovers. 

Its clear users of high volume dispense material in applications such as automotive ADAS cannot afford this severe interruption in their supply chains.  

This is where THERM-A-GAP GEL 37, the next generation of a single component, no cure required, thermal interface materials from Parker Chomerics is so useful

With a higher thermal conductivity and better flow control than its predecessor, we consider THERM-A-GAP GEL 37 to be the dispensable TIM that will help to lower downtime and re-calibration between vessels.

 

Need Better Flow Rate Control? Look to This Dispensable Thermal Material | GEL 37 Brian Mahoney Quote | Parker Chomerics

 


THERM-A-GAP GEL 37 significantly improves dispense variability and limits downtime due to material and processing adjustments. Other benefits include:

  • Pigmented blue for ease of use by vision systems

  • Offers a 50% higher flow rate compared to THERM-A-GAP GEL 30

  • Ideal for the automotive market segment where a dispensed thermal material with a tighter flow rate and an easier dispense material help to solve those critical changeover interruptions

THERM-A-GAP GEL 37 will be manufactured in Hudson, NH, and is available today for immediate sampling and prototyping. 

Need Better Flow Rate Control? Look to This Dispensable Thermal Material | Learn More about THERM-A-GAP GEL 37 | Parker Chomerics

 

 

 

 

 



 

 

Need Better Flow Rate Control? Look to This Dispensable Thermal Material | Jarrod Cohen | Parker Chomerics



This blog was contributed by Jarrod Cohen, marketing communications manager, Parker Chomerics Division.

 

 

 

 

Related Content:

The Benefits of Thermally Conductive, Fully Cured Dispensable Gel

New Thermal Gel Benefits Consumer and Automotive Applications

Viscosity vs. Flow Rate - Which Is Best in Thermal Interface Materials?

Have a question about Parker products or services? We can help: Contact Us!

Comments for Need Better Flow Rate Control? Look to THERM-A-GAP GEL 37


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha