Fluid Gas Handling

New 20,000 psi Coupler Takes Offshore Drilling Operations Deeper

New 20,000 psi Coupler Takes Offshore Drilling Operations Deeper - Offshore Drilling - Parker Hannifin Quick Coupling DivisionWithstanding the high pressures of deepwater reservoirs has been a challenge for offshore drilling operations limited by the capabilities of their equipment.

Going after deep reservoirs with higher internal pressures requires components that can operate reliably at higher-pressure levels. If a single component can’t handle the pressure, then the entire system is compromised. Until now, reliable component performance at extreme depths has been an issue for drillers, Christmas tree manufactures, and chemical injection companies. 

A new offering from Parker’s Quick Coupling Division (QCD) could be the innovation that helps operators reach more reservoirs than ever before.

 

Metal sealed coupler unique to the marketplace

Parker's Quick Coupling Division is introducing the new 20,000 psi Metal Sealed Coupler.

Unique to the marketplace, the coupler has a working pressure of 20,000 psi which allows for reliable connections and disconnections while working in higher-pressure formations. Features and benefits include:

  • One of the first subsea couplers with a working pressure of 20,000 psi
  • Designed for high-pressure, high-temperature (HPHT) environments 
  • Allows operators to reach more reservoirs than ever before
  • Ideal for connecting multiple pieces of equipment in deep water applications

The 20,000 psi Metal Sealed Coupler is one of the first couplers that can be used on equipment servicing higher-pressure reservoirs. This is ideal for connecting multiple pieces of equipment in the offshore industry, including Christmas tree manufacturing, oil production, and chemical injection.

To create reliable connections, the coupler combines two types of seals, making it ideal for harsh HPHT environments at extreme depths:

  • Seals designed for connection under full-system pressure
  • Seals designed with Parker patented metal sealing technology for increased wear and high-temperature resistance

 

Watch this video:

 

New 20,000 psi Coupler Takes Offshore Drilling Operations Deeper - SubSea Application - Parker Hannifin Quick Coupling DivisionMetal sealed, low separation force 15,000 psi couplings

  • Designed for low separation force while under pressure
  • Offer superior flow and reliable performance in the harshest environments
  • Primary and secondary seals create a secure barrier to prevent water leakage that could lead to unplanned downtime

MCD series stab plate

  • Designed for maximum performance, easy installation, long life, and a sound connection in harsh subsea conditions
  • Lightweight for easy handling and installation
  • Ideal for subsea production control applications

 

Are you attending the Offshore Technology Conference (OTC)?

New 20,000 psi Coupler Takes Offshore Drilling Operations Deeper - Schedule a Meeting - Parker Hannifin Quick Coupling DivisionSchedule a meeting with an engineer at the show to learn more about the new 20,000 psi Metal Sealed Coupler, see our other products, and discuss solutions to your application challenges. OTC is the largest event in the world for the oil and gas industry featuring more than 2,400 exhibitors and attendees representing 120 countries.

Parker Hannifin
OTC
Booth 3639
April 30 - May 3, 2018
NRG Park
Houston, TX

 

New 20,000 psi Coupler Takes Offshore Drilling Operations Deeper - Subsea Connections Product Brochure - Parker Hannifin Quick Coupling DivisionDownload the subsea connection systems product brochure.

 

 

 

 

 

 

New 20,000 psi Coupler Takes Offshore Drilling Operations Deeper - Jason Mikulski, subsea business development manager - Parker Hannifin Quick Coupling DivisionThis post was contributed by Jason Mikulski, subsea business development manager, Parker Quick Coupling Division.

 

 

 

 

Related posts:

A Deeper Look at Subsea Hydraulic Couplings

Do Your Seals Meet the Demands of the Oil and Gas Industry

Large Capacity Piston Accumulators Help Subsea Engineers Meet Extreme Demands

Advanced Material Development for High-Pressure/High-Temperature Oil & Gas Extraction

Categories
Recent Posts by Author

Do You Know How Extreme Cold Affects Your Hydraulic Hose Properties?

Extremely cold environments with conditions such as snow, ice, and high wind speeds are a challenge for all rubber hydraulic hoses.  Frequently, hoses must withstand temperature ranges below -57 °C...

Under Pressure: The Importance of Reinforcement in Hydraulic Hoses

Selecting the proper hose for a hydraulic assembly is critical to ensure that it meets the requirements for that specific application. One of the first steps in selecting the proper hose is to...

Why are Brass Fittings Preferred by Truck Manufacturers?

Like many industrial markets, the heavy truck market utilizes brass fittings for a variety of applications. With composite fittings gaining traction in the arena, why do many truck OEMs continue...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for New 20,000 psi Coupler Takes Offshore Drilling Operations Deeper


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha