Filtration

New Coalescer Technology Improves Performance and Protects Gas Turbines

New Coalescer Technology Improve Gas Turbine Performance - Power Plant - Parker GTFFor power plants located in moisture-rich environments, such as coastal locations, high levels of humidity, rain, fog, mist and sand can damage and impair the performance of the gas turbine. Coalescers are installed to remove moisture and liquid phase corrosives from the airstream — protecting the downstream filters and the turbine. In this blog, we will look at the coalescing process, issues with today's coalescers, and explore the effectiveness of a new coalescer technology.

 

New Coalescer Technology Improves Gas Turbine Performance - Improving Filter Performance in Harsh Environments White Paper - Parker GTFThis white paper, "Improving Filter Life in Harsh Environments", details comprehensive field tests conducted to test the effectiveness of a new coalescer technology designed to improve filter performance and protect gas turbines. Download now.  

 

 

 

 

How coalescing works

New Coalescer Technology Improves Gas Turbine Performance - How coalescing works - Parker GTFCoalescers remove moisture by agglomerating water droplets, making them larger and heavier. This allows a large proportion of the droplets to drain away rather than continue in the airstream, which helps avoid these two problems:

1. Small liquid droplets allowed to travel downstream can become embedded between the pleats of the filter (pleated filters are the current standard design for high-efficiency filter products). This impediment to the air can lead to differential pressure spikes. This can lead to an accelerated differential pressure increase in certain conditions such as fog, causing gas turbine alarm and trip levels to be reached quickly.

2. Small liquid droplets can also form mud caused by:

  • The associated increase in residence time, due to the small liquid droplets being embedded within the pleats rather than flowing vertically down and away.
  • The high total droplet surface area (associated with a large quantity of embedded small liquid droplets) allows for greater interaction with any accumulated dust.

In either case—and especially with mud—it is common to see a differential pressure spike. 

 

Is compressed air pulsing effective?

Unfortunately, the use of a compressed air pulsing system has a limited effect. The system would have to exceed normal operating limits to obtain the inertial forces required to overcome the surface and frictional effects present and adequately remove the embedded liquid and/or sticky dust.


The problem with today's coalescers

Historically, coalescer media has been similar to what is used in dust filtration. Thus, they naturally capture dust in addition to liquid, which can result in block up, differential pressure increase and, in high-dust environments, three other problems:

  • Constant monitoring
  • Frequent maintenance
  • Frequent coalescer replacement

 

New Coalescer Technology Improves Gas Turbine Performance - weather hood without moisture separator and clearcurrent coalescers - Parker GTFFor example, in a typical, self-cleaning filter house, the high-efficiency cartridge filters are protected from the elements by weather hoods. (see figure to the left). This arrangement provides basic protection only against big, heavy rain droplets. It does not protect filters against exposure to fine and light fog droplets. Exposure of the filter elements to fine water particles in the form of fog leads to wet filters and reduced filter life, manifested as high differential pressure across the filters and/or the gas turbine alarm being reached. If the high-efficiency filter is not hydrophobic (not moisture repellent), moisture droplets (potentially containing salts) will leach through the filters resulting in:

  • Power output reduction
  • Unplanned shutdown
  • Damage or even catastrophic failure of compressor and turbine components
     

Coalescers on the market today exhibit problems such as:

  • They require frequent replacement, resulting in extensive downtime. 
  • They are very difficult to clean and do not return to their original efficiency and pressure loss.
  • Often the dust and sand deposits become so great, they increase the pressure loss across the coalescer. When that happens, it triggers a pressure release mechanism, and the coalescer pops up. This allows air to pass through without being coalesced—removing the protection against fine droplets.

 

New filtration technology offers a solution

New Coalescer Technology Improves Performance and Protects Gas Turbines - TS1000 Coalescer - Parker GTFWhether the trouble stems from dust, fog or sand, power plants operating in harsh environments need an effective solution with coalescers to protect both the life of the high-efficiency filters and the performance of the gas turbine. The clearcurrent TS1000 coalescer panel filter from Parker, for example, uses a new technology to provide fine mist/fog removal effectiveness combined with significantly low dust removal efficiency.

Unlike traditional coalescers, the TS1000 coalescer panel uses 100 percent synthetic high-performance woven mesh that catches small liquid droplets, combines them with larger ones, then drops them out of the airstream while allowing bypass of sand and dust particles.
 

“The clearcurrent TS1000 has excellent fine mist/fog removal effectiveness with significantly low dust removal efficiency ... It provides superb performance during the fog season with low risk of clogging during a sand storm. In the end, it requires much less attention from the operator and helps reduce the maintenance to a minimum.”

— Tim Nicholas, powergen market manager, Parker Hannifin
 

New Coalescer Technology Improves Gas Turbine Performance - Weather hood with clearcurrent TS1000 - Parker GTFOther features and benefits include:

  • Coalesces 99% of water droplets down to 10 microns.
  • Pressure drop remains steady and not affected by dust deposits.
  • Can be easily cleaned in place, dramatically decreasing maintenance time.
  • Excellent service life performance.

 

Three comprehensive field tests were conducted to demonstrate the effectiveness of the TS1000 over competitive coalescers. The results showed the clearcurrent TS1000 coalescer panel filter went about three times longer than other products tested before needing to be cleaned, and when it did need cleaning, the work was quicker and extended the life of the coalescer for up to 12 months.

 

Key takeaway

The clearcurrent TS1000 coalescer panel filter helps maintain gas turbine inlet air quality, whether the harsh environment produces dust, fog or sand. Not only does it improve the overall coalescing performance, but it also delivers low pressure drop, requires low maintenance and extends service life to achieve better gas turbine operation.
 

New Coalescer Technology Improves Gas Turbine Performance - Download white paper Improving Filter Life in Harsh Environments - Parker GTFTo see the detailed field test data, download the full white paper "Improving Filter Life in Harsh Environments: Reducing Maintenance Costs, Extending Filter Life and Delivering Better Performance for Gas Turbines"


New Coalescer Technology Improves Gas Turbine Performance - Tim Nicholas - Parker GTFThis post was contributed by Tim Nicholas, powergen market manager, Parker Gas Turbine Filtration Division.

 

 

 

 

 

 

Related content

Improving Power Plant Gas Turbine Performance in Harsh Desert Environments

How to Avoid Gas Turbine Shutdowns in LNG Processing Facilities

What You Need to Know About Coalescing Filtration

 

Have a question about Parker products or services? We can help: Contact Us!

Comments for New Coalescer Technology Improves Performance and Protects Gas Turbines


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha