Aerospace

New Fittings Simplify & Verify Hydraulic System Connections

New Fittings Simplify & Verify Hydraulic System Connections - Visual Torque Indication Fitting - Parker Stratoflex Products DivisionTubing, piping, and hose – and the fittings that connect them – are the circulatory systems of today’s aircraft. Carrying high-pressure hydraulic fluid to and through critical subsystems and components such as flight control actuators, engine-driven pumps, auxiliary pumps, electric motor pumps, power transfer units, and more, these components are key to an aircraft’s power and flight control. Yet, despite the increased complexity of hydraulic systems today, fluid leakage is a nagging cause for re-work and unscheduled maintenance.

But what if there was a better way? What if an innovative approach offered lower installation time with a visual indicator for a leak-free connection?

Enter the new visual torque indication, a patent-pending family of fittings that offers these benefits and more from the Stratoflex Products Division of Parker Aerospace, the industry leader in fluid conveyance systems and components.


Current state: uncertainty of connection, time-consuming installation process

New Fittings Simplify & Verify Hydraulic System Connections - Connections Inside A321 Main Landing Gear Well - Parker Stratoflex Products DivisionPlumbing and maintaining the hydraulic system of a large commercial aircraft can be a daunting and time-consuming task. A typical commercial transport contains hundreds of feet of tubing and thousands of fittings and fitting connections1.

Today, installers use torque wrenches and specialized torque procedures to secure system connections and apply a torque stripe to indicate completed assembly. However, the large number of connections and challenging installation requirements lead to improper connections, with no means of detection until the system is pressurized. Should the connection leak, additional time must be taken to locate the improper connection, clean hydraulic fluid spills, and re-torque or replace the leaking assembly.


Connection innovation: Parker visual torque indication fittings

With patent-pending design features, visual torque indication fittings offer significantly lower installation time for connections while providing an immediate, visual verification of a properly assembled connection. These benefits combine to support the increased production rates required by aircraft OEMs for the demanding aerospace market.

Developed from proven Parker fluid connection technology and qualified to industry and customer requirements, visual torque indication fittings offer: 

  • Visual indication: verifies proper connection, eliminates torque striping and facilitates fast, error-free inspection
  • Unique thread design: provides faster connection time and is tolerant to misalignment during assembly
  • Dual seals: provide redundancy against system leakage and associated re-work
  • Standard wrench assembly: no specialty tools or torque procedure needed

Visual torque indication fittings are designed for operating pressures for today’s hydraulic systems. Visual torque indication fittings utilize aerospace materials (corrosion-resistant steel, aluminum, titanium) for sizes -4 through -24.

For additional information on Parker Aerospace systems and capabilities, please visit our website

 

New Fittings Simplify & Verify Hydraulic System Connections - Jonathan Golightly, senior engineer, and Scott Pearson, division engineering director - Parker Stratoflex Products DivisionThis post was contributed by Jonathan Golightly, senior engineer, and Scott Pearson, division engineering director, of Parker Aerospace’s Stratoflex Products Division.

 

 

References 

1 https://www.aviationpros.com/home/article/10388648/hydraulic-systems-tubing

 

Related content

Making Light Work of High-Pressure Aerospace Fluid Conveyance Applications

Keeping Aircraft Fleets Healthy Around the Clock and Around the Globe

Operational Initiatives Target Zero Defects and On-Time Delivery

China Joint Ventures Respond to Current and Future Growth Needs in the Asia-Pacific Region

Global Reach Expanded with Around-the-Clock Service and Pooling Centers

Categories
Recent Posts by Author

Parker Aerospace & American Magic on Course to Compete for the 36th America’s Cup

The America’s Cup is the oldest trophy in international sports and the highest prize in sailing. Although it has a colorful history dating to 1851, America’s Cup wind-powered racing yachts...

Giving Back to the Community During the Holidays Across Parker Aerospace

Parker Hannifin believes that creating a better tomorrow for everyone begins with a commitment to positively impacting the lives of our team members and the communities we call home. Our culture is...

Parker Employees Volunteer to Support Local Social Causes

Corporate social responsibility (CSR) means different things to different people. For some, it means improving the communities in which they live or helping feed people in need of assistance....
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for New Fittings Simplify & Verify Hydraulic System Connections


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha