Fluid Gas Handling

Nitrous Oxide Nasal Mask and Breathing Circuit Increases Patient Comfort

Nitrous Oxide Nasal Mask Breathing circuit increases patient comfortA renowned oral and maxillofacial surgeon from Phoenix, Arizona approached Parker's Porter Instrument Division in 2011 with a prototype design for an improved nitrous oxide mask. Robert Guyette, D.M.D., M.D. set out to create a mask that allowed better access to the oral cavity during dental procedures since current masks were bulky and often uncomfortable for his patients. Dr. Guyette was familiar with the Porter brand and approached Parker as a potential partner.

Watch this video to hear Dr. Guyette talk about his experience:

 

 

Engineering development approach

Employees at Porter quickly formed two high performance teams to lead engineering development and value stream mapping for the new product line to be manufactured at its Hatfield, Pennsylvania location. The manufacturing line was designed, developed, and installed in about three months by multi-functional teams including Engineering, Porter's in-house Model Shop, Process Engineering, and Manufacturing employees.

Since the product is a class one medical device, deployment of the entire production line was carefully monitored and documented under strict Design Validation and Verification methods that are recorded under formal Design Control Guidelines that comply with FDA Quality System Regulation ISO 13485, and CE Mark Medical Directive Directive 93/42/EEC, as well as ISO 9001.

Low profile nasal mask solution

Nitrous Oxide Nasal mask Breathing circuit Increases Patient Comfort - Parker Porter _ Dental Medical The result is the Silhouette low profile nasal mask; an anatomically accurate, low profile, lightweight mask that fits comfortably over the patient’s nose while providing excellent access to all areas of the mouth. Silhouette is a single use nasal mask and breathing circuit designed with lightweight tubing and an adhesive strip across the bridge of the nose that creates an unprecedented seal enabling a predictable analgesia experience. The product was commercially launched on March 1, 2015 after an initial introduction at the Chicago Dental Show in February.

 

Design advantages 

The unique design offers many advantages over traditional nasal hoods, including:

  • Unobstructed access to the oral cavity

  • A more predictable nitrous experience

  • Adhesive strip to secure the mask in place

  • Enhanced scavenging efficiency for reduced N2O exposure

  • Disposable mask and circuit for improved infection control

  • Four size options for a perfect fit on all patients

This new product line supports Parker Porter’s strategy to expand its market presence beyond dental applications to include hospitals and physicians’ offices that use nitrous oxide for pain management and minimal sedation. Increasing patient comfort with its streamlined design, the new Silhouette low profile nasal mask can accommodate many medical applications where nitrous oxide is used.

SILHOUETTE is a revolutionary new nitrous oxide nasal mask designed by a dentist for dentists. It eliminates the hassles many dentists associate with using nitrous oxide. The result is a compact and comfortable nasal mask that's nearly invisible and creates a safe and predictable experience for both the dentist and the patient.

Contact Parker Porter for more details on our latest innovations.

Related posts on Life Science:

Solving Product Design Challenges of Biocompatibility

Meeting the Biocompatibility Challenge in Respiratory Device Designs

Parker Collaborates with Cleveland Clinic to Develop Advanced Medical Technologies

Supply Chain Vertical Integration Saves Time and Money

 

Have a question about Parker products or services? We can help: Contact Us!

Comments for Nitrous Oxide Nasal Mask and Breathing Circuit Increases Patient Comfort


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha