Fluid Gas Handling

Non-Welded, Rapid Assembly Hydraulic Piping Solutions for Offshore Oil and Gas

Phastite for Pipe hydraulic piping solutions for offshore oil and gas

Speed, consistency, durability, and safety: the four criteria you seek for your offshore oil and gas piping connections, particularly those occurring in deep water where extreme pressure presents unique challenges. Phastite for Pipe, Parker's non-welded pipe connection system, answers the call with a mechanically attached, permanent solution.



Speed and Consistency

The Challenge: 
When Parker's engineers set out to design a failsafe method for connecting a pipe to secure against blowout risks, we worked with customers to ensure that every challenge was addressed. Chief among these were lengthy welding processes and operator-dependency that leads to outcome variance. 

Phastite solution:
Welding a typical connection can take up to 30 minutes per joint. Using Phastite for Pipe, an entire assembly can be completed in 10 minutes; a non-welded system for high-pressure piping applications can be assembled in minutes instead of hours. In addition, the time consuming and costly examination processes typically associated with welded pipe connections, such as radiography, liquid dye penetrant or x-ray inspection, can be eliminated.


Phastite for Pipe hydraulic plumbing solutions for offshore oil and gas BOP and HPU applicationsDurability

The Challenge:
Pressure, vibration, stress, torsion, tension, bending and static forces all conspire against the integrity of a pipe connection. 

Phastite solution:
We put our Phastite for Pipe system through rigorous testing for extreme conditions along each of these parameters and asked the most respected professional organizations to oversee this testing process.

Phastite survived every stress placed on it, holding under dynamic working pressures of 6,000 PSI and static pressures up to 10,000 PSI. In some of the deepest operations of up to 15,000 feet, Phastite still performs. In fact, Phastite for Pipe earned the highest level of approval offered by DNV-GL for subsea performance and reliability. 

Corrosion, a major concern in undersea operations, is almost non-existent because of the highly resistant stainless steel composition.

 

Safety

The Challenge:
Procedures and materials you add to your operation require hazardous materials documentation and safety training. They may also add small to significant risks of worker injury and add to your worker's compensation premiums. Minimizing this time, risk and administrative burden is always a challenge.

Phastite solution: 
With Phastite for Pipe, procedures like welding and subsequent non-destructive testing of the joints are unnecessary, saving the time and extra safety measures these operations require. 
 

Simply perfect

When it comes to the hydraulic plumbing connections for both subsea blowout preventers (BOP) and topside hydraulic power units, lengthy time consuming and complicated procedures have found their nemesis. Simplify with a fast, safe, durable sealing solution. To learn more about Parker's non-welded piping solutions for oil and gas applications watch our video, or please visit our Parker Complete Piping Solutions website for more information.

 

 

 

Ted Amling, Senior Project Engineer at Parker Tube Fittings Division

 


Contributed by Ted Amling, senior project engineer, Parker Tube Fittings Division

 

 

 

Related Content:

Non-Welded Piping Solutions for Oil and Gas Applications
Deeper Look at Subsea Hydraulic Couplings
Engineered Piping Systems for the Oil and Gas Industry 
Hydraulic Piping Solutions Save Time and Money

 

Categories
Recent Posts by Author

What Is ISO 14001:2015 and Why Is It Important?

ISO 14001 is recognized as the international standard for environmental management systems and provides organizations/businesses with criteria to follow, which will identify, control, and reduce their...

Point-of-Care Testing Requires Microfluidic Precision

Point-of-care testing (POCT) is a rapidly expanding segment of the healthcare industry. This expansion is driven by an increasingly diverse array of advanced medical diagnostic equipment that can be...

Key Design and Maintenance Challenges in Hose Applications

Formed hose and hose/tube assemblies have long been used to solve fluid handling system design challenges such as installation in confined areas or those necessitating a tight bend radius. While both...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Non-Welded, Rapid Assembly Hydraulic Piping Solutions for Offshore Oil and Gas


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha