Sealing Shielding

O-Ring Selection Made Easy with the Parker O-Ring Selector

O-Ring Selection Made Easy with the  Parker O-Ring Selector - Parker O-Ring Selector

Two things are equally important for the reliable performance of an O-Ring seal: the right size and the right material. Parker’s new O-Ring Selector is an engineering tool that enables users to make the right material and size selections easily, quickly and reliably – in a single application. The accuracy of the results ensures the desired performance of the O-Ring in the subsequent application. This is primarily based on the fact that both functionalities – the material selection and the O-Ring size calculation – are closely interlinked. This achieves a new quality in calculating the total sealing system.   

 

Overview of the O-Ring Selector

The Parker O-Ring Selector is divided into three main sections:

  • Service Conditions & Material Selector

  • Size Selector

  • Notes

 

Service Conditions & Material Selector

The Service Conditions & Material Selector section is focused on mapping the material-related application conditions. Entering the operating temperature range, the desired polymer family and/or material hardness will take the user to the suitable material selection. The Advanced Material Selector enables experienced users to specify the operating conditions in even greater detail. Here the medium to be sealed can be selected from a database containing 2,500 media. In addition, a search for required approvals and conformities can be run.

 

size selctor

After the dimensions of the system hardware have been entered, the Size Selector will calculate the dimensions and tolerances of the O-Ring based on international standards. Due to the great flexibility of possible entries, the sealing system will be “modeled” realistically. Factors such as thermal expansion or chemical swelling of the sealing element which are necessary for a precise calculation are taken into account.

 

O-Ring Selector NotesThe Notes section makes it possible for users to add their own comments and remarks to the calculation. Following the O-Ring selection process, the data obtained can be converted into a PDF document and exported.

 

 

O-Ring Selector Start metric

 

 

 

 

 

 

>>> Start imperial version
>>> Start metric version

 

Additional information:
www.parker.com/o-ring-selector

 

IFPE 2020Planning on attending IFPE 2020?

To learn more about Parker's off-road machinery solutions, stop by booth #S80245 at IFPE/CONEXPO-Con/AGG in Las Vegas, March 10-14.

 

Heinz Rost

 

 

Posted by:  
Dr. Heinz-Christian Rost
Technology & Innovation Manager
Engineered Materials Group Europe, Prädifa Technology Division

 

Related content for you:

How to Select the Right O-Ring Material with the Parker O-Ring Selector

How to Calculate the Right O-Ring Size with the Parker O-Ring Selector

 

Categories
Recent Posts by Author

How to Solve Large-Size Sealing Challenges at Temperatures up to 800 °C

When classic sealing materials – for instance in temperature ranges above 300°C and below -50°C – reach their limits alternative materials are required such as metal with appropriate coating/plating....

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for O-Ring Selection Made Easy with the Parker O-Ring Selector

Andy Todd
Hello, there is an error message when I press the imperial button. Is there a problem with the page or is the service not available anymore?

Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha