Fluid Gas Handling

Oil Changes Are Not So Traditional with QuickFit

Oil Changes Are Not So Traditional with QuickFit - Engine with Quickfit installed -  Quick Coupling DivisionLubrication is essential to machine maintenance. Equipment properly lubricated reduces wear and tear during production, ensures temperatures are in check with operational standards, minimizes corrosion and helps keep contaminants and pollutants out of the system. Organizations will allocate nearly half of their total maintenance costs to lubrication-related activities. The biggest of them all is deploying the oil change.

 

Spilling the truth on oil changes 

An oil change makes certain machines are running smoothly and prolongs engine life. There’s incentive to changing oil regularly. However, therein lies the issue. Performing an oil change is straightforward enough, correct? Not quite. For technicians and mechanics, the traditional oil change process is much more tedious and hazardous. The likelihood of making a mess or even worse can be a costly mistake. Equipment downtime, lost production, employee safety, and environmental integrity are factors an organization will risk when conducting an oil change.

 

The challenges of changing the oil   

A traditional maintenance oil change is cumbersome. From heavy machinery and power generation equipment to fleets and municipalities, changing oil involves thorough training on procedures and equipment and utilizing an arsenal of tools, which bring a multitude of challenges:

  • Each piece of equipment is different and requires a unique set of instructions

  • Multiple points can result in cross-contamination

  • Removing a filter full of oil can be difficult and result in spills, environmental contamination and cleanliness issues

  • Cramped engine compartments make access a challenge, leading to safety and ergonomic risks for maintenance staff

You can’t just stop performing oil changes. What is the solution then?

Oil Changes Are Not So Traditional with QuickFit Oil Change Quick Coupling Division

QuickFit™ Oil Change System revolutionizes oil maintenance

Parker's QuickFit Oil Change System is unlike anything else available in the marketplace. It’s radically transformed oil changes with a faster, cleaner and safer approach that hasn’t been accomplished until now. QuickFit is revolutionary, yet simple with a three-step process to purge, evacuate and refill oil.

Oil Changes are not so Traditional with QuickFit Table Quick Coupling Division

The architecture of QuickFit eliminates oil spills and greatly reduces safety hazards. This is achieved through an accessible, single connection point that allows oil to drain directly to the waste containment, and then can be used to extract the used oil from the filter and pump in new oil. The total number of steps in the process is reduced, which means a faster and safer oil change.

QuickFit combines ease-of-use with comprehensive functionality. Minimal training is necessary and maintenance is simplified as oil changes can be done efficiently and effectively. Productivity goes up while the chances of an error occurring during an oil change are greatly reduced.

Watch the video to see how a traditional oil change compares to Parker’s QuickFit Oil Change System.

Oil Changes Are Not So Traditional With QuickFit

Contributed by Matt Walley, product sales manager, Quick Coupling Division Division of Parker Hannifin.

 

 

 

 

 

Related links:

How to Change Your Engine and Machine Oil Faster, Cleaner and Safer

No More Spills! 8 Reasons Why You Need a New Oil Change Process

Improve the Efficiency of Your Fleet Service Team

 

Categories
Recent Posts by Author

Streamlining Fleet Management in 2020

Any business relying on a fleet of vehicles to operate understands that fleet-related costs are one of the most substantial expenses it will incur. Most often, controlling these expenses is the job...

Compamed Delivers on Energy-Saving Designs and Cost-Efficient Medical Devices

Compamed is a yearly international trade fair event located in Dusseldorf, Germany with a focus on delivering world-class high tech solutions for medical technology. This year the event occurred on...

Install Transair Push to Connect Fittings In 7 Easy Steps

Push to connect fittings have grown in popularity due to their ability to efficiently couple fittings to thermoplastic tubing while maintaining performance. Invented in 1969, push-to-connect fittings...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Oil Changes Are Not So Traditional with QuickFit


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha