Fluid Gas Handling

Optimize Hydraulic Systems with Top Fluid & Gas Handling Blogs of 2017

Optimize Hydraulic Systems with Top Fluid & Gas Handling Blogs of 2017-GlobalEnergy-Parker HannifinAs we look back on 2017, increased demand contributed to technology advancements and higher productivity across a range of industries including oil and gas, power generation, life science, construction, agriculture, and manufacturing. Design engineers and MRO managers placed a priority on the proper design, assembly and installation of fluid transfer components to ensure optimal performance of equipment and machinery. Here, we've compiled a list of the most read fluid and gas handling technology blogs for 2017 featuring tips, methods and solutions to optimize the function and reliability of hydraulic systems for maximum productivity and profitability. In these blogs you'll learn:

  • How to correctly measure hydraulic hose 
  • Factors that go into manufacturing and testing hose
  • Differences between skive and no skive hose
  • Key nomenclature for hose sizing
  • Testing and evaluating hydraulic hose
  • How to identify hydraulic fitting orientation
  • Materials used in hose construction
  • Important factors to consider for hydraulic fittings
  • Maintenance recommendations
  • Ways to limit exposure to respirable crystalline silica
     

Optimize Hydraulic Systems with Top Fluid & Gas Handling Blogs of 2017-Hydraulic-Hose-Parker HannifinMeasure and Specify Hydraulic Hose Length With Ease

Many hose installers are not trained on how to correctly measure and specify hose length. As a result, a replacement hose may end up being either a little shorter or a little longer than the original part. When inches matter, the confusion about properly measuring hose length can result in delays and extra expense. In this blog, you'll learn how to correctly measure hose length.

 

Optimize Hydraulic Systems with Top Fluid & Gas Handling Blogs of 2017 - Hydraulic Hose - Parker HannifinHydraulic Hose 101: Fast Facts

Hydraulic hose is more complicated than it seems. There are many factors that go into designing, manufacturing, and testing high-quality hydraulic hoses. Here are some fast facts that can make a difference for you and your productivity.

 

Optimize Hydraulic Systems with Top Fluid & Gas Handling Blogs of 2017-skive-no-skive-hoses-Parker HannifinThe Advantages of No-Skive Versus Skive Hydraulic Hose Assemblies

In this blog, you'll learn the differences between skive and no-skive hoses and the advantages of each.

 

 

 

Optimize Hydraulic Systems with Top Fluid & Gas Handling Blogs of 2017-Hose Sizing-Parker HannifinThree Key Words in Hydraulic Hose Sizing: I.D., Dash Size and Nomogram

Sizing is the most basic and essential factor in hydraulic hose selection. Here, we break down the inner diameter, dash size and nomogram for a hydraulic hose to ensure proper sizing in your application. 

 

Optimize Hydraulic Systems with Top Fluid & Gas Handling Blogs of 2017 - Standard Hose Testing - Parker HannifinStandard Testing for Hydraulic Hose and Fittings

The process for testing and evaluating hydraulic hose is defined by SAE and ISO Standards, which contain various test procedures including the change in corrosion resistance, hose construction integrity, burst, and impulse test. Read about the specifics of these tests.

 

 

Optimize Hydraulic Systems with Top Fluid & Gas Handling Blogs of 2017-An Effective Way to Identify Hydraulic Fitting Orientation - hose orientation  - Parker HannifinAn Effective Way to Identify Hydraulic Fitting Orientation

How do you determine the necessary hydraulic hose fitting when your application involves connecting two bent hoses? When your fittings are at an angle, understanding their orientation is critical. This blog presents the two methods used to simply identify the angle of a hose end.

 

 

Optimize Hydraulic Systems with Top Fluid & Gas Handling Blogs of 2017 - Manufacturing Plant - Parker HannifinThe Hydraulic Hose Mystery - How is it Made?

Hose manufacturers each use a diverse range of materials that can result in a variety of hose styles. Hoses from various manufacturers may have similar dimensions and constructions, but different rubber compounds and reinforcement materials make a huge difference when it comes to hose failures and every manufacturer's "recipe" is unique. Read this blog to get a look behind the scenes of hose manufacturing.

 

Optimize Hydraulic Systems with Top Fluid & Gas Handling Blogs of 2017 - Hydraulic Fittings - Parker HannifinFive Most Important Factors You Need to Consider for Hydraulic Fittings

OEMs and fitting manufacturers are constantly finding new ways to stump us with different threads and new ways to seal them. When making hydraulic fitting connection choices today, there are several features to research and understand for your application. We highlight connections, attachment styles and the 5 most important factors you need to consider for hydraulic fittings in this blog. 

 

Optimize Hydraulic Systems with Top Fluid & Gas Handling Blogs of 2017 - Damaged Hose - Parker Hannifin8 Simple Tips for Maintaining and Replacing Your Mast Hose

Employees often overlook hoses during routine maintenance checks for material handling equipment, which can lead to machine downtime and lost productivity. If a hose fails, it creates a potentially hazardous situation for anyone operating the unit or in close proximity. Read these 8 simple tips to properly maintain your mast hose.

 

Optimize Hydraulic Systems with Top Fluid & Gas Handling Blogs of 2017 - Jackhammer - Parker HannifinFour Ways to Use Hose in a Wet Method Silica Dust Suppression System

If the excitement of the construction industry takes your breath away, congratulations! You’re in the right business. But construction workers may have shortness of breath for a far more serious reason—exposure to Respirable Crystalline Silica (RCS)—and that’s a grave problem that must be addressed immediately. Learn about it in this blog.

 

Watch this video to learn more about our fluid and gas handling capabilities.

 

Related content

Top 9 Parker Blogs of 2017

Most Popular Filtration Technology Blogs of 2017

5 Technology Trends Behind the Top Hydraulics Blogs of 2017

Top 5 HVACR and HVAC Climate Control Technology Blogs of 2017

Fluid and Gas Handling Technologies and Key Markets

 

Have a question about Parker products or services? We can help: Contact Us!

Comments for Optimize Hydraulic Systems with Top Fluid & Gas Handling Blogs of 2017


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha