Fluid Gas Handling

Parker’s Most Powerful Diagnostic Tool is Now Wireless

Parker’s Most Powerful Diagnostic Tool is Now Wireless - Sensor on gauge - Parker Hannifin SensoNODEEvery year, manufacturing processes get leaner to ensure companies stay competitive. Part of that is to keep assets working and avoid shutdowns as much as possible. But without a solid predictive maintenance plan in place, you’re subject to one of two things:

  • Mandatory shutdowns for routine maintenance to help prevent asset failure
  • Waiting for something to happen, then reacting

Diagnosing a problem before it occurs is the primary objective. For this, having a steady flow of data that can be analyzed is crucial to help maintenance technicians make informed predictions of when something needs attention. For years, Parker’s SensoControl® product line has been one of the most versatile diagnostic solutions for hydraulic and pneumatic applications. And now, one of the more popular devices is even stronger.

 

ServiceJunior™ CONNECT … fast, accurate, and wireless

With the Internet of Things becoming the gold standard in innovation, wireless diagnostic solutions are giving companies an edge in predictive maintenance. The ServiceJunior™ CONNECT is such a solution.

An integrated digital pressure sensor, ServiceJunior CONNECT features min/max memory capability, and with a scan rate of 10ms, ServiceJunior provides increased accuracy and faster frequencies to diagnostics. Its backlit, digital readout is more accurate than a mechanical diagnostic gauge, and because it works seamlessly with SensoNODE™ Blue Sensors and SCOUT™ Mobile Software, users can:

  • export records and proof-of-work statements
  • set alarms and send notifications
  • create/view trend graphs and asset records

In addition to all the benefits associated with a wireless diagnostic solution, ServiceJunior CONNECT is available in four versions with varying pressure ranges, making it ideal for hydraulics and pneumatics. ServiceJunior CONNECT is also scalable and expandable, and there’s no need to reconfigure your wired infrastructure.

 

Learn More

Parker’s Most Powerful Diagnostic Tool is Now Wireless - SensoControl Service Junior CONNECT - Parker Hannifin SensoNODETo learn more about Service Junior CONNECT, download the product bulletin or Visit our website

 

 

 

 

Parker’s Most Powerful Diagnostic Tool is Now Wireless - SensoNODE SCOUT catalog - Parker Hannifin SensoNODEDownload our product catalog to learn about condition monitoring for predictive maintenance.

 

 

 

 

Find a distributor

 

 

High Strain Sensor Wins Gold at Sensors Midwest - David Shannon, business team manager, Parker Quick Coupling Division

Contributed by David Shannon, business team manager, Parker HannifinParker Quick Coupling Division

 

 

 

 

 

 

 

 

Related posts: 

 

Expanded SensoNODE™ Line Launched at Sensors Midwest Conference

Wireless Transmission of Performance Data Extends Equipment Life

New IIoT Sensors Debut

How to Easily Connect Users to the Digital Plant

Condition Monitoring for Today’s Metal Fab Industry

Improve Solar Panel Maintenance and Condition Monitoring Efficiency

Efficiency is King In a Technological World 

 

Categories
Recent Posts by Author

What's the Difference Between Volumetric Flow and Mass Flow?

What type of flow measuring device should I use? This is a recurring question. The choice is bounded by customer needs, product variables and different technologies available on the market today. It’s...

New High Pressure Hydraulic Hose Replaces Rubber Hose in Oil and Gas Applications

Products used in the rigorous oil and gas industry must be resilient and of high quality to properly support these complex operations. Hoses and connections need to be safe, versatile and efficient....

Check Valves Are the Unsung Heroes of Fluid Power

Check valves are unseen and undervalued. These valves are found in just about every mobile and industrial hydraulic system on the planet. Simply put, if there’s a pump, most likely you will find...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Parker’s Most Powerful Diagnostic Tool is Now Wireless


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha