Closure of bars and restaurants. Decreased consumer demand.
Tightened budgets. The Coronavirus pandemic's impact on the food
and beverage industry has been considerable. Yet the sector...
Posted On 02/25/2021
Read More ►
Air handling unit (AHU) filters are used in an HVAC system to
prevent dust and other contaminants from circulating in a building.
They help improve indoor air quality (IAQ), which has become...
Posted On 02/25/2021
Read More ►
Even in optimal conditions, and in cases where hydraulic hose
assemblies were properly made, the life expectancy of any hydraulic
hose assembly is directly related to the operating parameters of
your...
Posted On 02/24/2021
Read More ►
Machine building is critical to countless industrial applications,
from metals processing to rubber and plastics, food packaging
to in-plant supporting operations. Equipment manufacturers...
Posted On 02/24/2021
Read More ►
When designing a gland in which an O-ring or elastomeric seal is
the desired sealing component, there are several aspects that need
to be considered. A perfectly designed seal with the right
material,...
Posted On 02/23/2021
Read More ►
If the words “Fire Seal” bring to your imagination a Sea World show
gone terribly wrong, then you probably won’t be interested in this
blog. But, for anyone associated with the field of aviation,...
Posted On 02/18/2021
Read More ►
The U.S. transportation industry is rapidly evolving to meet the
demand for clean energy. And for design engineers working at the
forefront of truck electrification, this represents an opportunity
to...
Posted On 02/17/2021
Read More ►
Most manufacturing facilities use compressed air to power their
production lines, but improper management of this unseen utility
during routine maintenance and emergency situations can have
serious...
Posted On 02/17/2021
Read More ►
Despite the uncertainty and challenges brought by changing times in
2020 specifically, the HVAC/R business was better than good for
industry professionals. Many companies experienced record sales...
Posted On 02/16/2021
Read More ►
Helen Fitzgerald was hired by Company founder Art Parker on
November 6, 1923. She was a confident 20-year-old woman, who grew
up on Cleveland’s West Side as the oldest of six children. After
high...
Posted On 02/15/2021
Read More ►
The original equipment manufacturer (OEM) parts are the best parts
to use when replacing a part on a machine. The OEM part will
be matched to the original specification of the machine and will
give...
Posted On 02/12/2021
Read More ►
For packaged wine to be successfully placed on the market within
the country of import, it must be microbiologically stable,
visually clear and particulate free. The accepted method of
achieving...
Posted On 02/11/2021
Read More ►
Combining innovative thinking with core technological competency
can tame the challenges of off-road machinery operating in
hazardous mining, agricultural, forestry, material handling,
and...
Posted On 02/11/2021
Read More ►
The marine market is especially demanding when it comes to high
pressure hydraulic connections. These need to withstand the
harshest conditions and vibrations. With classic welded connections
there...
Posted On 02/10/2021
Read More ►
When truck and trailer OEMs select DOT air brake fittings, a
number of considerations frequently come into play including
performance, price, assembly time and the ability to customize to
their...
Posted On 02/09/2021
Read More ►
Since its industry introduction in the 1960s, automation has made
an accelerated climb to be a significant trend in material handling
applications. Now, automated material handling systems handle...
Posted On 02/05/2021
Read More ►
Traditionally dependent on fossil fuels to run key equipment,
mining is known as a carbon-intensive industry. New trends, such as
battery-powered underground mining equipment, are promising to
disrupt...
Posted On 02/05/2021
Read More ►
In manufacturing and warehouse operations, forklifts are an
indispensable piece of equipment. Responsible for safely and
reliably lifting and transporting materials, the heart of these
machines is...
Posted On 02/04/2021
Read More ►
Considering that more than six million people live in the
Philadelphia region, government officials realized they needed a
fast-response emergency river vessel with both fire fighting and
rescue...
Posted On 02/03/2021
Read More ►
Unpredictable weather, stringent government regulation, and
dramatic changes in market conditions challenge the oil and gas
industry. Whether upstream or downstream, on land or at sea,
the most...
Posted On 02/03/2021
Read More ►