Process Control
Reducing Fugitive Emissions - Meeting ISO Standards with Process to Instrument Valves
Managing emissions is a major challenge for many companies. In Europe alone, a typical refinery can lose between 600 and 10,000 tonnes of fugitive emissions every year; and the majority of...
Read More ►
THM Analysis Applications in Water Treatment
The quick, accurate, and inexpensive measurement of Trihalomethanes (THMs) creates numerous opportunities to improve the water treatment process. THM levels can be lowered throughout the distribution...
Read More ►
Meeting NACE Requirements for Materials Used in the Manufacture of Fittings
Since the NACE (National Association of Corrosion Engineers) MR0175 standard was updated to ISO status in December 2003, there has been an air of confusion on what and how products conform to NACE....
Read More ►
Beyond Stainless Steel: Corrosion Resistant Alloys in the Oil and Gas Industry
From surgical equipment to cooking pans to skyscrapers, stainless steel has transformed the world as we know it today. Stainless steel is present in our daily lives and has made a significant impact...
Read More ►
Avoiding Corrosion Offshore
If you are an instrumentation engineer designing systems for offshore oil and gas platforms, you don’t need us to tell you about corrosion damage. It’s a huge and well-recognized problem, especially...
Read More ►
Three Reasons Why You Should Include Bolts in Material Specification
There are many reasons why bolts should be included in the material specification, particularly in the oil & gas and petrochemical industry. In this latest blog from the Process Control team,...
Read More ►
10 Tips to Ensure Best Practice in the Installation of Condensate Pots
Condensate pots play a key role in maximising the accuracy of differential pressure flow measurement on steam or vapour applications. When installed correctly, these simple devices can significantly...
Read More ►
Making Ash Analysis Simpler in the Field | White Paper
Traditional coal ash sampling and analysis using a laboratory facility can take a few hours if there is an on-site lab or days if the samples are sent away for analysis. Using the Parker...
Read More ►
A Wealth of Worldwide Opportunities For High Pressure Technology
There are many different industries that work with pressures over 10,000 psi, ranging from the oil and gas industry to laboratories and waterjet applications. With such high pressures and...
Read More ►
The Choice Between LNG and CNG as Transportation Fuel
Of the many transport fuel choices available today, none plays a more strategic role than natural gas in having an immediate and major positive economic and environmental impact. But of the two most...
Read More ►
Medium Pressure Safety - All Tubing is Not Created Equal
In industrial applications where high pressures (over 6,000 psi) are used, safety is of paramount importance. Even well below these pressures, precautions are needed to ensure a safe...
Read More ►
Counting the Cost of Cutting Corners in the Oil and Gas Industry
History is littered with examples of how cutting corners has led to near or actual disaster. Despite advances in instrumentation and tubing, small bore tubing assemblies still represent the...
Read More ►
Reducing Lost and Unaccounted Natural Gas
Lost and unaccounted for natural gas, particularly at pipeline custody transfer points, is becoming a focal point for both buyers and sellers. Even somewhat small measurement error can result in very...
Read More ►
Mixing Materials in Corrosive Environments
Selecting materials for a given application is one of the main design steps towards a safe and cost efficient system, yet a commonly overlooked stage, mainly performed from a purely...
Read More ►
How to Avoid Risk of Ignition When Oxygen is Present in Valve Applications
Manufacture of cryogenic valves where oxygen is present requires careful adherence to strict BAM and DIN standards to avoid ignition during use. It is a well-known fact that oils and grease...
Read More ►
Unravelling the Mystery of Supplying Instrumentation Products into Russia
In the past, the process of product manufacturers supplying into Russia was relatively straightforward. The manufacturer (ie. Parker) gained a GOST R certificate for the product, which was the state...
Read More ►
How to Avoid Boil-off Gas in Cryogenic Vessels
The space-saving benefits of storing gas in liquid form were recognised back in the 19th Century, but a practical, commercially viable solution for storing liquid gases did not come about until around...
Read More ►
Choosing the Right Tube Clamps for High Temperature Environments
Instrumentation tubing clamps are often used in very arduous environments, where they are faced with severe environmental conditions and high temperatures. The correct specification of clamp is...
Read More ►
How Parker's THM Analyzer Helps to Improve Safety of Drinking Water
Most public drinking water supplies in the developed world are treated with a disinfectant chemical such as chlorine, to eliminate any harmful organisms and to preserve the quality and safety of...
Read More ►
Improving Performance of Stream Switching Systems Under Low Air Conditions
As a user of analytical equipment such as process analyzers or gas chromatographs, are you affected by the vagaries of your compressed air supply? How often does a drop in its pressure affect...
Read More ►