techConnect

Proper Assembly Steps for 37° Flare Fittings Using the Flats Method

Learn how to properly assemble 37° flare fittings using the recommended flats method.
Properly assembling your fitting connections help to ensure that your systems install and stay leak-free. This is why we have started a series of assembly posts/videos featuring the proper assembly of the most popular tube and port ends. Today we are talking about the proper assembly steps for 37° flare fittings, which are also known as JIC fittings. Improper flaring or installation causes over half of the leakage with flared fittings. Thus, proper installation is critical for trouble-free operation.

For the 37° flare fitting, the flats method of installation is recommended because it is more forgiving than the torque method. It circumvents the effects of friction due to the differences in plating surfaces, finishes, and lubrication that can greatly influence the torque required to achieve proper joint tightness or clamping load.

Watch the video to learn the proper process for assembly of 37° flare fittings, or follow the steps outlined below.

 

Proper 37° flare fittings assembly and installation steps:

Step 1: Check your flared tube, if applicable. 
If connecting to a flared tube, start by verifying that the tube end is properly flared. The flare should be reasonably square and concentric with the other diameter of the tube. Ensure that it is free from rust, scratches, splits, embedded chips, and dirt, all of which can compromise the connection. For detailed instructions on proper tube end preparation, please see our blog post and video: Tube End Preparation Best Practices for Leak-Free Hydraulic Tube Fitting Connections.

Step 2: Align the flare ends and tighten.
Next, align the flared tube or hose end with the nose of the fitting. Lightly tighten the nut until you feel wrench resistance, approximately 30-inch pounds will be needed.

Step 3: Mark the nut.
It's good practice to mark the nut position relative to the body. Using a permanent marker, make a mark on one of the flats of the nut and continue the mark to the body of the fitting.

Step 4: Tighten using recommended flats.
Now tighten the nut further using the number of flats recommended in the Assembly and Installation section of the Parker Catalog 4300. A flat is equivalent to one side of the hexagonal nut, or one-sixth of a turn. 

Step 5: Make a second mark on the fitting.
Once properly tightened, use a permanent marker to place a second mark on the fitting adjacent to the previously marked line on the nut. This second mark serves as a check that the connection has been tightened during final inspection and allows for an easy check to see if the nut has come loose and backed off during operation. It also provides a reference for subsequent remakes.

Tech Tip: It's important not to force or "draw in" a tube assembly that is too short, too long, or misaligned. The misalignment places an undesirable strain on the joint leading to premature loosening/leakage. 

By following these steps, your 37° flare fitting connections will be properly installed. To help you ensure that all of your hydraulic fitting connections are installed properly, Parker Tube Fittings Division has created a series of tube and port end assembly and installation videos for the most common hydraulic fitting connections, which will be shared on TFDtechConnect.com over the next couple of months. You can also find detailed assembly and installation information for port end threads and tube fittings in the Assembly/Installation section of our Catalog 4300

Did you find this post helpful? Subscribe to TFD techConnect posts by email. TFD techConnect is a technically-focused monthly blog written by engineers for engineers specifically around motion and control engineering challenges.

Burleigh Bailey, senior product engineer at Parker Tube Fittings Division

 


Contributed by Burleigh Bailey, senior product engineer at Parker Tube Fittings Division

 

 

 

Additional related content about hydraulic tube, hose, and port fitting connections:
Assembly Instructions for Ensuring Leak-Free O-ring Face Seal Fittings

Proper Assembly Steps for Parallel Thread Adjustable Style Port End Fittings 

Non-Adjustable Parallel Thread Port End Assembly Instructions for Hydraulic Fittings 

Tapered Thread Port Assembly Instructions for Hydraulic Fittings

How Many Times Can I Reassemble a Hydraulic Fitting?

AN 37° Flare vs Industrial 37° Flare Fittings: What's the Difference?
 

Have a question about Parker products or services? We can help: Contact Us!

Comments for Proper Assembly Steps for 37° Flare Fittings Using the Flats Method

Andy Van Herwynen
Good video, like that it shows the 3-mark system. Should also show a hose end swivel nut, straight and 90 to show the two wrench method.
Rick Brown
Simple but important installation instructions.

Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha