Robotic surgery systems or robot-assisted surgery, offer immense patient benefits -- from shorter recovery time to better surgeon visualization, which leads to a more precise, effective, and successful surgery. Robot systems are used for various surgical procedures, including urologic, gynecologic, cardiothoracic, general, and head and neck surgeries. Manufacturers and designers of these surgical systems are now focusing on robot specialization instead of all-encompassing surgical systems.
This means there will be more specialized systems developed to perform specific surgeries, and the breadth of those procedures is expanding too. General surgery uses are increasing the fastest, followed by gynecology and urology uses. In 2017, there were 877,000 robotic surgeries performed in the US alone. That number is expected to rise exponentially in the years to come.
Robotic surgery system manufacturers and engineers consider EMI shielding when designing their systems. EMI shielding prevents equipment failure and keeps manufacturers compliant with federal regulations. Understanding EMI and taking steps to prevent it is paramount, as the resultant issues could cause robots to behave unexpectedly, such as requiring frequent restarts, showing a limited radio frequency range, moving unintentionally or affecting other nearby robots.
Remember, EMI is when electromagnetic emissions from a device or natural source interfere with another device or system. EMI might occur if the following three factors are present — the source of EMI, a coupling path, and a receptor.
The coupling path from the source to the receptor can be either an electric current, magnetic field, or electromagnetic field. The EMI source can be a natural source, such as lightning. It can also come from devices such as radios, computers, wireless networks, cell phones, or any electric device designed to transmit signals.
Robotic surgery systems are computer-controlled, and therefore sensitive electronic components must be shielded from electromagnetic interference (EMI) and generated heat must be effectively dissipated from various integrated circuits (ICs). On top of these stringent requirements, components must be able to withstand high heat sterilization and resist damage caused by harsh chemical cleaning agents in the hospital environment.
With proven solutions in EMI shielding and critical thermal management, Parker Chomerics gives you a wealth of integrated, multi-technology systems and components that meet or exceed your specifications and expectations.

This blog post was contributed by Jarrod Cohen, marketing communications for Parker Chomerics.
Related Articles:
Have a question about Parker products or services? We can help: Contact Us!
Comments for Protecting Robotic Surgery Systems from Electromagnetic Interference (EMI)
Please note that, in an effort to combat spam, comments with hyperlinks will not be published.