Filtration

Protecting Your Bioprocess From the Risk of Human Error

Protecting Your Bioprocess From the Risk of Human Error_Parker Bioscience Division_MistakeIn Parker Bioscience’s webinar entitled Protect The Process, Protect The Patient, the concern that biopharmaceutical manufacturers have regarding the impact of human error on their processes was all too evident.

When asked "what do you see as the biggest cause of operational errors?" 71.4 percent of participants cited "human error", compared to 14.3 percent who cited "consumables failure" and 7.1 percent who named "equipment failure" as the main culprit. 

Protecting Your Bioprocess From the Risk of Human Error_Parker Bioscience Division_View on Demand Icon
 
 
 
 

 

 

Protecting Your Bioprocess From the risk of Human Error_Parker Bioscience_Protect the Process Webinar Poll Results

The risk of human error and the subsequent damage this can cause to a process — product batches, delivery to market and ultimately, patient health — is clear.

But what can be done to mitigate this risk?

One option is to use automation. Let’s look at the main benefits that automation can provide within the single-use sector.

A fully manual process is very labour and operator intensive and involves a high level of manual data acquisition, manual analysis and manning of workstations. Indeed, sometimes many operators are required simply to look after one single process step.

Timings and end points can be subjective, and variation can be caused by human error.

 

Benefits of using automation

In a world of standardization, manual processing is not the ideal scenario. On the other hand, if we look at automation within the single-use sector, it can offer a huge number of improvements to biopharma process:

  • It can free up the operator and allows for safe and effective multitasking while ensuring the safety of processes and products.
  • It can reduce the number of operators required for the process tasks.
  • The process can be standardized with many single-use sensors such as those within Parker Bioscience’s SciLog® range controlling parameters such as pressure, and monitoring and feeding back on parameters such as conductivity and temperature.
  • Automation can eliminate many of the errors associated with human interfacing by utilizing standardized reliable programming to ensure consistency and robustness.
  • Data acquisition and analysis can be automated, and transcription error-free reports can be generated automatically.

Even with clear batch records and SOPs, it is possible there are differences in the way that different teams perform tasks, and there is also the potential for transcription and other human errors which can produce some variation in process controls, systems and quality documentation.

Also, when processes are transferred between facilities, there may be differences in the way processing steps are conducted in order to achieve facility fit. As much standardisation as possible surrounding this area would be an ideal scenario as it allows for faster implementation and validation.

Automation can help in all of these scenarios and is able to detect and reduce variation within processing parameters which would be impossible to perform manually.

Protecting Your Bioprocess From the Risk of Human Error_Parker Bioscience Division_View on Demand Icon
 
 
 
 
 
 
 
 
 
 
 

Protecting Your Bioprocess From the Risks of Human Error - Graeme Proctor, product manager - Parker BioscienceThis post was contributed by Graeme Proctor, product manager (single-use technologies), Parker Bioscience Division, United Kingdom

 

 

 

 

Parker Bioscience Division specializes in automating and controlling single-use bioprocesses. By integrating sensory and automation technology into a process, a manufacturer can control the fluid more effectively, ensuring the quality of the final product. Visit www.parker.com/bioscience to find out more.

 

Related Content

What's Stopping You From Automating Your Single-Use Process?

Automated Single-Use Technology and Its Impact on Quality

Engineering Managers: Streamline Your Bioprocess With Automation

Four Sources of Process Variation in Biopharmaceutical Manufacturing

A Strategy for Avoiding Manual Errors in Biomanufacturing

Have a question about Parker products or services? We can help: Contact Us!

Comments for Protecting Your Bioprocess From the Risk of Human Error


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha