Fluid Gas Handling

Pump Design Solves Dry Run Failures for Facility Operators in Oil and Gas

Pump Design Solves Dry Run Failures in the Oil and Gas Market - Gas storage tank farm - Parker Hannifin

Facility operators in the oil and gas industry have raised concerns on how to solve their top failure modes: extremely short or non-existent dry run pump time limits and unacceptable levels of cavitation when pumping extremely light liquids with high vapor pressures. 

Pump cavitation and dry run related failures cost companies millions of dollars annually, including replacement costs for damaged equipment and lost sales due to poor performance. With an improving economy and anticipated fuel production increase, sales of fluid-handling pumps are forecast to rise 5.5% annually to $84 billion in 2018. Given this proliferation, the historical pattern suggests that costs associated with repairs or replacements also will increase dramatically.

Learn how Parker's innovation in pump technology can reduce your operational downtime, decrease operating costs, and improve performance. Download our white paper now.

 

Disastrous consequences

Dry running occurs when a pump operates without sufficient lubricating liquid around the pumping element. This can be caused by either widespread vapor formation, also known as cavitation, inside the pump or absence of pumping fluid altogether. These adverse conditions can lead to dangerously unstable pressure, flow, or overheating which may cause the pumping element to seize or break.

When cavitation occurs, vapor bubbles form and expand in the pumping liquid on the suction side of the pump before reaching the higher-pressure discharge side of the pump and violently collapsing near the surface of the pumping element. This triggers shock waves inside the pump which cause significant damage to the pumping element. If left untreated, cavitation will destroy the pumping element and other components over time, drastically shortening the pump’s life.

Cavitation may also cause excessive vibration leading to premature seal and/or bearing failure, in addition to creating an immediate increase in power consumption and a decrease in flow and pressure output.

Cavitation itself may also be so widespread that it creates a dry run situation inside the pump due to excessive vapor formation. Pumps most often rely on the pumping fluid itself to lubricate the bearing surfaces of the pumping element – if a pump is operated without this fluid, the low to non-existent lubrication at these bearing surfaces will cause excess heat generation, increased wear, and potentially even failure of the pump if the pumping element seizes or breaks. The life of a pump subjected to dry run will be significantly reduced or, in the worst case, brought to an untimely end.

 

Human error as the main cause of dry running

Pump Design Solves Dry Run Failures for Facility Operators in Oil and Gas - transfer facility oil and gas facility - Parker Hannifin Whereas cavitation is a common cause of pump degradation and failure related to the physics involved in the pumping operation, dry running, on the other hand, is usually related to how pumps are actively operated by end users. The most immediate cause of dry running is usually human error. Companies rely on operators to monitor their pumps, but problems occur in cases where operators unintentionally leave pumps running after the pumping operation is complete.

 

Despite an operator’s best efforts, harmful events still may occur from:

  • malfunctioning monitoring systems;

  • improper use of even well-designed control equipment;

  • pumps running overtime after the pumping operation is complete;

  • unpredictable events.

 

Solving the dry running challenge

Pump Design Solves Dry Run Failures for Facility Operators in Oil and Gas  | 3-inch Fluid Transfer System | Parker HannifinOur engineers were up for the challenge and developed the next generation solution of fluid transfer systems. The new technology combines advanced engineering and manufacturing capabilities to deliver a rugged solution for stationary, mobile, and high vapor-pressure fluid applications.

The solution offers customers efficiency improvements as well as increases their uptime, which ultimately translates into revenue to the bottom line.

“What separates our solution from our competitors is, our technology is automated and integrated into the pump design. You don’t need to worry about pumps stopping and starting every 20 – 30 seconds, they will dry run continuously.”
James Chu, PE, chief engineer, Corporate Technology Ventures, Parker Hannifin

 

Pump Innovation solves dry run failures in Oil and Gas Market | Download whitepaper

Learn how this innovation in pump technology can reduce your operational downtime, decrease operating costs, and improve performance. Download our white paper now.

 

 

Pump Design Solves Dry Run Failures for Facility Operators in Oil and Gas - Sara Weichman business development manager - Fluid Transfer Solutions, Parker Hannifin Article contributed by Sara Weichman, business development manager, Fluid Transfer Solutions, Parker Hannifin

 

 

 

 

Related, helpful content for you:

Continuously Dry Runnable Lobe Pump Maximizes Uptime

Counting the Cost of Cutting Corners in the Oil and Gas Industry

Advanced Material Development for High-Pressure/High-Temperature Oil & Gas Extraction

Macro Motion Control and Drive Solutions Meet Demands of Offshore

Do Your Seals Meet the Demands of the Oil and Gas Industry?

 

 

 

 

Categories
Recent Posts by Author

How Condition Monitoring Can Transform the Food and Beverage Industry

Our sense of taste is changing. We’re becoming more health conscious of the foods and beverages we consume to living a better life. No more perplexing and hard-to-pronounce food labels....

Frequently Asked Questions About Seal-Lok for CNG Fittings

Seal-Lok for CNG Fittings and Adapters provide reliable natural gas fuel conveyance in CNG applications with an O-ring face seal design that incorporates an elastomeric seal compound made of...

Any pressure. Any project. One solution. Infographic

GlobalCore is the future that OEMs and end users around the world have been asking for: a unified family of robust hydraulic hoses designed to endure the tough conditions where work gets...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Pump Design Solves Dry Run Failures for Facility Operators in Oil and Gas


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha