Today, in the midst of the COVID-19 pandemic, keeping workers, patients and families safe from the spread of disease in facilities is more important than ever. For facilities managers, this means employing various strategies that can reduce the threat of transmission in:
The spread of the novel coronavirus (COVID-19) mainly occurs through respiratory droplet transfer from person-to-person within a close range of about six feet according to the Center for Disease Control (CDC). The virus can be transmitted on skin, objects, and surfaces that a contagious person may cough on, sneeze on, or touch.
Pathogens can also travel on dust and dirt particles as those particles move through the air. Therefore, the potential for airborne transmission through an HVAC system exists.
As part of a protection plan, maintaining healthier breathable air in facilities can help to reduce the risk of infection.
Our team members work collaboratively to solve the unique challenges presented by the coronavirus pandemic.
One recent example is the collaboration between two Parker Divisions to provide a new government-approved HVAC filtration solution to up to 8 remote hospital sites in New Jersey—one of several regions in the U.S. where patient intake had greatly outpaced the capacity of local hospitals.
The team needed to develop a filtration solution for an air handling system used to generate clean air for emergency workers in medical tents set up for overflow care. And they needed to act quickly, turning around a solution in five days.
To support a comprehensive protection plan that reduces the risk of airborne transmission for hospital staff and patients, Parker offers a range of high-efficiency filters that:
HVAC filters can reduce but not eliminate the threat of infection. The coronavirus and the particulate it travels on is very small in size and can range from sub-micron (less than 1.0 micron in size) and larger. High-efficiency filters on the market today can trap particulate sizes that are likely to remain in the air. Selecting the right filter can reduce risk while improving the quality of indoor air.
Parker is dedicated to providing honest and transparent information about our filtration products to help customers decide which technologies provide the highest chances of trapping virulent pathogens before they enter a building or circulate to different rooms.
— Parker HVAC Filtration Division
IMPORTANT: Parker’s products can reduce airborne particulate in a controlled environment. They would not eliminate the risk of exposure to airborne viruses but can be part of a comprehensive plan to help reduce that risk.
The American Society of Heating, Refrigerating and Air-Conditioning Engineers (ASHRAE) has developed proactive guidance for building industry professionals to help address the ongoing concerns of the coronavirus (COVID-19) outbreak. Please visit www.ashrae.org to access the latest response resources from ASHRAE/Covid19 and other leading organizations with respect to the operation and maintenance of HVAC systems.
Parker HVAC filters are manufactured in the U.S. and engineered to the highest standards of design, quality, and assembly. When selecting a filter to combat the threat of airborne transmission, we suggest a minimum efficiency reporting value (MERV) rating of 13 to 16. The higher the value, the better the filter will be at capturing small particles. Our Sub-HEPA, HEPA, and ULPA filters provide the highest level of protection (up to 99.999% on 0.12 microns). Our MERV 16 rated filters provide 90% and higher efficiencies, capturing airborne particles that are the size of viruses.
The following high-efficiency filters are designed for commercial use. All of them meet Leadership in Energy Design (LEED) requirements. They can be ordered through our global network of dealers and distributors.
This post was contributed by the HVAC Filtration Team.
Bring Our Purpose to Life: On the Front Lines of the Covid-19 Crisis
Defining Our Unique Contribution to the World
Critical Systems and Components for Ventilator Manufacturing
Supporting Medical Device Manufacturing With Business Critical Parts
Learn more about Parker's solutions for Healthcare and Life Science Industry
Have a question about Parker products or services? We can help: Contact Us!
Comments for Reducing Airborne Transmission with HVAC Air Filters
Please note that, in an effort to combat spam, comments with hyperlinks will not be published.