Hydraulic Filtration

Rising Tide of Clean Power

Rising Tide of Clean Power - wind turbine cutawayRising tide of clean power. Gearbox lubrication and thorough sealing of equipment in the Atlantis project.

Turning on the lights is taken for granted by most, yet with a quarter of electricity generating capacity being lost over the next decade, the search is on to find cleaner sustainable power for the next generation.

Rising tide of clean power

Producing adequate power is vital to daily life, yet the process is largely neither clean nor efficient. Indeed, in many parts of the world, smog from coal-fired power generation stations remains a visible reminder of the problem. And, it is not just the threat to human health, all kinds of ecological systems are suffering as a consequence. Despite some skeptics dismissing evidence on climate change, pollution and its adverse effects are undisputed. The past decade has seen the rapid rollout of wind farms both in and around the UK, a move mirrored throughout much of Europe. It is the first major step in cleaning up power production. Despite a slower start than many would have liked, last year wind-based renewable energy made up 11% of electric power generation.

Despite the success, however, a fundamental problem remains the baseload requirement. Baseload is the minimum level of power demand on the electrical network over a 24 hour period. And since baseload power sources are those plants that generate continuous and dependable power – wind turbines are never likely to take over completely.

“The UK baseload requirement comes from nuclear; you can’t cycle it, it is on or off. But, overnight you find there is no demand,” said Peter Oram, global renewables sales at General Electric Power Conversion.

As electricity can’t be stored in volume, if it is not used at the point of production, it is lost. And with plants only shutting for maintenance, baseload thermal power plant operations can be inherently inefficient.

The unpredictability of wind combined with the need to keep nuclear plants on means the current infrastructure is far from ideal. But, not all renewable sources of power are created equally.

For years many have questioned why tidal and wave power has not featured more highly in the mix. In all probability it’s likely they will, once the engineering is more fully developed and better understood. Offshore wind power has had its fair share of unforeseen maintenance issues, having equipment underwater only compounds the difficulties.

Take a step back, though, and the global renewable energy picture is very different. Power generation from moving water is actually the planets' biggest source of renewable energy by some margin. Hydro plants are common, reliable, efficient, well understood, and clean.

The trouble is, not everywhere has the nature channels and lagoons to exploit the resource. So then, why not build them instead?

This is the principle being put forth by Tidal Lagoon Power. The company wants to build artificial lagoons in areas that have high tidal ranges. It is currently developing its first project in Swansea Bay to show the principle but wants to have lagoons built all around the UK and beyond.

The concept is simple, as water floods into the lagoons it rotates turbines that produce electricity. This process is mirrored at lower tides as the water is released out of the lagoon producing predictable and reliable clean power. What’s more, due to regional differences in the time of high tide and low tide, the system can be made up of a series of lagoon networks that can produce 24-hour power.

“Tidal is the new baseload,” said Oram. “Nuclear is about 18GW in the UK, so if you follow that tidal pattern around the UK you almost get yourself a baseload replacement for nuclear, but this lasts 120 years.”

General Electric is partnering with Tidal Lagoon on the project, developing the turbine systems and power electronics that will make the system smart, flexible, and responsive to grid demand. GE brings years of operational experience in maintaining thermal and hydropower plants to give the project technical soundness and genuine commercial credibility.

At the heart of this work are GE’s large induction generators and variable speed drives (VSD) based on its medium voltage drive technology and hydro turbine technology supplied by partner Andritz Hydro. The equipment is well proven across multiple industrial and renewable energy applications such as onshore and offshore wind, oil and gas and marine.

“We are able to connect remotely to our plants and every single inverter,” said Oram. “We can then take that data, feed it back to optimise operations, and improve products in the future.”

The UK is currently in transition with eight nuclear reactors and nine coal-fired power stations closing over the next eight years. It means 21,000 MW, around one-quarter of total installed capacity, will be lost.

This has prompted the Government to commit to a new generation of nuclear reactors, potentially by foreign contractors. While nuclear is certainly a low carbon option, the nuclear waste generated is far from environmentally inert. Tidal Lagoon, however, has ambitions to offer an alternative renewable option that will last longer, and potentially fill the energy gap.

Chief executive of Tidal Lagoon Power, Mark Shorrock, said: “Our ambition is predictable baseload renewable energy. Our first project at Swansea Bay is playing with 10m high tides. The concept is to build a big breakwater wall, 9.5km long. That is 11.5km2 of water that we impound. We put generators between the lagoon and ocean and wait three hours for the tidal difference. Then we exchange a 100m3 of water over the next four hours through turbines as we empty the lagoon. We generate electricity in the same way when water comes in. We can also delay generation by up to 90 minutes.”

Swansea Bay will use 16, 7.5m turbines, giving 320MW of installed capacity and 14 hours of reliable power generation every day. At an expected cost of £1 billion, many have pointed out a similarly priced gas-fired power station could produce as much as 1000MW. Tidal Lagoon argues that purchase cost can be deceiving and it is through life cost that really shows the true comparison.

Fuel costs for a gas-fired power plant over a 25-year life are high, volatile, and dependant on supply from other countries. It is also polluting and needs significant maintenance. Tidal Lagoon states its hydropower stations have an operational lifespan of 120 years, with no major refurbishment needed for the first 50 years of operation. In short, far less maintenance and zero fuel costs.

“You put in this infrastructure, and it goes and goes,” said Shorrock. “And we are adamant we are not making these turbines in China or the Far East. We want to source, use the expertise and manufacturing base that is here in the UK for as much of this project as possible. We have a fundamental theme in the company that is we have to be reverent towards nature in what we do. To try and live in harmony with it. We want the birds to still live there, the mollusks and nature to thrive.”

It is clear that Shorrock doesn’t want this to be a one-off project and he has big plans for its expansion. “Swansea Bay, we hope, gives birth to an industry,” he said.

With the construction of the breakwater due to start in 2017 and operation due to start in 2020, it remains to be seen if this prototype project will deliver on its promises and live up to high expectations.

Not alone

However, the Tidal Lagoon project is not the only tidal renewable energy project that is gaining traction. The MeyGen Project, for example, claims to be the largest planned tidal energy project in the world. Here, energy generation takes perhaps the more traditional form of turbines placed on the ocean floor, a concept known as tidal stream generation. As tides flow in and out of channels, they turn the turbines and generate electricity in much the same way as wind turbines.

The turbines are being produced by Atlantis / Lockheed Martin and Andritz Hydro Hammerfest and the project is scheduled to install four 1MW turbines in 2016. These will prove the concept and power approximately 3,000 homes, before the array is scaled up to 80+ turbines, and finally, in early 2020, the remaining turbines to make up the 396MW of capacity.

The MeyGen array will be located 2km off the north Caithness coast within the Inner Sound of the Pentland Firth. The area is recognised as a highly active site for tidal flows with a maximum tidal current speed of 5m/s.

“We are witnessing the transformation of a sector. MeyGen is one of the most exciting and innovative renewable energy developments in the world, marking the long-awaited arrival of tidal stream generation as a serious, large-scale player in global energy markets,” said Atlantis chief executive, Tim Cornelius

Suppliers step up

The tidal renewable energy development has required many in the supply chain to procure equipment and subsystems that are capable of withstanding the underwater environment.

“There is a lot customisation in MeyGen, but we are trying to do it with as many standard components as possible.” said Callum McConnell, global business development manager, at Parker Hannifin.

Parker has played a critical part in providing many components including gearbox lubrication and thorough sealing of equipment. However, a major part of keeping the underwater turbines moving has been the condition monitoring systems and predictive maintenance.

Condition monitoring plays a big role in the project,” said McConnell. “We need to know what is happening inside the nacelles, with the lubrication, hydraulics and power electronic systems. It allows the operator to more easily predict problems. You might see water in the oil, or metal particles, and that will tell a certain story about what is going on so you can accurately predict how long it might last before something fails. If you know when something is going to fail, it allows you to plan ahead and not wait for unscheduled breakdowns.”

Despite the ongoing wait for the broader rollout of renewables, it looks as if many of the known problems of tidal energy are being overcome. However, this is all before the build phase has even started. It is an anxious time, no doubt, for engineers as this is when the unknown problems tend to arise. In the short term expect some increases in cost and delays in the project. But long term, expect a cheap and clean power. A fair compromise?

Fact File: Tidal Lagoon vs MeyGen

 

 

 

 

 

Tidal Lagoon - area

 

Tidal Lagoon – not without controversy

Despite strong initial backing, the Government’s stance has softened significantly in recent months. The Prime Minister admitted last month his enthusiasm had been ‘reduced’. The reservations were reportedly related to engineering concerns raised around the turbines, and the merit of the Lagoon’s power producing capability. While the site is a prototype to prove the concept, in practice, any significant unforeseen side effects would spell disaster for the £1 billion project. The Government does not want the lagoon to turn into a money pit and political embarrassment.

The turbines are developed off the back of experience gained in hydro generation facilities, but there is lack of practical measurement using them in this way. Using the turbines to generate power in two directions assumes equal efficiency, yet some experts have called this a theoretical prediction that will not hold up in real operation.

Tidal Lagoon Power said questions on the engineering and environmental impact had been addressed in depth by experts through a robust planning and validation process.

Written by: Justin Cunningham | Published: 10 February 2016 | Eureka magazine

 

Submitted by Callum McConnell, renewable energy - business development manager - EMEA Calum McConnell

Hydraulic & Fuel Filtration Division 

 

 

RELATED CONTENT

Websites

GE Power Conversion Ltd

http://www.meygen.com/

http://www.tidallagoonpower.com/

________________________________________

Condition Monitoring Solutions for Power Generation Plants

Innovative New Fluid Purifier Saves Time, Money in Hydroelectric Plants

 

Categories
Recent Posts by Author

How to Perform a Cold Corrosion Test for Cylinder Oil

The oil used to lubricate the cylinders of large 2-stroke marine diesel engines has to contend with high temperatures and acidic products formed during the combustion of sulphur-rich bunker...

Industrial Machine Vibration Analysis and Condition Monitoring

A condition monitoring system is concerned with the early detection of failure. Vibration monitoring systems, whether they use traditional techniques based on displacement or acoustic emission sensor...

Fuel Monitoring Matters

Whether you choose distillates, liquefied natural gas (LNG) or scrubbers to meet the new International Maritime Organization (IMO) fuel regulations in 2020, it will be even more critical to regularly...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Rising Tide of Clean Power


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha